The util_adxcvr IP core instantiate a Gigabit Transceiver (GT) and set's up the required configuration. Basically is a simple wrapper file for a GT* Column, exposing just the necessary ports and attributes.
Currently this IP supports three different GT type:
The following diagram shows a GTXE2 Column, which contains four GT Quad. Each quad contains a GTEX2_COMMON and four GTXE2_CHANNEL primitive.
Name | Description | Default Value |
---|---|---|
XCVR_TYPE | Define the current GT type, GTXE2(0), GTHE3(1), GTHE4(2) | 0 |
QPLL_REFCLK_DIV | QPLL reference clock divider M, see User Guide for more info | 1 |
QPLL_FBDIV_RATIO | QPLL reference clock divider N ratio, see User Guide for more info | 1 |
QPLL_CFG | Configuration settings for QPLL, see User Guide for more info | 27'h0680181 |
QPLL_FBDIV | QPLL reference clock divider N, see User Guide for more info | 10'b0000110000 |
CPLL_FBDIV | CPLL feedback divider N2 settings, see User Guide for more info | 2 |
CPLL_FBDIV_45 | CPLL reference clock divider N1 settings, see User Guide for more info | 5 |
TX_NUM_OF_LANES | Number of transmit lanes. | 8 |
TX_OUT_DIV | CPLL/QPLL output clock divider D for the TX datapath, see User Guide for more info | 1 |
TX_CLK25_DIV | Divider for internal 25 MHz clock for the TX datapath, see User Guide for more info | 20 |
TX_LANE_INVERT | Per lane polarity inversion. Set the n-th bit to invert the polarity of the n-th transmit lane. | 0 |
RX_NUM_OF_LANES | Number of transmit lanes | 8 |
RX_OUT_DIV | CPLL/QPLL output clock divider D for the RX datapath, see User Guide for more info | 1 |
RX_CLK25_DIV | Divider for internal 25 MHz clock for the RX datapath, see User Guide for more info | 20 |
RX_DFE_LPM_CFG | Configure the GT use modes, LPM or DFE, see User Guide for more info | 16'h0104 |
RX_PMA_CFG | Search for PMA_RSV in User Guide for more info | 32'h001e7080 |
RX_CDR_CFG | Configure the RX clock data recovery circuit for GTXE2, see User Guide for more info | 72'h0b000023ff10400020 |
RX_LANE_INVERT | Per lane polarity inversion. Set the n-th bit to invert the polarity of the n-th receive lane. | 0 |
Interface | Pin | Type | Description |
---|---|---|---|
Microprocessor clock and reset | |||
up_clk | input | System clock, running on 100 MHz | |
up_rstn | input | System reset, the same as AXI memory map slave interface reset | |
PLL reference clock | |||
qpll_ref_clk_0 | input | Reference clock for the QPLL | |
cpll_ref_clk_0 | input | Reference clock for the CPLL | |
RX interface | |||
rx_*_p | input | Positive differential serial data input | |
rx_*_n | input | Negative differential serial data input | |
rx_out_clk_* | output | Core logic clock output. Frequency = serial line rate/40 | |
rx_clk_* | input | Core logic clock loop-back input | |
rx_charisk_* | output[ 3:0] | RX Char is K to the JESD204B IP | |
rx_disperr_* | output[ 3:0] | RX disparity error to the JESD204B IP | |
rx_notintable_* | output[ 3:0] | RX Not In Table to the JESD204B IP | |
rx_data_* | output[31:0] | RX data to the JESD204B IP | |
rx_calign_* | input | RX enable comma alignment from the JESD204B IP | |
TX interface | |||
tx_*_p | output | Positive differential serial output | |
tx_*_n | output | Negative differential serial output | |
tx_out_clk_* | output | Core logic clock output. Frequency = lane rate/40 | |
tx_clk_* | input | Core logic clock loop-back input | |
tx_charisk_* | input[ 3:0] | TX Char is K from the JESD204B IP | |
tx_data_* | input[31:0] | TX data from the JESD204B IP | |
Common DRP interface | |||
up_cm_* | IO | The common DRP interface, must be connected to the equivalent DRP ports of AXI_ADXCVR. This is a QUAD interface, shared by four transceiver lanes. This interface is available only if parameter QPLL_ENABLE is set to 0x1. | |
Channel DRP interface | |||
up_ch_* | IO | The channel DRP interface, must be connected to the equivalent DRP ports of AXI_ADXCVR. This is a channel interface, one per each transceiver lane. | |
Eye Scan DRP interface | |||
up_es_* | IO | The Eye-Scan DRP interface, must be connected to the equivalent DRP ports of UTIL_ADXCVR. This is a channel interface, one per each transceiver lane. This interface is available only if parameter TX_OR_RX_N is set to 0x0. |
For porting on different Xilinx transceiver types, there is the following guide.
the util_adxcvr allocates resources/quads (channels and common) sequentially. Meaning if you have 8 lanes, it will insert two quads, 4 channels and a common block for each quad.
Channels within a quad are tightly coupled to the common block, the placement of the channel resources can be permuted within a quad and is affected by the constraint file with the restriction that rx_<N>_p/n connect to tx_<N>_p/n must connect to the same channel.
Supposing we have the following pin constraints and connections to the util_adxcvr:
So in this case we end up with a conflict during implementation:
We have to ensure that in implementation the mapping is correct either by rearranging the Rx connections.
or the Tx connections of the util_adxcvr
In such cases when rearrangement is required due placement constraints, complementary reordering is required either in the converter device (lane crossbars) or inside the FPGA between the physical and link layer to connect the logical lanes with the same index on both end of the link.
The software can configure this core through the AXI_ADXCVR IP core.