This is an old revision of the document!
The 7 series and Ultrascale FPGAs Transceivers Wizard can be used to configure the transceivers inside the util_adxcvr cores. In general in all reference designs the gigabit transceivers are configured to the highest supported line rate of the device. If the user want to use their system in a different line rate, she need to reconfigure the transceivers. This can be done by software, which does the reconfiguration through the DRP interface of the transceivers. Due the complexity of the transceivers, it can happen that the user needs to do addition settings in HDL using the Wizard. The following wiki provides a short guide how to use the wizard to generate a transceiver configuration for a JESD204B interface.
The following features are required for a JESD204B interface:
To start the wizard in the Vivado, a project should be loaded with a 7 Series FPGA which has gigabit transceivers. In the Project Manager select IP catalog and search after the keyword wizard, then select the 7 Series FPGAs Transceivers Wizard IP.
You can define a custom name for your component and leave it on default. The tools should recognize your transceiver type automatically, if not you may have to double check if you have the right FPGA device selected for your project. You also need to select Include Shared Logic in core at the Shared Logic section in order to have both COMMON and CHANNEL instances in the generated code.
First, you need to select JESD204 as targeted protocol and specify your line rate and reference clock. A valid reference clock is depending on your line rate, make sure that you're using a valid reference clock form the drop-down list. Also you should set the used PLL's for TX and RX. If your line rate is equal for both directions, you can use the same PLL. Be aware that each PLL's VCO have a different frequency range, where the circuit can function correctly, if you targeted line rate is to high or too low, you may be restricted to use just one of the two PLL's. All other settings can be left on its default value in this tab.
If you selected JESD204 to be the used protocol, you don't have to change anything here. The JESD204B interface is using 8B/10B encoding/decoding, and the internal data width will be 40 bits. In all the reference designs the DRP frequency is connected to the system clock (100 MHz). At the Synchronization and Clocking section, both TX and RX should have an enabled buffer. The PLLREFCLK is used as the source for TXOUTCLK and RXOUTCLK.
The setting at the tabs PCIe, SATA, PRBS and CB and CC Sequence can be left with its default values.
Location of the COMMON instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/<component_name>_common.v Location of the CHANNEL instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/<component_name>_gt.v
[~] less daq2_zc706.srcs/sources_1/ip/gtwizard_0/gtwizard_0_common.v [~] less daq2_zc706.srcs/sources_1/ip/gtwizard_0/gtwizard_0_gt.v
This instances should be compared with the COMMON and CHANNEL instances used in util_adxcvr_cm.v and util_adxcvr_ch.v.
The overall workflow with the Ultrascale FPGAs Transceiver Wizard is similar to the 7 Series ones, it just has a different GUI. To open up the wizard in the Project Manager select IP Catalog and search after the keyword wizard, then select the Ultrascale FPGAs Transceivers Wizard. You can define a custom name for your component and leave it on default. The tools should recognize your transceiver type automatically, if not you may have to double check if you have the right FPGA device selected for your project. To apply the general JESD204B setting, select the GTH-JESD204 preset. In the first tab, called Basic you can find all the necessary settings. Select the targeted line rate, PLL and reference clock. The tool will tell what PLL and reference clock can be used with a specific line rate. Note that the current version of the util_adxcvr core does not support QPLL Fractional-N option.
To have both COMMON and CHANNEL instances inside the generated core, at the Structural Options tab the Include transceiver COMMON in the Core must be selected.
To find the actual instance attributes, two different file should be examined. A generic one, which contains the actual software macro instance, and a wrapper, which instanciate the previous file, and sets the required attributes.
Location of the COMMON instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/gtwizard_ultrascale_v1_7_gthe4_common.v
Location of the COMMON wrapper: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/<component_name>_gthe4_common_wrapper.v
Location of the CHANNEL instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/gtwizard_ultrascale_v1_7_gthe4_channel.v
Location of the CHANNEL instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/<component_name>_gthe4_channel_wrapper.v
[~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gtwizard_ultrascale_v1_7_gthe4_common.v [~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gth_jesd204_gthe4_common_wrapper.v [~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gtwizard_ultrascale_v1_7_gthe4_channel.v [~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gth_jesd204_gthe4_channel_wrapper.v
This generated attributes values should be compared with the values used with the COMMON and CHANNEL instances in util_adxcvr_cm.v and util_adxcvr_ch.v.