Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:docs:hdl:regmap [27 Jan 2022 13:29] – ADC, DAC external sync Laszlo Nagyresources:fpga:docs:hdl:regmap [19 Feb 2024 13:35] (current) – [PWM Generator (axi_pwm_gen)] Quick register fixes Adrian Costina
Line 1: Line 1:
- 
- 
 ==== Base (common to all cores) ==== ==== Base (common to all cores) ====
  
Line 25: Line 23:
 |::: |::: |[9] |SCALECORRECTION_ONLY |RO |0x0 |If set, indicates that the IQ Correction module implements only scale correction. IQ correction must be enabled. (as a result of a configuration of the IP instance) | |::: |::: |[9] |SCALECORRECTION_ONLY |RO |0x0 |If set, indicates that the IQ Correction module implements only scale correction. IQ correction must be enabled. (as a result of a configuration of the IP instance) |
 |::: |::: |[12] |EXT_SYNC |RO |0x0 |If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal. | |::: |::: |[12] |EXT_SYNC |RO |0x0 |If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal. |
 +|::: |::: |[13] |RD_RAW_DATA |RO |0x0 |If set, the ADC has the capability to read raw data in register REG_CHAN_RAW_DATA from adc_channel. |
 ^0x0004 ^0x0010 ^REG_PPS_IRQ_MASK ^^^^PPS Interrupt mask ^ ^0x0004 ^0x0010 ^REG_PPS_IRQ_MASK ^^^^PPS Interrupt mask ^
 | | |[0] |PPS_IRQ_MASK |RW |0x1 |Mask bit for the 1PPS receiver interrupt | | | |[0] |PPS_IRQ_MASK |RW |0x1 |Mask bit for the 1PPS receiver interrupt |
Line 32: Line 31:
 |::: |::: |[15:8] |SPEED_GRADE |RO |0x0 |Encoded value describing the FPGA's speed-grade | |::: |::: |[15:8] |SPEED_GRADE |RO |0x0 |Encoded value describing the FPGA's speed-grade |
 |::: |::: |[7:0] |DEV_PACKAGE |RO |0x0 |Encoded value describing the device package. The package might affect high-speed interfaces | |::: |::: |[7:0] |DEV_PACKAGE |RO |0x0 |Encoded value describing the device package. The package might affect high-speed interfaces |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 50: Line 49:
 |::: |::: |[15] |SYMB_OP |RW |0x0 |Select symbol data format mode (0x1) | |::: |::: |[15] |SYMB_OP |RW |0x0 |Select symbol data format mode (0x1) |
 |::: |::: |[14] |SYMB_8_16B |RW |0x0 |Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b) | |::: |::: |[14] |SYMB_8_16B |RW |0x0 |Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b) |
-|::: |::: |[12:8] |NUM_LANES[4:0] |RW |0x0 |Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane) |+|::: |::: |[12:8] |NUM_LANES[4:0] |RW |0x0 |Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane).  For AD7768, AD7768-4 and AD777x number of active lanes : 1/2/4/8 where supported. |
 |::: |::: |[3] |SYNC |RW |0x0 |Initialize synchronization between multiple ADCs | |::: |::: |[3] |SYNC |RW |0x0 |Initialize synchronization between multiple ADCs |
 |::: |::: |[2] |R1_MODE |RW |0x0 |Select number of RF channels 1 (0x1) or 2 (0x0). | |::: |::: |[2] |R1_MODE |RW |0x0 |Select number of RF channels 1 (0x1) or 2 (0x0). |
 |::: |::: |[1] |DDR_EDGESEL |RW |0x0 |Select rising edge (0x0) or falling edge (0x1) for the first part of a sample (if applicable) followed by the successive edges for the remaining parts. This only controls how the sample is delineated from the incoming data post DDR registers. | |::: |::: |[1] |DDR_EDGESEL |RW |0x0 |Select rising edge (0x0) or falling edge (0x1) for the first part of a sample (if applicable) followed by the successive edges for the remaining parts. This only controls how the sample is delineated from the incoming data post DDR registers. |
 |::: |::: |[0] |PIN_MODE |RW |0x0 |Select interface pin mode to be clock multiplexed (0x1) or pin multiplexed (0x0). In clock multiplexed mode, samples are received on alternative clock edges. In pin multiplexed mode, samples are interleaved or grouped on the pins at the same clock edge. | |::: |::: |[0] |PIN_MODE |RW |0x0 |Select interface pin mode to be clock multiplexed (0x1) or pin multiplexed (0x0). In clock multiplexed mode, samples are received on alternative clock edges. In pin multiplexed mode, samples are interleaved or grouped on the pins at the same clock edge. |
-^0x0012 ^0x0048 ^REG_CNTRL_2 ^^^^DAC Interface Control & Status ^+^0x0012 ^0x0048 ^REG_CNTRL_2 ^^^^ADC Interface Control & Status ^
 | | |[1] |EXT_SYNC_ARM |RW |0x0 |Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a ADC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. | | | |[1] |EXT_SYNC_ARM |RW |0x0 |Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a ADC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
 |::: |::: |[2] |EXT_SYNC_DISARM |RW |0x0 |Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. | |::: |::: |[2] |EXT_SYNC_DISARM |RW |0x0 |Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
 |::: |::: |[8] |MANUAL_SYNC_REQUEST |RW |0x0 |Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. | |::: |::: |[8] |MANUAL_SYNC_REQUEST |RW |0x0 |Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
 +^0x0013 ^0x004c ^REG_CNTRL_3 ^^^^ADC Interface Control & Status ^
 +| | |[8] |CRC_EN |RW |0x0 |Setting this bit will enable the CRC generation. |
 +|::: |::: |[7:0] |CUSTOM_CONTROL |RW |0x00 |{{page>:resources:fpga:docs:hdl:regmap_adc_custom}} |
 ^0x0015 ^0x0054 ^REG_CLK_FREQ ^^^^ADC Interface Control & Status ^ ^0x0015 ^0x0054 ^REG_CLK_FREQ ^^^^ADC Interface Control & Status ^
 | | |[31:0] |CLK_FREQ[31:0] |RO |0x0000 |Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock. | | | |[31:0] |CLK_FREQ[31:0] |RO |0x0000 |Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock. |
Line 64: Line 66:
 | | |[31:0] |CLK_RATIO[31:0] |RO |0x0000 |Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr). | | | |[31:0] |CLK_RATIO[31:0] |RO |0x0000 |Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr). |
 ^0x0017 ^0x005c ^REG_STATUS ^^^^ADC Interface Control & Status ^ ^0x0017 ^0x005c ^REG_STATUS ^^^^ADC Interface Control & Status ^
-| | |[3] |PN_ERR |RO |0x0 |If set, indicates pn error in one or more channels. |+| | |[4] |ADC_CTRL_STATUS |RO |0x0 |If set, indicates that the device'​s register data is available on the data bus. | 
 +|::: |::: |[3] |PN_ERR |RO |0x0 |If set, indicates pn error in one or more channels. |
 |::: |::: |[2] |PN_OOS |RO |0x0 |If set, indicates pn oos in one or more channels. | |::: |::: |[2] |PN_OOS |RO |0x0 |If set, indicates pn oos in one or more channels. |
 |::: |::: |[1] |OVER_RANGE |RO |0x0 |If set, indicates over range in one or more channels. | |::: |::: |[1] |OVER_RANGE |RO |0x0 |If set, indicates over range in one or more channels. |
Line 91: Line 94:
 ^0x001F ^0x007c ^REG_DRP_RDATA ^^^^ADC DRP Read Data ^ ^0x001F ^0x007c ^REG_DRP_RDATA ^^^^ADC DRP Read Data ^
 | | |[15:0] |DRP_RDATA[15:0] |RO |0x00 |DRP read data (does not include GTX lanes). | | | |[15:0] |DRP_RDATA[15:0] |RO |0x00 |DRP read data (does not include GTX lanes). |
 +^0x0020 ^0x0080 ^REG_ADC_CONFIG_WR ^^^^ADC Write Configuration ​Data ^
 +| | |[31:0] |ADC_CONFIG_WR[31:0] |RW |0x0000 |Custom ​Write to the available registers. |
 +^0x0021 ^0x0084 ^REG_ADC_CONFIG_RD ^^^^ADC Read Configuration ​Data ^
 +| | |[31:0] |ADC_CONFIG_RD[31:0] |RO |0x0000 |Custom read of the available registers. |
 ^0x0022 ^0x0088 ^REG_UI_STATUS ^^^^User Interface Status ^ ^0x0022 ^0x0088 ^REG_UI_STATUS ^^^^User Interface Status ^
 | | |[2] |UI_OVF |RW1C |0x0 |User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. | | | |[2] |UI_OVF |RW1C |0x0 |User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
 |::: |::: |[1] |UI_UNF |RW1C |0x0 |User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. | |::: |::: |[1] |UI_UNF |RW1C |0x0 |User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
 |::: |::: |[0] |UI_RESERVED |RW1C |0x0 |Reserved for backward compatibility. | |::: |::: |[0] |UI_RESERVED |RW1C |0x0 |Reserved for backward compatibility. |
 +^0x0023 ^0x008c ^REG_ADC_CONFIG_CTRL ^^^^ADC RD/WR configuration ^
 +| | |[31:0] |ADC_CONFIG_CTRL[31:​0] |RW |0x0000 |Control RD/WR requests to the device'​s register map: bit 1 - RD ('b1) , WR ('b0), bit 0 - enable WR/RD operation. |
 ^0x0028 ^0x00a0 ^REG_USR_CNTRL_1 ^^^^ADC Interface Control & Status ^ ^0x0028 ^0x00a0 ^REG_USR_CNTRL_1 ^^^^ADC Interface Control & Status ^
 | | |[7:0] |USR_CHANMAX[7:0] |RW |0x00 |This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules post data capture as another input to this common multiplexer. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). | | | |[7:0] |USR_CHANMAX[7:0] |RW |0x00 |This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules post data capture as another input to this common multiplexer. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
Line 107: Line 116:
 ^0x0031 ^0x00c4 ^REG_PPS_STATUS ^^^^PPS Status register ^ ^0x0031 ^0x00c4 ^REG_PPS_STATUS ^^^^PPS Status register ^
 | | |[0] |PPS_STATUS |RO |0x0 |If this bit is asserted there is no incomming 1PPS signal. Maybe the source is out of sync or it's not active. | | | |[0] |PPS_STATUS |RO |0x0 |If this bit is asserted there is no incomming 1PPS signal. Maybe the source is out of sync or it's not active. |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Fri Aug 11 18:29:53 2023 ^^^^^^
 ++++ ++++
- 
  
 ==== ADC Channel (axi_ad*) ==== ==== ADC Channel (axi_ad*) ====
Line 130: Line 138:
 |::: |::: |[0] |ENABLE |RW |0x0 |If set, enables channel. A 0x0 to 0x1 transition transfers all the control signals to the respective channel processing module. If a channel is part of a complex signal (I/Q), even channel is the master and the odd channel is the slave. Though a single control is used, both must be individually selected. | |::: |::: |[0] |ENABLE |RW |0x0 |If set, enables channel. A 0x0 to 0x1 transition transfers all the control signals to the respective channel processing module. If a channel is part of a complex signal (I/Q), even channel is the master and the odd channel is the slave. Though a single control is used, both must be individually selected. |
 ^0x0101 ^0x0404 ^REG_CHAN_STATUS ^^^^ADC Interface Control & Status ^ ^0x0101 ^0x0404 ^REG_CHAN_STATUS ^^^^ADC Interface Control & Status ^
-| | |[2] |PN_ERR |RW1C |0x0 |PN errors. If set, indicates spurious mismatches in sync state. This bit is cleared if OOS is set and is only indicates errors when OOS is cleared. |+| | |[12] |CRC_ERR |RW1C |0x0 |CRC errors. If set, indicates CRC error. Software must first clear this bit before initiating a transfer and monitor afterwards. | 
 +|::: |::: |[11:4] |STATUS_HEADER |RO |0x00 |The status header sent by the ADC.(compatible with AD7768/AD7768-4/AD777x). | 
 +|::: |::: |[2] |PN_ERR |RW1C |0x0 |PN errors. If set, indicates spurious mismatches in sync state. This bit is cleared if OOS is set and is only indicates errors when OOS is cleared. |
 |::: |::: |[1] |PN_OOS |RW1C |0x0 |PN Out Of Sync. If set, indicates an OOS status. OOS is set, if 64 consecutive patterns mismatch from the expected pattern. It is cleared, when 16 consecutive patterns match the expected pattern. | |::: |::: |[1] |PN_OOS |RW1C |0x0 |PN Out Of Sync. If set, indicates an OOS status. OOS is set, if 64 consecutive patterns mismatch from the expected pattern. It is cleared, when 16 consecutive patterns match the expected pattern. |
 |::: |::: |[0] |OVER_RANGE |RW1C |0x0 |If set, indicates over range. Note that over range is independent of the data path, it indicates an over range over a data transfer period. Software must first clear this bit before initiating a transfer and monitor afterwards. | |::: |::: |[0] |OVER_RANGE |RW1C |0x0 |If set, indicates over range. Note that over range is independent of the data path, it indicates an over range over a data transfer period. Software must first clear this bit before initiating a transfer and monitor afterwards. |
 +^0x0102 ^0x0408 ^REG_CHAN_RAW_DATA ^^^^ADC Raw Data Reading ^
 +| | |[31:0] |ADC_READ_DATA[31:0] |RO |0x0000 |Raw data read from the ADC. |
 ^0x0104 ^0x0410 ^REG_CHAN_CNTRL_1 ^^^^ADC Interface Control & Status ^ ^0x0104 ^0x0410 ^REG_CHAN_CNTRL_1 ^^^^ADC Interface Control & Status ^
 | | |[31:16] |DCFILT_OFFSET[15:0] |RW |0x0000 |DC removal (if equipped) offset. This is a 2's complement number added to the incoming data to remove a known DC offset. NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1). | | | |[31:16] |DCFILT_OFFSET[15:0] |RW |0x0000 |DC removal (if equipped) offset. This is a 2's complement number added to the incoming data to remove a known DC offset. NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1). |
Line 154: Line 166:
 ^0x0120 ^0x0480 ^REG_* ^^^^Channel 2, similar to register 0x100 to 0x10f. ^ ^0x0120 ^0x0480 ^REG_* ^^^^Channel 2, similar to register 0x100 to 0x10f. ^
 ^0x01F0 ^0x07c0 ^REG_* ^^^^Channel 15, similar to register 0x100 to 0x10f. ^ ^0x01F0 ^0x07c0 ^REG_* ^^^^Channel 15, similar to register 0x100 to 0x10f. ^
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 172: Line 184:
 ^0x0F ^0x003c ^REG_DELAY_CONTROL_F ^^^^Delay Control & Status ^ ^0x0F ^0x003c ^REG_DELAY_CONTROL_F ^^^^Delay Control & Status ^
 | | |[4:0] |DELAY_CONTROL_IO_F |RW |0x00 |Tap value for input/output delay primitive of the last interface line. In general the data and frame  lines are controlled with delay primitives, the number of registers of a controller is device specific. | | | |[4:0] |DELAY_CONTROL_IO_F |RW |0x00 |Tap value for input/output delay primitive of the last interface line. In general the data and frame  lines are controlled with delay primitives, the number of registers of a controller is device specific. |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 227: Line 239:
 ^0x001F ^0x007c ^REG_DRP_RDATA ^^^^DAC Interface Control & Status ^ ^0x001F ^0x007c ^REG_DRP_RDATA ^^^^DAC Interface Control & Status ^
 | | |[15:0] |DRP_RDATA |RO |0x0000 |DRP read data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). | | | |[15:0] |DRP_RDATA |RO |0x0000 |DRP read data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
 +^0x0020 ^0x0080 ^REG_DAC_CUSTOM_RD ^^^^DAC Read Configuration Data ^
 +| | |[31:0] |DAC_CUSTOM_RD[31:0] |RO |0x00000000 |Custom Read of the available registers. |
 +^0x0021 ^0x0084 ^REG_DAC_CUSTOM_WR ^^^^DAC Write Configuration Data ^
 +| | |[31:0] |DAC_CUSTOM_WR[31:0] |RW |0x00000000 |Custom Write of the available registers. |
 ^0x0022 ^0x0088 ^REG_UI_STATUS ^^^^User Interface Status ^ ^0x0022 ^0x0088 ^REG_UI_STATUS ^^^^User Interface Status ^
-| | |[1] |UI_OVF |RW1C |0x0 |User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |+| | |[4] |IF_BUSY |RO |0x0 |Interface busy. If set, indicates that the data interface is busy. | 
 +|::: |::: |[1] |UI_OVF |RW1C |0x0 |User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
 |::: |::: |[0] |UI_UNF |RW1C |0x0 |User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. | |::: |::: |[0] |UI_UNF |RW1C |0x0 |User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
 +^0x0023 ^0x008c ^REG_DAC_CUSTOM_CTRL ^^^^DAC Control Configuration Data ^
 +| | |[31:0] |DAC_CUSTOM_CTRL[31:0] |RW |0x00000000 |Custom Control of the available registers. |
 ^0x0028 ^0x00a0 ^REG_USR_CNTRL_1 ^^^^DAC User Control & Status ^ ^0x0028 ^0x00a0 ^REG_USR_CNTRL_1 ^^^^DAC User Control & Status ^
 | | |[7:0] |USR_CHANMAX[7:0] |RW |0x00 |This indicates the maximum number of inputs for the channel data multiplexers. User may add  different processing modules as inputs to the dac. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). | | | |[7:0] |USR_CHANMAX[7:0] |RW |0x00 |This indicates the maximum number of inputs for the channel data multiplexers. User may add  different processing modules as inputs to the dac. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
Line 236: Line 255:
 ^0x002F ^0x00bc ^REG_DAC_GPIO_OUT ^^^^DAC GPIO outputs ^ ^0x002F ^0x00bc ^REG_DAC_GPIO_OUT ^^^^DAC GPIO outputs ^
 | | |[31:0] |DAC_GPIO_OUT[31:0] |RW |0x00000000 |This controls auxiliary GPO pins of the DAC core NOT-APPLICABLE if GPIO_DISABLE is set (0x1). | | | |[31:0] |DAC_GPIO_OUT[31:0] |RW |0x00000000 |This controls auxiliary GPO pins of the DAC core NOT-APPLICABLE if GPIO_DISABLE is set (0x1). |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
 +
 +
  
  
Line 247: Line 268:
 |DWORD |BYTE |::: |::: |::: |::: |::: | |DWORD |BYTE |::: |::: |::: |::: |::: |
 ^0x0100 ^0x0400 ^REG_CHAN_CNTRL_1 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x0100 ^0x0400 ^REG_CHAN_CNTRL_1 ^^^^DAC Channel Control & Status (channel - 0) ^
-| | |[15:0] |DDS_SCALE_1[15:0] |RW |0x0000 |The DDS scale for tone 1. Defines the amplitude of the tone. The format is  1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on  16-bits, note that if you do use both channels and set both scale to 0x4000,  it is over-range. The final output is (channel_1_fullscale * scale_1) +  (channel_2 * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1). |+| | |[21:16] |DDS_PHASE_DW[5:0] |R |0x0000 |The DDS phase data width offers the HDL parameter configuration with the same name. This information is used in conjunction with REG_CHAN_CNTRL_9 and REG_CHAN_CNTRL_10. More info at https://wiki.analog.com/resources/fpga/docs/dds | 
 +|::: |::: |[15:0] |DDS_SCALE_1[15:0] |RW |0x0000 |The DDS scale for tone 1. Sets the amplitude of the tone. The format is 1.1.14  fixed point (signed, integer, fractional). The DDS in general runs on 16-bits,  note that if you do use both channels and set both scale to 0x4000, it is  over-range. The final output is (tone_1_fullscale * scale_1) (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
 ^0x0101 ^0x0404 ^REG_CHAN_CNTRL_2 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x0101 ^0x0404 ^REG_CHAN_CNTRL_2 ^^^^DAC Channel Control & Status (channel - 0) ^
-| | |[31:16] |DDS_INIT_1[15:0] |RW |0x0000 |The DDS phase initialization for tone 1. Defines the initial phase offset of  the tone. NOT-APPLICABLE if DDS_DISABLE is set (0x1). | +| | |[31:16] |DDS_INIT_1[15:0] |RW |0x0000 |The DDS phase initialization for tone 1. Sets the initial phase offset  of the tone. NOT-APPLICABLE if DDS_DISABLE is set (0x1). | 
-|::: |::: |[15:0] |DDS_INCR_1[15:0] |RW |0x0000 |Defines the resolution of the phase accumulator. Its value can be defined by  <m>INCR = (f_out * 2^16) * clkratio / f_if</m>; where f_out is the generated  output frequency, and f_if is the frequency of the digital interface, and  clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |+|::: |::: |[15:0] |DDS_INCR_1[15:0] |RW |0x0000 |Sets the frequency of the phase accumulator. Its value can be calculated  by <m>INCR = (f_out * 2^16) * clkratio / f_if</m>; where f_out is the  generated output frequency, and f_if is the frequency of the digital  interface, and clock_ratio is the ratio between the sampling clock and  the interface clock. If DDS_PHASE_DW is greater than 16(from REG_CHAN_CNTRL_1), the phase increment for tone 1 is extended in REG_CHAN_CNTRL_9. NOT-APPLICABLE  if DDS_DISABLE is set (0x1). |
 ^0x0102 ^0x0408 ^REG_CHAN_CNTRL_3 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x0102 ^0x0408 ^REG_CHAN_CNTRL_3 ^^^^DAC Channel Control & Status (channel - 0) ^
-| | |[15:0] |DDS_SCALE_2[15:0] |RW |0x0000 |The DDS scale for tone 1Defines the amplitude of the tone. The format is  1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on  16-bits, note that if you do use both channels and set both scale to 0x4000,  it is over-range. The final output is (channel_1_fullscale * scale_1) +  (channel_2 * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1). |+| | |[15:0] |DDS_SCALE_2[15:0] |RW |0x0000 |The DDS scale for tone 2Sets the amplitude of the tone. The format  is 1.1.14 fixed point (signed, integer, fractional).  The DDS in general runs on 16-bits, note that if you do use both  channels and set both scale to 0x4000, it is over-range. The final  output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2).  NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
 ^0x0103 ^0x040c ^REG_CHAN_CNTRL_4 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x0103 ^0x040c ^REG_CHAN_CNTRL_4 ^^^^DAC Channel Control & Status (channel - 0) ^
-| | |[31:16] |DDS_INIT_2[15:0] |RW |0x0000 |The DDS phase initialization for tone 1Defines the initial phase offset of  the tone. NOT-APPLICABLE if DDS_DISABLE is set (0x1). | +| | |[31:16] |DDS_INIT_2[15:0] |RW |0x0000 |The DDS phase initialization for tone 2Sets the initial phase offset of the  tone. If DDS_PHASE_DW is greater than 16(from REG_CHAN_CNTRL_1), the phase init  for tone 2 is extended in REG_CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is  set (0x1). | 
-|::: |::: |[15:0] |DDS_INCR_2[15:0] |RW |0x0000 |Defines the resolution of the phase accumulator. Its value can be defined by  <m>INCR = (f_out * 2^16) * clkratio / f_if</m>; where f_out is the generated  output frequency, and f_if is the frequency of the digital interface, and  clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |+|::: |::: |[15:0] |DDS_INCR_2[15:0] |RW |0x0000 |Sets the frequency of the phase accumulator. Its value can be calculated by  <m>INCR = (f_out * 2^16) * clkratio / f_if</m>; where f_out is the generated  output frequency, and f_if is the frequency of the digital interface, and  clock_ratio is the ratio between the sampling clock and the interface clock.  If DDS_PHASE_DW is greater than 16(from REG_CHAN_CNTRL_1), the phase increment  for tone 2 is extended in REG_CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is  set (0x1). |
 ^0x0104 ^0x0410 ^REG_CHAN_CNTRL_5 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x0104 ^0x0410 ^REG_CHAN_CNTRL_5 ^^^^DAC Channel Control & Status (channel - 0) ^
 | | |[31:16] |DDS_PATT_2[15:0] |RW |0x0000 |The DDS data pattern for this channel. | | | |[31:16] |DDS_PATT_2[15:0] |RW |0x0000 |The DDS data pattern for this channel. |
Line 275: Line 297:
 |::: |::: |[7:0] |USR_DATATYPE_BITS[7:0] |RW |0x00 |The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). | |::: |::: |[7:0] |USR_DATATYPE_BITS[7:0] |RW |0x00 |The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
 ^0x0109 ^0x0424 ^REG_USR_CNTRL_4 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x0109 ^0x0424 ^REG_USR_CNTRL_4 ^^^^DAC Channel Control & Status (channel - 0) ^
-| | |[31:16] |USR_INTERPOLATION_M[15:0] |RW |0x0000 |This holds the user interpolation M value of the channel that is currently being selected on  the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |+| | |[31:16] |USR_INTERPOLATION_M[15:0] |RW |0x0000 |This holds the user interpolation M value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the  form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
 |::: |::: |[15:0] |USR_INTERPOLATION_N[15:0] |RW |0x0000 |This holds the user interpolation N value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). | |::: |::: |[15:0] |USR_INTERPOLATION_N[15:0] |RW |0x0000 |This holds the user interpolation N value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
 ^0x010A ^0x0428 ^REG_USR_CNTRL_5 ^^^^DAC Channel Control & Status (channel - 0) ^ ^0x010A ^0x0428 ^REG_USR_CNTRL_5 ^^^^DAC Channel Control & Status (channel - 0) ^
 | | |[0] |DAC_IQ_MODE[0] |RW |0x0 |Enable complex mode. In this mode the driven data to the DAC must be a sequence  of I and Q sample pairs. | | | |[0] |DAC_IQ_MODE[0] |RW |0x0 |Enable complex mode. In this mode the driven data to the DAC must be a sequence  of I and Q sample pairs. |
-|::: |::: |[1] |DAC_IQ_SWAP[1] |RW |0x0 |Allows IQ swapping in complex mode. Only takes effect if complex mode is enabled. |+|::: |::: |[1] |DAC_IQ_SWAP[1] |RW |0x0 |Allows IQ swapping in complex mode. Only takes effect if complex mode  is enabled. | 
 +^0x010B ^0x042c ^REG_CHAN_CNTRL_9 ^^^^DAC Channel Control & Status (channel - 0) ^ 
 +| | |[31:16] |DDS_INIT_1_EXTENDED[15:0] |RW |0x0000 |The extended DDS phase initialization for tone 1. Sets the initial phase offset  of the tone. The extended init(phase) value should be calculated according to  DDS_PHASE_DW value from REG_CHAN_CNTRL_1 NOT-APPLICABLE if DDS_DISABLE is  set (0x1). | 
 +|::: |::: |[15:0] |DDS_INCR_1_EXTENDED[15:0] |RW |0x0000 |Sets the frequency of tone 1's phase accumulator. Its value can be calculated  by <m>INCR = (f_out * 2^phaseDW) * clkratio / f_if</m>; Where f_out is the  generated output frequency, DDS_PHASE_DW value can be found in REG_CHAN_CNTRL_1 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface,  and clock_ratio is the ratio between the sampling clock and the interface clock.  NOT-APPLICABLE if DDS_DISABLE is set (0x1). | 
 +^0x010C ^0x0430 ^REG_CHAN_CNTRL_10 ^^^^DAC Channel Control & Status (channel - 0) ^ 
 +| | |[31:16] |DDS_INIT_2_EXTENDED[15:0] |RW |0x0000 |The extended DDS phase initialization for tone 2. Sets the initial phase offset  of the tone. The extended init(phase)  value should be calculated according to  DDS_PHASE_DW value from REG_CHAN_CNTRL_2 NOT-APPLICABLE if DDS_DISABLE is  set (0x1). | 
 +|::: |::: |[15:0] |DDS_INCR_2_EXTENDED[15:0] |RW |0x0000 |Sets the frequency of tone 2's phase accumulator. Its value can be calculated  by <m>INCR = (f_out * 2^phaseDW) * clkratio / f_if</m>; Where f_out is the  generated output frequency, DDS_PHASE_DW value can be found in REG_CHAN_CNTRL_2  in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface,  and clock_ratio is the ratio between the sampling clock and the interface clock.  NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
 ^0x0110 ^0x0440 ^REG_* ^^^^Channel 1, similar to registers 0x100 to 0x10f. ^ ^0x0110 ^0x0440 ^REG_* ^^^^Channel 1, similar to registers 0x100 to 0x10f. ^
 ^0x0120 ^0x0480 ^REG_* ^^^^Channel 2, similar to registers 0x100 to 0x10f. ^ ^0x0120 ^0x0480 ^REG_* ^^^^Channel 2, similar to registers 0x100 to 0x10f. ^
 ^0x01F0 ^0x07c0 ^REG_* ^^^^Channel 15, similar to registers 0x100 to 0x10f. ^ ^0x01F0 ^0x07c0 ^REG_* ^^^^Channel 15, similar to registers 0x100 to 0x10f. ^
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Fri Sep  8 16:01:53 2023 ^^^^^^ 
 +++++ 
 + 
 + 
 +==== Generic TDD Control (axi_tdd) ==== 
 + 
 +++++ Click to expand regmap | 
 +|< 100% 5% 5% 5% 25% 5% 5% 50% >| 
 +|Address ||Bits |Name |Type |Default |Description | 
 +|DWORD |BYTE |::: |::: |::: |::: |::: | 
 +^0x0000 ^0x0000 ^VERSION ^^^^Version of the peripheral. Follows semantic versioning. Current version 2.00.61. ^ 
 +| | |[31:16] |VERSION_MAJOR |R |0x0002 | | 
 +|::: |::: |[15:8] |VERSION_MINOR |R |0x00 | | 
 +|::: |::: |[7:0] |VERSION_PATCH |R |0x61 | | 
 +^0x0001 ^0x0004 ^PERIPHERAL_ID ^^^^ ^ 
 +| | |[31:0] |PERIPHERAL_ID |R |''ID'' |Value of the ID configuration parameter. | 
 +^0x0002 ^0x0008 ^SCRATCH ^^^^ ^ 
 +| | |[31:0] |SCRATCH |RW |0x00000000 |Scratch register useful for debug. | 
 +^0x0003 ^0x000c ^IDENTIFICATION ^^^^ ^ 
 +| | |[31:0] |IDENTIFICATION |R |0x5444444E |Peripheral identification ('T', 'D', 'D', 'N'). | 
 +^0x0004 ^0x0010 ^INTERFACE_DESCRIPTION ^^^^ ^ 
 +| | |[30:24] |SYNC_COUNT_WIDTH |R |''SYNC_COUNT_WIDTH'' |Width of internal synchronization counter | 
 +|::: |::: |[21:16] |BURST_COUNT_WIDTH |R |''BURST_COUNT_WIDTH'' |Width of burst counter | 
 +|::: |::: |[13:8] |REGISTER_WIDTH |R |''REGISTER_WIDTH'' |Width of internal reference counter and timing registers | 
 +|::: |::: |[7] |SYNC_EXTERNAL_CDC |R |''SYNC_EXTERNAL_CDC'' |Enable CDC for external synchronization pulse | 
 +|::: |::: |[6] |SYNC_EXTERNAL |R |''SYNC_EXTERNAL'' |Enable external synchronization support | 
 +|::: |::: |[5] |SYNC_INTERNAL |R |''SYNC_INTERNAL'' |Enable internal synchronization support | 
 +|::: |::: |[4:0] |CHANNEL_COUNT_EXTRA |R |''CHANNEL_COUNT''-1 |Number of channels starting from CH1, excluding CH0 | 
 +^0x0005 ^0x0014 ^DEFAULT_POLARITY ^^^^ ^ 
 +| | |[31:0] |DEFAULT_POLARITY |R |''DEFAULT_POLARITY'' |Default polarity per every channel - LSB corresponds to CH0, MSB to CH31 | 
 +^0x0010 ^0x0040 ^CONTROL ^^^^TDD Control ^ 
 +| | |[4] |SYNC_SOFT |RW |0x0 |Trigger the TDD core through a register write. This bit self clears. | 
 +|::: |::: |[3] |SYNC_EXT |RW |0x0 |Enable external sync trigger. This bit is implemented if ''SYNC_EXTERNAL'' is set. | 
 +|::: |::: |[2] |SYNC_INT |RW |0x0 |Enable internal sync trigger. This bit is implemented if ''SYNC_INTERNAL'' is set. | 
 +|::: |::: |[1] |SYNC_RST |RW |0x0 |Reset the internal counter while running when receiving a sync event | 
 +|::: |::: |[0] |ENABLE |RW |0x0 |Module enable | 
 +^0x0011 ^0x0044 ^CHANNEL_ENABLE ^^^^TDD Channel Enable ^ 
 +| | |[31:0] |CHANNEL_ENABLE |RW |0x00000000 |Enable bits per channel - LSB corresponds to CH0, MSB to CH31 | 
 +^0x0012 ^0x0048 ^CHANNEL_POLARITY ^^^^TDD Channel Polarity ^ 
 +| | |[31:0] |CHANNEL_POLARITY |RW |0x00000000 |Polarity bits per channel - LSB corresponds to CH0, MSB to CH31 | 
 +^0x0013 ^0x004c ^BURST_COUNT ^^^^TDD Number of frames per burst ^ 
 +| | |[31:0] |BURST_COUNT |RW |0x00000000 |If set to 0x0 and enabled - the controller operates in TDD mode as long as the ENABLE bit is set. If set to a non-zero value, the controller operates for the set number of frames and then stops. | 
 +^0x0014 ^0x0050 ^STARTUP_DELAY ^^^^TDD Transmission startup delay ^ 
 +| | |[31:0] |STARTUP_DELAY |RW |0x00000000 |The initial delay value before the beginning of the first frame; defined in clock cycles. | 
 +^0x0015 ^0x0054 ^FRAME_LENGTH ^^^^TDD Frame length ^ 
 +| | |[31:0] |FRAME_LENGTH |RW |0x00000000 |The length of the transmission frame; defined in clock cycles. | 
 +^0x0016 ^0x0058 ^SYNC_COUNTER_LOW ^^^^TDD Sync counter ^ 
 +| | |[31:0] |SYNC_COUNTER_LOW |RW |0x00000000 |The LSB slice of the offset (from sync counter equal zero) when an internal sync pulse is generated. This register is implemented if ''SYNC_COUNT_WIDTH''>0. | 
 +^0x0017 ^0x005c ^SYNC_COUNTER_HIGH ^^^^TDD Sync counter ^ 
 +| | |[31:0] |SYNC_COUNTER_HIGH |RW |0x00000000 |The MSB slice of the offset (from sync counter equal zero) when an internal sync pulse is generated. This register is implemented if ''SYNC_COUNT_WIDTH''>32. | 
 +^0x0018 ^0x0060 ^STATUS ^^^^Peripheral Status ^ 
 +| | |[1:0] |STATE |R |0x0 |The current state of the peripheral FSM; used for debugging purposes. | 
 +^0x0020 ^0x0080 ^CH0_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH0_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH0 is set. | 
 +^0x0021 ^0x0084 ^CH0_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH0_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH0 is reset. | 
 +^0x0022 ^0x0088 ^CH1_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH1_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH1 is set. This register is implemented if ''CHANNEL_COUNT''>1. | 
 +^0x0023 ^0x008c ^CH1_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH1_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH1 is reset. This register is implemented if ''CHANNEL_COUNT''>1. | 
 +^0x0024 ^0x0090 ^CH2_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH2_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH2 is set. This register is implemented if ''CHANNEL_COUNT''>2. | 
 +^0x0025 ^0x0094 ^CH2_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH2_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH2 is reset. This register is implemented if ''CHANNEL_COUNT''>2. | 
 +^0x0026 ^0x0098 ^CH3_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH3_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH3 is set. This register is implemented if ''CHANNEL_COUNT''>3. | 
 +^0x0027 ^0x009c ^CH3_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH3_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH3 is reset. This register is implemented if ''CHANNEL_COUNT''>3. | 
 +^0x0028 ^0x00a0 ^CH4_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH4_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH4 is set. This register is implemented if ''CHANNEL_COUNT''>4. | 
 +^0x0029 ^0x00a4 ^CH4_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH4_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH4 is reset. This register is implemented if ''CHANNEL_COUNT''>4. | 
 +^0x002A ^0x00a8 ^CH5_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH5_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH5 is set. This register is implemented if ''CHANNEL_COUNT''>5. | 
 +^0x002B ^0x00ac ^CH5_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH5_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH5 is reset. This register is implemented if ''CHANNEL_COUNT''>5. | 
 +^0x002C ^0x00b0 ^CH6_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH6_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH6 is set. This register is implemented if ''CHANNEL_COUNT''>6. | 
 +^0x002D ^0x00b4 ^CH6_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH6_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH6 is reset. This register is implemented if ''CHANNEL_COUNT''>6. | 
 +^0x002E ^0x00b8 ^CH7_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH7_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH7 is set. This register is implemented if ''CHANNEL_COUNT''>7. | 
 +^0x002F ^0x00bc ^CH7_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH7_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH7 is reset. This register is implemented if ''CHANNEL_COUNT''>7. | 
 +^0x0030 ^0x00c0 ^CH8_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH8_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH8 is set. This register is implemented if ''CHANNEL_COUNT''>8. | 
 +^0x0031 ^0x00c4 ^CH8_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH8_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH8 is reset. This register is implemented if ''CHANNEL_COUNT''>8. | 
 +^0x0032 ^0x00c8 ^CH9_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH9_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH9 is set. This register is implemented if ''CHANNEL_COUNT''>9. | 
 +^0x0033 ^0x00cc ^CH9_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH9_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH9 is reset. This register is implemented if ''CHANNEL_COUNT''>9. | 
 +^0x0034 ^0x00d0 ^CH10_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH10_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH10 is set. This register is implemented if ''CHANNEL_COUNT''>10. | 
 +^0x0035 ^0x00d4 ^CH10_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH10_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH10 is reset. This register is implemented if ''CHANNEL_COUNT''>10. | 
 +^0x0036 ^0x00d8 ^CH11_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH11_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH11 is set. This register is implemented if ''CHANNEL_COUNT''>11. | 
 +^0x0037 ^0x00dc ^CH11_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH11_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH11 is reset. This register is implemented if ''CHANNEL_COUNT''>11. | 
 +^0x0038 ^0x00e0 ^CH12_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH12_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH12 is set. This register is implemented if ''CHANNEL_COUNT''>12. | 
 +^0x0039 ^0x00e4 ^CH12_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH12_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH12 is reset. This register is implemented if ''CHANNEL_COUNT''>12. | 
 +^0x003A ^0x00e8 ^CH13_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH13_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH13 is set. This register is implemented if ''CHANNEL_COUNT''>13. | 
 +^0x003B ^0x00ec ^CH13_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH13_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH13 is reset. This register is implemented if ''CHANNEL_COUNT''>13. | 
 +^0x003C ^0x00f0 ^CH14_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH14_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH14 is set. This register is implemented if ''CHANNEL_COUNT''>14. | 
 +^0x003D ^0x00f4 ^CH14_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH14_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH14 is reset. This register is implemented if ''CHANNEL_COUNT''>14. | 
 +^0x003E ^0x00f8 ^CH15_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH15_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH15 is set. This register is implemented if ''CHANNEL_COUNT''>15. | 
 +^0x003F ^0x00fc ^CH15_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH15_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH15 is reset. This register is implemented if ''CHANNEL_COUNT''>15. | 
 +^0x0040 ^0x0100 ^CH16_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH16_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH16 is set. This register is implemented if ''CHANNEL_COUNT''>16. | 
 +^0x0041 ^0x0104 ^CH16_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH16_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH16 is reset. This register is implemented if ''CHANNEL_COUNT''>16. | 
 +^0x0042 ^0x0108 ^CH17_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH17_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH17 is set. This register is implemented if ''CHANNEL_COUNT''>17. | 
 +^0x0043 ^0x010c ^CH17_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH17_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH17 is reset. This register is implemented if ''CHANNEL_COUNT''>17. | 
 +^0x0044 ^0x0110 ^CH18_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH18_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH18 is set. This register is implemented if ''CHANNEL_COUNT''>18. | 
 +^0x0045 ^0x0114 ^CH18_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH18_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH18 is reset. This register is implemented if ''CHANNEL_COUNT''>18. | 
 +^0x0046 ^0x0118 ^CH19_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH19_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH19 is set. This register is implemented if ''CHANNEL_COUNT''>19. | 
 +^0x0047 ^0x011c ^CH19_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH19_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH19 is reset. This register is implemented if ''CHANNEL_COUNT''>19. | 
 +^0x0048 ^0x0120 ^CH20_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH20_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH20 is set. This register is implemented if ''CHANNEL_COUNT''>20. | 
 +^0x0049 ^0x0124 ^CH20_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH20_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH20 is reset. This register is implemented if ''CHANNEL_COUNT''>20. | 
 +^0x004A ^0x0128 ^CH21_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH21_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH21 is set. This register is implemented if ''CHANNEL_COUNT''>21. | 
 +^0x004B ^0x012c ^CH21_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH21_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH21 is reset. This register is implemented if ''CHANNEL_COUNT''>21. | 
 +^0x004C ^0x0130 ^CH22_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH22_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH22 is set. This register is implemented if ''CHANNEL_COUNT''>22. | 
 +^0x004D ^0x0134 ^CH22_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH22_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH22 is reset. This register is implemented if ''CHANNEL_COUNT''>22. | 
 +^0x004E ^0x0138 ^CH23_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH23_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH23 is set. This register is implemented if ''CHANNEL_COUNT''>23. | 
 +^0x004F ^0x013c ^CH23_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH23_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH23 is reset. This register is implemented if ''CHANNEL_COUNT''>23. | 
 +^0x0050 ^0x0140 ^CH24_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH24_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH24 is set. This register is implemented if ''CHANNEL_COUNT''>24. | 
 +^0x0051 ^0x0144 ^CH24_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH24_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH24 is reset. This register is implemented if ''CHANNEL_COUNT''>24. | 
 +^0x0052 ^0x0148 ^CH25_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH25_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH25 is set. This register is implemented if ''CHANNEL_COUNT''>25. | 
 +^0x0053 ^0x014c ^CH25_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH25_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH25 is reset. This register is implemented if ''CHANNEL_COUNT''>25. | 
 +^0x0054 ^0x0150 ^CH26_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH26_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH26 is set. This register is implemented if ''CHANNEL_COUNT''>26. | 
 +^0x0055 ^0x0154 ^CH26_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH26_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH26 is reset. This register is implemented if ''CHANNEL_COUNT''>26. | 
 +^0x0056 ^0x0158 ^CH27_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH27_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH27 is set. This register is implemented if ''CHANNEL_COUNT''>27. | 
 +^0x0057 ^0x015c ^CH27_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH27_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH27 is reset. This register is implemented if ''CHANNEL_COUNT''>27. | 
 +^0x0058 ^0x0160 ^CH28_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH28_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH28 is set. This register is implemented if ''CHANNEL_COUNT''>28. | 
 +^0x0059 ^0x0164 ^CH28_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH28_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH28 is reset. This register is implemented if ''CHANNEL_COUNT''>28. | 
 +^0x005A ^0x0168 ^CH29_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH29_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH29 is set. This register is implemented if ''CHANNEL_COUNT''>29. | 
 +^0x005B ^0x016c ^CH29_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH29_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH29 is reset. This register is implemented if ''CHANNEL_COUNT''>29. | 
 +^0x005C ^0x0170 ^CH30_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH30_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH30 is set. This register is implemented if ''CHANNEL_COUNT''>30. | 
 +^0x005D ^0x0174 ^CH30_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH30_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH30 is reset. This register is implemented if ''CHANNEL_COUNT''>30. | 
 +^0x005E ^0x0178 ^CH31_ON ^^^^Channel Set ^ 
 +| | |[31:0] |CH31_ON |RW |0x00000000 |The offset (from frame count equal zero), when CH31 is set. This register is implemented if ''CHANNEL_COUNT''>31. | 
 +^0x005F ^0x017c ^CH31_OFF ^^^^Channel Reset ^ 
 +| | |[31:0] |CH31_OFF |RW |0x00000000 |The offset (from frame count equal zero), when CH31 is reset. This register is implemented if ''CHANNEL_COUNT''>31. | 
 +^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 359: Line 567:
 ^0x003B ^0x00ec ^REG_TDD_TX_DP_OFF_2 ^^^^TDD Control & Status ^ ^0x003B ^0x00ec ^REG_TDD_TX_DP_OFF_2 ^^^^TDD Control & Status ^
 | | |[23:0] |TDD_TX_DP_OFF_2 |RW |0x000000 |The secondary pointer for TX_DP_OFF. | | | |[23:0] |TDD_TX_DP_OFF_2 |RW |0x000000 |The secondary pointer for TX_DP_OFF. |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 383: Line 591:
 ^0x00092 ^0x0248 ^REG_* ^^^^Profile 1, similar to registers 0x00010 to 0x00011. ^ ^0x00092 ^0x0248 ^REG_* ^^^^Profile 1, similar to registers 0x00010 to 0x00011. ^
 ^0x00094 ^0x0250 ^REG_* ^^^^Profile 2, similar to registers 0x00010 to 0x00011. ^ ^0x00094 ^0x0250 ^REG_* ^^^^Profile 2, similar to registers 0x00010 to 0x00011. ^
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 492: Line 700:
 ^0xc1 + 0x08*n ^0x0304 +0x20*n ^LANEn_LATENCY ^^^^ ^ ^0xc1 + 0x08*n ^0x0304 +0x20*n ^LANEn_LATENCY ^^^^ ^
 | | |[31:14] |Reserved |RO |0x0 | | | | |[31:14] |Reserved |RO |0x0 | |
-|::: |::: |[13:0] |LATENCY |RO-V |0x0 |Lane latency in octets. |+|::: |::: |[13:0] |LATENCY |RO-V |0x0 |For 8b10b mode: represents the lane latency in octets; For 64b66b mode: represents the delay from the received EOEMB indicator to the next (SYSREF aligned) LEMC edge in octets. In other words, this amount of data is stored in the elastic buffer before it gets released on the LEMC edge. Must be greater than 64. Its max value is KxF octets.  Where LEMC period = KxF/8 link clock periods. |
 ^0xc2 + 0x08*n ^0x0308 +0x20*n ^LANEn_ERROR_STATISTICS ^^^^ ^ ^0xc2 + 0x08*n ^0x0308 +0x20*n ^LANEn_ERROR_STATISTICS ^^^^ ^
 | | |[31:0] |ERROR_REGISTER |RO |0x0 |This register shows the number of total errors for this lane. Errors counted depend on the configuration in LINK_CONF3. It must always be manually reset. | | | |[31:0] |ERROR_REGISTER |RO |0x0 |This register shows the number of total errors for this lane. Errors counted depend on the configuration in LINK_CONF3. It must always be manually reset. |
Line 504: Line 712:
 ^0xc5 + 0x08*n ^0x0314 +0x20*n ^LANEn_ILAS1 ^^^^Received ILAS config data for the n-th lane. ^ ^0xc5 + 0x08*n ^0x0314 +0x20*n ^LANEn_ILAS1 ^^^^Received ILAS config data for the n-th lane. ^
 | | |[31:29] |Reserved |RO |0x00 | | | | |[31:29] |Reserved |RO |0x00 | |
-|::: |::: |[28:24] |K |RO |0x00 |K (Frames per multi-frame) field of the ILAS config sequence. | +|::: |::: |[28:24] |K |RO |0x00 |K (Frames per multi-frame) field of the ILAS config sequence - 1. | 
-|::: |::: |[23:16] |F |RO |0x00 |F (Octets per frame) field of the ILAS config sequence. |+|::: |::: |[23:16] |F |RO |0x00 |F (Octets per frame) field of the ILAS config sequence - 1. |
 |::: |::: |[15] |SCR |RO |0x0 |SCR (Scrambling enabled) field of the ILAS config sequence. | |::: |::: |[15] |SCR |RO |0x0 |SCR (Scrambling enabled) field of the ILAS config sequence. |
 |::: |::: |[14:13] |Reserved |RO |0x0 | | |::: |::: |[14:13] |Reserved |RO |0x0 | |
-|::: |::: |[12:8] |L |RO |0x00 |L (Number of lanes) field of the ILAS config sequence. |+|::: |::: |[12:8] |L |RO |0x00 |L (Number of lanes) field of the ILAS config sequence - 1. |
 |::: |::: |[7:5] |Reserved |RO |0x0 | | |::: |::: |[7:5] |Reserved |RO |0x0 | |
 |::: |::: |[4:0] |LID |RO |0x00 |LID (Lane ID) field of the ILAS config sequence. | |::: |::: |[4:0] |LID |RO |0x00 |LID (Lane ID) field of the ILAS config sequence. |
 ^0xc6 + 0x08*n ^0x0318 +0x20*n ^LANEn_ILAS2 ^^^^Received ILAS config data for the n-th lane. ^ ^0xc6 + 0x08*n ^0x0318 +0x20*n ^LANEn_ILAS2 ^^^^Received ILAS config data for the n-th lane. ^
 | | |[31:29] |JESDV |RO |0x0 |JESDV (JESD204 version) field of the ILAS config sequence. | | | |[31:29] |JESDV |RO |0x0 |JESDV (JESD204 version) field of the ILAS config sequence. |
-|::: |::: |[28:24] |S |RO |0x00 |S (Samples per frame) field of the ILAS config sequence. |+|::: |::: |[28:24] |S |RO |0x00 |S (Samples per frame) field of the ILAS config sequence - 1. |
 |::: |::: |[23:21] |SUBCLASSV |RO |0x0 |SUBCLASSV (JESD204B subclass) field of the ILAS config sequence. | |::: |::: |[23:21] |SUBCLASSV |RO |0x0 |SUBCLASSV (JESD204B subclass) field of the ILAS config sequence. |
-|::: |::: |[20:16] |NP |RO |0x00 |N' (Total number of bits per sample) field of the ILAS config sequence. |+|::: |::: |[20:16] |NP |RO |0x00 |N' (Total number of bits per sample) field of the ILAS config sequence - 1. |
 |::: |::: |[15:14] |CS |RO |0x0 |CS (Control bits per sample) field of the ILAS config sequence. | |::: |::: |[15:14] |CS |RO |0x0 |CS (Control bits per sample) field of the ILAS config sequence. |
 |::: |::: |[13] |Reserved |RO |0x0 | | |::: |::: |[13] |Reserved |RO |0x0 | |
-|::: |::: |[12:8] |N |RO |0x00 |N (Converter resolution) field of the ILAS config sequence. | +|::: |::: |[12:8] |N |RO |0x00 |N (Converter resolution) field of the ILAS config sequence - 1. | 
-|::: |::: |[7:0] |M |RO |0x00 |M (Number of converters) field of the ILAS config sequence. |+|::: |::: |[7:0] |M |RO |0x00 |M (Number of converters) field of the ILAS config sequence - 1. |
 ^0xc7 + 0x08*n ^0x031c +0x20*n ^LANEn_ILAS3 ^^^^Received ILAS config data for the n-th lane. ^ ^0xc7 + 0x08*n ^0x031c +0x20*n ^LANEn_ILAS3 ^^^^Received ILAS config data for the n-th lane. ^
 | | |[31:24] |FCHK |RO |0x00 |FCHK (Checksum) field of the ILAS config sequence. | | | |[31:24] |FCHK |RO |0x00 |FCHK (Checksum) field of the ILAS config sequence. |
Line 526: Line 734:
 |::: |::: |[6:5] |Reserved |RO |0x0 | | |::: |::: |[6:5] |Reserved |RO |0x0 | |
 |::: |::: |[4:0] |CF |RO |0x00 |CF (control words per frame) field of the ILAS config sequence | |::: |::: |[4:0] |CF |RO |0x00 |CF (control words per frame) field of the ILAS config sequence |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 625: Line 833:
 ^0xc5 + 0x08*n ^0x0314 +0x20*n ^LANEn_ILAS1 ^^^^ILAS config data for the n-th lane. Valid for 8B/10B link. ^ ^0xc5 + 0x08*n ^0x0314 +0x20*n ^LANEn_ILAS1 ^^^^ILAS config data for the n-th lane. Valid for 8B/10B link. ^
 | | |[31:29] |Reserved |RO |0x00 | | | | |[31:29] |Reserved |RO |0x00 | |
-|::: |::: |[28:24] |K |RW |0x00 |K (Frames per multi-frame) field of the ILAS config sequence. | +|::: |::: |[28:24] |K |RW |0x00 |K (Frames per multi-frame) field of the ILAS config sequence - 1. | 
-|::: |::: |[23:16] |F |RW |0x00 |F (Octets per frame) field of the ILAS config sequence. |+|::: |::: |[23:16] |F |RW |0x00 |F (Octets per frame) field of the ILAS config sequence - 1. |
 |::: |::: |[15] |SCR |RW |0x0 |SCR (Scrambling enabled) field of the ILAS config sequence. | |::: |::: |[15] |SCR |RW |0x0 |SCR (Scrambling enabled) field of the ILAS config sequence. |
 |::: |::: |[14:13] |Reserved |RO |0x0 | | |::: |::: |[14:13] |Reserved |RO |0x0 | |
-|::: |::: |[12:8] |L |RW |0x00 |L (Number of lanes) field of the ILAS config sequence. |+|::: |::: |[12:8] |L |RW |0x00 |L (Number of lanes) field of the ILAS config sequence - 1. |
 |::: |::: |[7:5] |Reserved |RO |0x0 | | |::: |::: |[7:5] |Reserved |RO |0x0 | |
 |::: |::: |[4:0] |LID |RW |0x00 |LID (Lane ID) field of the ILAS config sequence. | |::: |::: |[4:0] |LID |RW |0x00 |LID (Lane ID) field of the ILAS config sequence. |
 ^0xc6 + 0x08*n ^0x0318 +0x20*n ^LANEn_ILAS2 ^^^^ILAS config data for the n-th lane. Valid for 8B/10B link. ^ ^0xc6 + 0x08*n ^0x0318 +0x20*n ^LANEn_ILAS2 ^^^^ILAS config data for the n-th lane. Valid for 8B/10B link. ^
 | | |[31:29] |JESDV |RW |0x0 |JESDV (JESD204 version) field of the ILAS config sequence. | | | |[31:29] |JESDV |RW |0x0 |JESDV (JESD204 version) field of the ILAS config sequence. |
-|::: |::: |[28:24] |S |RW |0x00 |S (Samples per frame) field of the ILAS config sequence. |+|::: |::: |[28:24] |S |RW |0x00 |S (Samples per frame) field of the ILAS config sequence - 1. |
 |::: |::: |[23:21] |SUBCLASSV |RW |0x0 |SUBCLASSV (JESD204B subclass) field of the ILAS config sequence. | |::: |::: |[23:21] |SUBCLASSV |RW |0x0 |SUBCLASSV (JESD204B subclass) field of the ILAS config sequence. |
-|::: |::: |[20:16] |NP |RW |0x00 |N' (Total number of bits per sample) field of the ILAS config sequence. |+|::: |::: |[20:16] |NP |RW |0x00 |N' (Total number of bits per sample) field of the ILAS config sequence - 1. |
 |::: |::: |[15:14] |CS |RW |0x0 |CS (Control bits per sample) field of the ILAS config sequence. | |::: |::: |[15:14] |CS |RW |0x0 |CS (Control bits per sample) field of the ILAS config sequence. |
 |::: |::: |[13] |Reserved |RO |0x0 | | |::: |::: |[13] |Reserved |RO |0x0 | |
-|::: |::: |[12:8] |N |RW |0x00 |N (Converter resolution) field of the ILAS config sequence. | +|::: |::: |[12:8] |N |RW |0x00 |N (Converter resolution) field of the ILAS config sequence - 1. | 
-|::: |::: |[7:0] |M |RW |0x00 |M (Number of converters) field of the ILAS config sequence. |+|::: |::: |[7:0] |M |RW |0x00 |M (Number of converters) field of the ILAS config sequence - 1. |
 ^0xc7 + 0x08*n ^0x031c +0x20*n ^LANEn_ILAS3 ^^^^ILAS config data for the n-th lane. Valid for 8B/10B link. ^ ^0xc7 + 0x08*n ^0x031c +0x20*n ^LANEn_ILAS3 ^^^^ILAS config data for the n-th lane. Valid for 8B/10B link. ^
 | | |[31:24] |FCHK |RW |0x00 |FCHK (Checksum) field of the ILAS config sequence. | | | |[31:24] |FCHK |RW |0x00 |FCHK (Checksum) field of the ILAS config sequence. |
Line 647: Line 855:
 |::: |::: |[6:5] |Reserved |RO |0x0 | | |::: |::: |[6:5] |Reserved |RO |0x0 | |
 |::: |::: |[4:0] |CF |RO |0x00 |CF (control words per frame) field of the ILAS config sequence | |::: |::: |[4:0] |CF |RO |0x00 |CF (control words per frame) field of the ILAS config sequence |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 657: Line 865:
 |Address ||Bits |Name |Type |Default |Description | |Address ||Bits |Name |Type |Default |Description |
 |DWORD |BYTE |::: |::: |::: |::: |::: | |DWORD |BYTE |::: |::: |::: |::: |::: |
-^0x000 ^0x0000 ^VERSION ^^^^Version of the peripheral. Follows semantic versioning. Current version 4.03.61. ^+^0x000 ^0x0000 ^VERSION ^^^^Version of the peripheral. Follows semantic versioning. Current version 4.05.61. ^
 | | |[31:16] |VERSION_MAJOR |RO |0x04 | | | | |[31:16] |VERSION_MAJOR |RO |0x04 | |
-|::: |::: |[15:8] |VERSION_MINOR |RO |0x03 | |+|::: |::: |[15:8] |VERSION_MINOR |RO |0x05 | |
 |::: |::: |[7:0] |VERSION_PATCH |RO |0x61 | | |::: |::: |[7:0] |VERSION_PATCH |RO |0x61 | |
 ^0x001 ^0x0004 ^PERIPHERAL_ID ^^^^ ^ ^0x001 ^0x0004 ^PERIPHERAL_ID ^^^^ ^
Line 672: Line 880:
 |::: |::: |[11:8] |BYTES_PER_BEAT_SRC_LOG2 |R |log2(''DMA_DATA_WIDTH_SRC''/8) |Width of data bus on source interface. Log2 of interface data widths in bytes. | |::: |::: |[11:8] |BYTES_PER_BEAT_SRC_LOG2 |R |log2(''DMA_DATA_WIDTH_SRC''/8) |Width of data bus on source interface. Log2 of interface data widths in bytes. |
 |::: |::: |[13:12] |DMA_TYPE_SRC |R |''DMA_TYPE_SRC'' |Value of ''DMA_TYPE_SRC'' parameter.(0 - AXI MemoryMap, 1 -  AXI Stream, 2 - FIFO | |::: |::: |[13:12] |DMA_TYPE_SRC |R |''DMA_TYPE_SRC'' |Value of ''DMA_TYPE_SRC'' parameter.(0 - AXI MemoryMap, 1 -  AXI Stream, 2 - FIFO |
 +|::: |::: |[19:16] |BYTES_PER_BURST_WIDTH |R |''BYTES_PER_BURST_WIDTH'' |Value of ''BYTES_PER_BURST_WIDTH'' interface parameter. Log2 of the real ''MAX_BYTES_PER_BURST''. The starting address of the transfer must be aligned with ''MAX_BYTES_PER_BURST'' to avoid crossing the 4kB address boundary. |
 ^0x020 ^0x0080 ^IRQ_MASK ^^^^ ^ ^0x020 ^0x0080 ^IRQ_MASK ^^^^ ^
 | | |[1] |TRANSFER_COMPLETED |RW |0x1 |Masks the TRANSFER_COMPLETED IRQ. | | | |[1] |TRANSFER_COMPLETED |RW |0x1 |Masks the TRANSFER_COMPLETED IRQ. |
Line 682: Line 891:
 |::: |::: |[0] |TRANSFER_QUEUED |RO |0x0 |This bit will be asserted if a transfer has been queued and it is possible to queue the next transfer. Cleared together with the corresponding IRQ_PENDING bit. | |::: |::: |[0] |TRANSFER_QUEUED |RO |0x0 |This bit will be asserted if a transfer has been queued and it is possible to queue the next transfer. Cleared together with the corresponding IRQ_PENDING bit. |
 ^0x100 ^0x0400 ^CONTROL ^^^^ ^ ^0x100 ^0x0400 ^CONTROL ^^^^ ^
-| | |[1] |PAUSE |RW |0x0 |When set to 1 the currently active transfer is paused. It will be resumed once the bit is cleared again. |+| | |[2] |HWDESC |RW |0x0 |When set to 1 the scatter-gather transfers are enabled.  Note, this field is only valid if the DMA channel has been configured with SG transfer support. | 
 +|::: |::: |[1] |PAUSE |RW |0x0 |When set to 1 the currently active transfer is paused. It will be resumed once the bit is cleared again. |
 |::: |::: |[0] |ENABLE |RW |0x0 |When set to 1 the DMA channel is enabled. | |::: |::: |[0] |ENABLE |RW |0x0 |When set to 1 the DMA channel is enabled. |
 ^0x101 ^0x0404 ^TRANSFER_ID ^^^^ ^ ^0x101 ^0x0404 ^TRANSFER_ID ^^^^ ^
 | | |[1:0] |TRANSFER_ID |RO |0x00 |This register contains the ID of the next transfer. The ID is generated by the DMAC and after the transfer has been started can be used to check if the transfer has finished by checking the corresponding bit in the TRANSFER_DONE register. The contents of this register is only valid if TRANSFER_SUBMIT is 0. | | | |[1:0] |TRANSFER_ID |RO |0x00 |This register contains the ID of the next transfer. The ID is generated by the DMAC and after the transfer has been started can be used to check if the transfer has finished by checking the corresponding bit in the TRANSFER_DONE register. The contents of this register is only valid if TRANSFER_SUBMIT is 0. |
 ^0x102 ^0x0408 ^TRANSFER_SUBMIT ^^^^ ^ ^0x102 ^0x0408 ^TRANSFER_SUBMIT ^^^^ ^
-| | |[0] |TRANSFER_SUBMIT |RW |0x00 |Writing a 1 to this register queues a new transfer. The bit transitions back to 0 once the transfer has been queued or the DMA channel is disabled.  Writing a 0 to this register has no effect. |+| | |[0] |TRANSFER_SUBMIT |RW |0x0 |Writing a 1 to this register queues a new transfer. The bit transitions back to 0 once the transfer has been queued or the DMA channel is disabled.  Writing a 0 to this register has no effect. |
 ^0x103 ^0x040c ^FLAGS ^^^^ ^ ^0x103 ^0x040c ^FLAGS ^^^^ ^
 | | |[0] |CYCLIC |RW |''CYCLIC'' |Setting this field to 1 puts the DMA transfer into cyclic mode. In cyclic mode the controller will re-start a transfer again once it has finished. In cyclic mode no end-of-transfer interrupts will be generated. | | | |[0] |CYCLIC |RW |''CYCLIC'' |Setting this field to 1 puts the DMA transfer into cyclic mode. In cyclic mode the controller will re-start a transfer again once it has finished. In cyclic mode no end-of-transfer interrupts will be generated. |
Line 713: Line 923:
 | | |[4:0] |ACTIVE_TRANSFER_ID |RO |0x00 |ID of the currently active transfer. When no transfer is active this register will be equal to the TRANSFER_ID register. | | | |[4:0] |ACTIVE_TRANSFER_ID |RO |0x00 |ID of the currently active transfer. When no transfer is active this register will be equal to the TRANSFER_ID register. |
 ^0x10c ^0x0430 ^STATUS ^^^^ ^ ^0x10c ^0x0430 ^STATUS ^^^^ ^
-| | |[31:0] |RESERVED |RO |0x00 |This register is reserved for future usage. Reading it will always return 0. |+| | |[31:0] |RESERVED |RO |0x00000000 |This register is reserved for future usage. Reading it will always return 0. |
 ^0x10d ^0x0434 ^CURRENT_DEST_ADDRESS ^^^^ ^ ^0x10d ^0x0434 ^CURRENT_DEST_ADDRESS ^^^^ ^
-| | |[31:0] |CURRENT_DEST_ADDRESS |RO |0x00 |Address to which the next data sample is written to.  This register is only valid if the DMA channel has been configured for write to memory support. |+| | |[31:0] |CURRENT_DEST_ADDRESS |RO |0x00000000 |Address to which the next data sample is written to.  This register is only valid if the DMA channel has been configured for write to memory support. |
 ^0x10e ^0x0438 ^CURRENT_SRC_ADDRESS ^^^^ ^ ^0x10e ^0x0438 ^CURRENT_SRC_ADDRESS ^^^^ ^
-| | |[31:0] |CURRENT_SRC_ADDRESS |RO |0x00 |Address form which the next data sample is read.  This register is only valid if the DMA channel has been configured for read from memory support. |+| | |[31:0] |CURRENT_SRC_ADDRESS |RO |0x00000000 |Address form which the next data sample is read.  This register is only valid if the DMA channel has been configured for read from memory support. |
 ^0x112 ^0x0448 ^TRANSFER_PROGRESS ^^^^ ^ ^0x112 ^0x0448 ^TRANSFER_PROGRESS ^^^^ ^
 | | |[23:0] |TRANSFER_PROGRESS |RO |0x000000 |This field presents the number of bytes transferred to the destination for the current transfer. This register will be cleared once the transfer completes. This should be used for debugging purposes only. | | | |[23:0] |TRANSFER_PROGRESS |RO |0x000000 |This field presents the number of bytes transferred to the destination for the current transfer. This register will be cleared once the transfer completes. This should be used for debugging purposes only. |
 ^0x113 ^0x044c ^PARTIAL_TRANSFER_LENGTH ^^^^ ^ ^0x113 ^0x044c ^PARTIAL_TRANSFER_LENGTH ^^^^ ^
-| | |[31:0] |PARTIAL_LENGTH |RO |0x000000 |Length of the partial transfer in bytes. Represents the number of bytes received until the moment of TLAST assertion. This will be smaller than the programmed length from the X_LENGTH and Y_LENGTH registers. |+| | |[31:0] |PARTIAL_LENGTH |RO |0x00000000 |Length of the partial transfer in bytes. Represents the number of bytes received until the moment of TLAST assertion. This will be smaller than the programmed length from the X_LENGTH and Y_LENGTH registers. |
 ^0x114 ^0x0450 ^PARTIAL_TRANSFER_ID ^^^^Must be read after the PARTIAL_TRANSFER_LENGTH registers. ^ ^0x114 ^0x0450 ^PARTIAL_TRANSFER_ID ^^^^Must be read after the PARTIAL_TRANSFER_LENGTH registers. ^
 | | |[1:0] |PARTIAL_TRANSFER_ID |RO |0x0 |ID of the transfer that was partial.  | | | |[1:0] |PARTIAL_TRANSFER_ID |RO |0x0 |ID of the transfer that was partial.  |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^0x115 ^0x0454 ^DESCRIPTOR_ID ^^^^ ^ 
 +| | |[31:0] |DESCRIPTOR_ID |RO |0x00000000 |ID of the descriptor that points to the current memory segment being transferred. If HWDESC is set to 0, then this register returns 0.  | 
 +^0x11f ^0x047c ^SG_ADDRESS ^^^^ ^ 
 +| | |[31:0] |SG_ADDRESS |RW |0x00000000 |This register contains the starting address of the scatter-gather transfer. The address needs to be aligned to the bus width.  This register is only valid if the DMA channel has been configured with SG transfer support. | 
 +^0x124 ^0x0490 ^DEST_ADDRESS_HIGH ^^^^ ^ 
 +| | |[31:0] |DEST_ADDRESS_HIGH |RW |0x00000000 |This register contains the HIGH segment of the destination address of the transfer.  This register is only valid if the DMA_AXI_ADDR_WIDTH is bigger than 32 and if DMA channel has been configured for write to memory support. | 
 +^0x125 ^0x0494 ^SRC_ADDRESS_HIGH ^^^^ ^ 
 +| | |[31:0] |SRC_ADDRESS_HIGH |RW |0x00000000 |This register contains the HIGH segment of the source address of the transfer.  This register is only valid if the DMA_AXI_ADDR_WIDTH is bigger than 32 and if the DMA channel has been configured for read from memory support. | 
 +^0x126 ^0x0498 ^CURRENT_DEST_ADDRESS_HIGH ^^^^ ^ 
 +| | |[31:0] |CURRENT_DEST_ADDRESS_HIGH |RO |0x00000000 |HIGH segment of the address to which the next data sample is written to.  This register is only valid if the DMA_AXI_ADDR_WIDTH is bigger than 32 and if the DMA channel has been configured for write to memory support. | 
 +^0x127 ^0x049c ^CURRENT_SRC_ADDRESS_HIGH ^^^^ ^ 
 +| | |[31:0] |CURRENT_SRC_ADDRESS_HIGH |RO |0x00000000 |HIGH segment of the address from which the next data sample is read.  This register is only valid if the DMA_AXI_ADDR_WIDTH is bigger than 32 and if the DMA channel has been configured for read from memory support. | 
 +^0x12f ^0x04bc ^SG_ADDRESS_HIGH ^^^^ ^ 
 +| | |[31:0] |SG_ADDRESS_HIGH |RW |0x00000000 |HIGH segment of the starting address of the scatter-gather transfer.  This register is only valid if the DMA_AXI_ADDR_WIDTH is bigger than 32 and if the DMA channel has been configured with SG transfer support. | 
 +^Thu Feb  1 12:18:03 2024 ^^^^^^
 ++++ ++++
  
Line 807: Line 1031:
 ^0x57 ^0x015c ^TACHO_100_TOL ^^^^ ^ ^0x57 ^0x015c ^TACHO_100_TOL ^^^^ ^
 | | |[31:0] |TACHO_100_TOL |RW |''TACHO_T100'' \\ ''*TACHO_TOL_PERCENT'' \\ ''/100'' |Tolerance for the 100% PWM tacho period | | | |[31:0] |TACHO_100_TOL |RW |''TACHO_T100'' \\ ''*TACHO_TOL_PERCENT'' \\ ''/100'' |Tolerance for the 100% PWM tacho period |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 831: Line 1055:
 ^0x400 ^0x1000 ^PRROM_START ^^^^ ^ ^0x400 ^0x1000 ^PRROM_START ^^^^ ^
 | | |[31:0] |SYSROM_START |RO |''N/A'' |Start of register space for partial reconfiguration block ROM. Initialized at synthesis. | | | |[31:0] |SYSROM_START |RO |''N/A'' |Start of register space for partial reconfiguration block ROM. Initialized at synthesis. |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 858: Line 1082:
 ^0x0050 ^0x0140 ^REG_FPGA_VOLTAGE ^^^^FPGA device voltage information ^ ^0x0050 ^0x0140 ^REG_FPGA_VOLTAGE ^^^^FPGA device voltage information ^
 | | |[15:0] |FPGA_VOLTAGE |RO |0x0 |The voltage of the FPGA device in mv | | | |[15:0] |FPGA_VOLTAGE |RO |0x0 |The voltage of the FPGA device in mv |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^ 
 +++++ 
 + 
 + 
 +==== Clock Monitor (axi_clock_monitor) ==== 
 + 
 +++++ Click to expand regmap | 
 +|< 100% 5% 5% 5% 25% 5% 5% 50% >| 
 +|Address ||Bits |Name |Type |Default |Description | 
 +|DWORD |BYTE |::: |::: |::: |::: |::: | 
 +^0x0000 ^0x0000 ^PCORE_VERSION ^^^^PCORE Version Registers ^ 
 +| | |[31:0] |PCORE_VERSION |RO |0x00000001 |PCORE Version number | 
 +^0x0001 ^0x0004 ^ID ^^^^ID Registers ^ 
 +| | |[31:0] |ID |RW |0x00000000 |Instance identifier number | 
 +^0x0003 ^0x000c ^NUM_OF_CLOCKS ^^^^Number of Clocks Registers ^ 
 +| | |[31:0] |NUM_OF_CLOCKS |RW |0x00000008 |Number of clock inputs | 
 +^0x0004 ^0x0010 ^OUT_RESET ^^^^Reset Control Registers ^ 
 +| | |0x0 |reset |RW |0x00 |Control the out reset signal | 
 +^0x0010 ^0x0040 ^CLOCK_0 ^^^^Measured clock_0 ^ 
 +| | |[31:0] |clock_0 |RO |0x00000000 |Measured frequency of clock_0 | 
 +^0x0011 ^0x0044 ^CLOCK_1 ^^^^Measured clock_1 ^ 
 +| | |[31:0] |clock_1 |RO |0x00000000 |Measured frequency of clock_1 | 
 +^0x0012 ^0x0048 ^CLOCK_2 ^^^^Measured clock_2 ^ 
 +| | |[31:0] |clock_2 |RO |0x00000000 |Measured frequency of clock_2 | 
 +^0x0013 ^0x004c ^CLOCK_3 ^^^^Measured clock_3 ^ 
 +| | |[31:0] |clock_3 |RO |0x00000000 |Measured frequency of clock_3 | 
 +^0x0014 ^0x0050 ^CLOCK_4 ^^^^Measured clock_4 ^ 
 +| | |[31:0] |clock_4 |RO |0x00000000 |Measured frequency of clock_4 | 
 +^0x0015 ^0x0054 ^CLOCK_5 ^^^^Measured clock_5 ^ 
 +| | |[31:0] |clock_5 |RO |0x00000000 |Measured frequency of clock_5 | 
 +^0x0016 ^0x0058 ^CLOCK_6 ^^^^Measured clock_6 ^ 
 +| | |[31:0] |clock_6 |RO |0x00000000 |Measured frequency of clock_6 | 
 +^0x0017 ^0x005c ^CLOCK_7 ^^^^Measured clock_7 ^ 
 +| | |[31:0] |clock_7 |RO |0x00000000 |Measured frequency of clock_7 | 
 +^0x0018 ^0x0060 ^CLOCK_8 ^^^^Measured clock_8 ^ 
 +| | |[31:0] |clock_8 |RO |0x00000000 |Measured frequency of clock_8 | 
 +^0x0019 ^0x0064 ^CLOCK_9 ^^^^Measured clock_9 ^ 
 +| | |[31:0] |clock_9 |RO |0x00000000 |Measured frequency of clock_9 | 
 +^0x001A ^0x0068 ^CLOCK_10 ^^^^Measured clock_10 ^ 
 +| | |[31:0] |clock_10 |RO |0x00000000 |Measured frequency of clock_10 | 
 +^0x001B ^0x006c ^CLOCK_11 ^^^^Measured clock_11 ^ 
 +| | |[31:0] |clock_11 |RO |0x00000000 |Measured frequency of clock_11 | 
 +^0x001C ^0x0070 ^CLOCK_12 ^^^^Measured clock_12 ^ 
 +| | |[31:0] |clock_12 |RO |0x00000000 |Measured frequency of clock_12 | 
 +^0x001D ^0x0074 ^CLOCK_13 ^^^^Measured clock_13 ^ 
 +| | |[31:0] |clock_13 |RO |0x00000000 |Measured frequency of clock_13 | 
 +^0x001E ^0x0078 ^CLOCK_14 ^^^^Measured clock_14 ^ 
 +| | |[31:0] |clock_14 |RO |0x00000000 |Measured frequency of clock_14 | 
 +^0x001F ^0x007c ^CLOCK_15 ^^^^Measured clock_15 ^ 
 +| | |[31:0] |clock_15 |RO |0x00000000 |Measured frequency of clock_15 | 
 +^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 914: Line 1188:
 | | |[31:16] |V_ENABLE_MAX[15:0] |RW |0x0000 |This is the vertical data enable maximum. It is the sum of V_ENABLE_MIN and the active pixel height. e.g. 1121 (41 + 1080) (1080p) | | | |[31:16] |V_ENABLE_MAX[15:0] |RW |0x0000 |This is the vertical data enable maximum. It is the sum of V_ENABLE_MIN and the active pixel height. e.g. 1121 (41 + 1080) (1080p) |
 |::: |::: |[15:0] |V_ENABLE_MIN[15:0] |RW |0x0000 |This is the vertical data enable minimum. It is the sum of vertical back porch (number of lines between the falling edge of VSYNC to the rising edge of DE) and the sync width. e.g. 41 (36 + 5) (1080p) | |::: |::: |[15:0] |V_ENABLE_MIN[15:0] |RW |0x0000 |This is the vertical data enable minimum. It is the sum of vertical back porch (number of lines between the falling edge of VSYNC to the rising edge of DE) and the sync width. e.g. 41 (36 + 5) (1080p) |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 951: Line 1225:
 | | |[31:16] |VS_COUNT[15:0] |RO |0x0000 |This is the detected horizontal active pixel lines (active resolution length). This field is valid only if VS_OOS is zero. | | | |[31:16] |VS_COUNT[15:0] |RO |0x0000 |This is the detected horizontal active pixel lines (active resolution length). This field is valid only if VS_OOS is zero. |
 |::: |::: |[15:0] |HS_COUNT[15:0] |RO |0x0000 |This is the detected horizontal pixel count (no. of pixel clocks per line). This field is valid only if HS_OOS is zero. | |::: |::: |[15:0] |HS_COUNT[15:0] |RO |0x0000 |This is the detected horizontal pixel count (no. of pixel clocks per line). This field is valid only if HS_OOS is zero. |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 977: Line 1251:
 ^0x0220 ^0x0880 ^REG_* ^^^^Channel 2, similar to register 0x200 to 0x20f. ^ ^0x0220 ^0x0880 ^REG_* ^^^^Channel 2, similar to register 0x200 to 0x20f. ^
 ^0x02f0 ^0x0bc0 ^REG_* ^^^^Channel 15, similar to register 0x200 to 0x20f. ^ ^0x02f0 ^0x0bc0 ^REG_* ^^^^Channel 15, similar to register 0x200 to 0x20f. ^
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 1034: Line 1308:
 ^0x45 ^0x0114 ^OFFLOAD0_SDO_FIFO ^^^^ ^ ^0x45 ^0x0114 ^OFFLOAD0_SDO_FIFO ^^^^ ^
 | | |[31:0] |OFFLOAD0_SDO_FIFO |WO |0x???????? |Offload SDO FIFO register. Writing to this register inserts an entry into the offload SDO FIFO. Writing to this register when the SDO FIFO is full has no effect and the written entry is discarded. Reading from this register always returns 0x00000000. | | | |[31:0] |OFFLOAD0_SDO_FIFO |WO |0x???????? |Offload SDO FIFO register. Writing to this register inserts an entry into the offload SDO FIFO. Writing to this register when the SDO FIFO is full has no effect and the written entry is discarded. Reading from this register always returns 0x00000000. |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^
 ++++ ++++
  
Line 1128: Line 1402:
 | | |[8] |PRBSERR |RO |0x00 |This sticky status output indicates that PRBS errors have occurred. Value of error counter must be accessed via DRP. | | | |[8] |PRBSERR |RO |0x00 |This sticky status output indicates that PRBS errors have occurred. Value of error counter must be accessed via DRP. |
 |::: |::: |[0] |PRBSLOCKED |RO |0x00 |Ignore this bit for GTX transceivers. For others: Indicates that the RX PRBS checker has been error free for 15 XCLK cycles after reset. Once asserted High, it does not deassert until reset of the RX pattern checker via PRBSCNTRESET | |::: |::: |[0] |PRBSLOCKED |RO |0x00 |Ignore this bit for GTX transceivers. For others: Indicates that the RX PRBS checker has been error free for 15 XCLK cycles after reset. Once asserted High, it does not deassert until reset of the RX pattern checker via PRBSCNTRESET |
-^Thu Jan 27 14:25:46 2022 ^^^^^^+^Tue Mar 14 10:17:59 2023 ^^^^^^ 
 +++++ 
 + 
 + 
 +==== PWM Generator (axi_pwm_gen) ==== 
 + 
 +++++ Click to expand regmap | 
 +|< 100% 5% 5% 5% 25% 5% 5% 50% >| 
 +|Address ||Bits |Name |Type |Default |Description | 
 +|DWORD |BYTE |::: |::: |::: |::: |::: | 
 +^0x0000 ^0x0000 ^REG_VERSION ^^^^Version and Scratch Registers ^ 
 +| | |[31:0] |VERSION[31:0] |RO |0x00020000 |Version number. Unique to all cores. | 
 +^0x0001 ^0x0004 ^REG_ID ^^^^Core ID ^ 
 +| | |[31:0] |ID[31:0] |RO |0x00000000 |Instance identifier number. | 
 +^0x0002 ^0x0008 ^REG_SCRATCH ^^^^Version and Scratch Registers ^ 
 +| | |[31:0] |SCRATCH[31:0] |RW |0x00000000 |Scratch register. | 
 +^0x0003 ^0x000c ^REG_CORE_MAGIC ^^^^Identification number ^ 
 +| | |[31:0] |CORE_MAGIC[31:0] |RW |0x601A3471 |Identification number. | 
 +^0x0004 ^0x0010 ^REG_RSTN ^^^^Reset and load values ^ 
 +| | |[1] |LOAD_CONFIG |WO |0x0 |Loads the new values written in the config registers. | 
 +|::: |::: |[0] |RESET |RW |0x0 |Reset, default is (0x0). | 
 +^0x0005 ^0x0014 ^REG_NB_PULSES ^^^^Number of pulses ^ 
 +| | |[31:0] |NB_PULSES |RO |0x0000 |Number of configurable pulses. | 
 +^0x0010 ^0x0040 ^REG_PULSE_X_PERIOD ^^^^Pulse x period ^ 
 +| | |[31:0] |PULSE_X_PERIOD[31:0] - base + 'h4 for each channel -> e.g. CH3 period - 'h4C|RW |0x0000 |Pulse x duration, defined in number of clock cycles. | 
 +^0x0020 ^0x0080 ^REG_PULSE_X_WIDTH ^^^^Pulse x width ^ 
 +| | |[31:0] |PULSE_X_WIDTH[31:0] - base + 'h4 for each channel -> e.g. CH3 width - 'h8C|RW |0x0000 |Pulse x width (high time), defined in number of clock cycles. | 
 +^0x0030 ^0x00C0 ^REG_PULSE_X_OFFSET ^^^^Pulse x offset ^ 
 +| | |[31:0] |PULSE_X_OFFSET[31:0] - base + 'h4 for each channel -> e.g. CH3 offset - 'hCC|RW |0x0000 |Pulse x offset, defined in number of clock cycles. | 
 ++++ ++++
 ~~NOTOC~~ ~~NOTOC~~
  
  
resources/fpga/docs/hdl/regmap.txt · Last modified: 19 Feb 2024 13:35 by Adrian Costina