This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:docs:axi_tdd [09 Oct 2021 13:44] – Minor review Adrian Costina | resources:fpga:docs:axi_tdd [27 Jul 2023 21:56] (current) – Removed obsolete linux references Ionut Podgoreanu | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
- | TDD (Time Division Duplex) mode allows the user to control the time period of the receive and transmit bursts. | + | TDD (Time-Division Duplex) mode allows the user to control the time period of the receive and transmit bursts. |
- | The AXI TDD engine | + | The generic |
+ | |||
+ | The reason of creating | ||
===== Features ===== | ===== Features ===== | ||
- | * 6 independent output channels | + | * Up to 32 independent output channels |
- | * Primary | + | * Start/stop time values per channel |
- | * 24 bit accumulator | + | * Enable |
- | * External (1 PPS, shared or from GPSDO, etc.) synchronization to work with multiple devices | + | * 32 bit-max internal reference counter |
- | + | * Initial startup delay before waveform generation | |
- | ===== Utilization ===== | + | * Configurable frame length and number of frames per burst |
- | + | * 3 sources of synchronization: | |
- | ^ Device Family ^ LUTs ^ FFs ^ | + | |
- | | Xilinx Zynq UltraScale+ | 990 | 2738 | | + | |
Line 22: | Line 22: | ||
^ Name ^ Description ^ | ^ Name ^ Description ^ | ||
- | | [[https:// | + | | [[https:// |
- | | [[https:// | + | | [[https:// |
- | | [[https:// | + | | [[https:// |
- | | [[https:// | + | | [[https:// |
- | | [[https:// | + | | [[https:// |
+ | | [[https:// | ||
+ | | [[https://github.com/analogdevicesinc/ | ||
+ | | [[https:// | ||
- | ===== Theory of Operation ===== | ||
- | The central idea of the TDD engine is " | + | ===== Synthesis Configuration Parameters ===== |
- | {{: | + | ^ Name ^ Description ^ Max value ^ Default ^ |
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | ===== Signal and Interface Pins ===== | ||
- | This diagram tries to illustrate how the different channels can be enabled at different times relative to the beginning of a frame. | + | {{: |
- | <note tip> | + | ^ Name ^ Type ^ Description ^ |
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | ===== Register Map ===== | ||
- | ===== Connectivity ===== | + | {{page>: |
- | {{: | + | |< 100% 10em 10em >| |
+ | ^ Access Type ^ Name ^ Description ^ | ||
+ | | R | Read-only | Reads will return the current register value. Writes have no effect. | | ||
+ | | RW | Read-write | Reads will return the current register value. Writes will change the current register value. | | ||
+ | | U | Unimplemented | Register field is unimplemented. | | ||
+ | ===== Theory of Operation ===== | ||
- | ==== Detailed description ==== | + | The central idea of the TDD controller is “frame”-based operation, i.e. all the timing defined for the individual channels is relative to the beginning of a frame. The '' |
- | When there is asymmetry (caused by dynamically allocating the amount of time for uplink and downlink) between the data rates of the uplink and downlink, the IP is able to control when the RX buffer is read from and the TX buffer is played. | + | {{: |
- | There will be a fixed time offset between every i-th RX and TX sample, synchronizing the communication between the transmit and receive paths, as simple as possible, without using network synchronization. | + | |
- | AXI TDD divides data streams into frames and assigns different time slots to forward and reverse transmissions, | + | This diagram tries to illustrate how the different channels can be enabled |
- | The TDD control contains 2 counters: a 24 bit free running counter for frames, and a 6 bit counter for bursts, | + | <note tip> |
- | The frame counter counts to the length of the current frame that is processed, and marks further if the end of the frame has been reached (also resetting the counter). Depending on the registers it is compared with, some control signals are turned on or off (for VCO and RF paths). | ||
- | The end of a burst is marked by the last burst and the end of the frame. | ||
- | The frame counter is implemented using a state machine. | + | ==== Detailed description ==== |
- | When counter is working (ON state), and either the TDD is not enabled or it reached the end of burst, the counter in the next state will stop counting. | + | |
- | When the counter is stopped (OFF state), it can be turned on again by enabling the TDD. | + | |
+ | In order to begin its operation, the peripheral must be enabled. This is done by setting the '' | ||
- | ==== I/O Interface ==== | + | The external synchronization capability allows the alignment of frames between multiple devices in different locations, for example using a GPSDO 1 PPS output. The internal sync signal is generated based on a dedicated counter, when its value matches the one defined in '' |
- | ^ Interface ^ Pin ^ Type ^ Description ^ | + | The next diagram shows the peripheral’s FSM, which transitions between 4 states: IDLE, ARMED, WAITING |
- | | **Core clock and reset** |||| | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | **TDD control interface** |||| | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | **TDD sync interface** |||| | + | |
- | | | '' | + | |
- | | | '' | + | |
- | | **AXI4 Lite interface** |||| | + | |
- | | | '' | + | |
- | + | ||
- | ===== Register Map ===== | + | |
- | < | + | {{: |
- | |< 100% 5% 5% 5% 25% 5% 5% 50% >| | + | In case a synchronization signal |
- | |Address ||Bits |Name |Type |Default |Description | | + | |
- | |DWORD |BYTE |::: |::: |::: |::: |::: | | + | |
- | ^0x0010 ^0x0040 ^REG_TDD_CONTROL_0 ^^^^TDD Control & Status ^ | + | |
- | | | |[5] |TDD_GATED_TX_DMAPATH |RW |0x0 |If this bit is set, the core requests data from the TX DMA, just when the data path is active. Otherwise will requests continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity. | | + | |
- | |::: |::: |[4] |TDD_GATED_RX_DMAPATH |RW |0x0 |If this bit is set, the core provides data for the RX DMA, just when the data path is active. Otherwise will provides continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity. | | + | |
- | |::: |::: |[3] |TDD_TXONLY |RW |0x0 |If this bit is set- the TDD controller ignores all the TX_* timing registers | + | |
- | |::: |::: |[2] |TDD_RXONLY |RW |0x0 |If this bit is set- the TDD controller ignores all the RX_* timing registers | + | |
- | |::: |::: |[1] |TDD_SECONDARY |RW |0x0 |Enable the secondary transmit/ | + | |
- | |::: |::: |[0] |TDD_ENABLE |RW |0x0 |If set, enables | + | |
- | ^0x0011 ^0x0044 ^REG_TDD_CONTROL_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[7:0] |TDD_BURST_COUNT |RW |0x00 |If set to 0x0 and enabled (TDD_ENABLE is set) - the controller operates in TDD mode as long as the TDD_ENABLE bit is set. If set to a non-zero value, the controller operates for the set number of frames and stops. | | + | |
- | ^0x0012 ^0x0048 ^REG_TDD_CONTROL_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_COUNTER_INIT |RW |0x000000 |The controller sets the frame counter | + | |
- | ^0x0013 ^0x004c ^REG_TDD_FRAME_LENGTH ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_FRAME_LENGTH |RW |0x000000 |The frame length is the terminal count for the 10ms counter running at the digital | + | |
- | ^0x0014 ^0x0050 ^REG_TDD_SYNC_TERMINAL_TYPE ^^^^TDD Control & Status ^ | + | |
- | | | |[0] |TDD_SYNC_TERMINAL_TYPE |RW |0x0 |Set this bit, if the current terminal will generate the syncronization pulse, reset otherwise. | | + | |
- | ^0x0018 ^0x0060 ^REG_TDD_STATUS ^^^^TDD Control & Status ^ | + | |
- | | | |[0] |TDD_RXTX_VCO_OVERLAP |RO |0x0 |This bit is asserted, if exist a time interval when both the TX and RX VCOs are powered up. | | + | |
- | |::: |::: |[1] |TDD_RXTX_RF_OVERLAP |RO |0x0 |This bit is asserted, if exist a time interval when both the TX and RX RF datapath are powered up. | | + | |
- | ^0x0020 ^0x0080 ^REG_TDD_VCO_RX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX VCO powers up at the first time. The controller enables the receive VCO, when the frame count reaches this value. The VCO may have to be enabled before data can be received. The user needs to make sure, that the RF device is in a state, from where this operation is valid. | + | |
- | ^0x0021 ^0x0084 ^REG_TDD_VCO_RX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX VCO powers down at the first time. The controller disables the receive VCO, when the frame count reaches this value. | + | |
- | ^0x0022 ^0x0088 ^REG_TDD_VCO_TX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX VCO powers up at the first time. The controller enables the transmit VCO, when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. | | + | |
- | ^0x0023 ^0x008c ^REG_TDD_VCO_TX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX VCO powers down at the first time. The controller disables the transmit VCO when the frame count reaches this value. | + | |
- | ^0x0024 ^0x0090 ^REG_TDD_RX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX data path is activated at the first time. The controller enables the receive chain when the frame count reaches this value. | + | |
- | ^0x0025 ^0x0094 ^REG_TDD_RX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX data path is deactivated the first time. The controller disables the receive chain when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. | + | |
- | ^0x0026 ^0x0098 ^REG_TDD_TX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX data path is activated at the first time. The controller enables the transmit chain, when the frame count reaches this value. This register and the TX_DP_ON register controls the delay between the data path being activated and the time to actually push the transmit data through the transmit chain in the device. | | + | |
- | ^0x0027 ^0x009c ^REG_TDD_TX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX data path is deactivated at the first time. The controller disables the transmit chain, when the frame count reaches this value. This register and the TX_DP_OFF register controls the delay between the data path being deactivated and the time to actually stop transmitting data through the transmit chain in the device. | | + | |
- | ^0x0028 ^0x00a0 ^REG_TDD_RX_DP_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller starts to accept data from the digital interface for receive. | | + | |
- | ^0x0029 ^0x00a4 ^REG_TDD_RX_DP_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller stops to accept data from the digital interface for receive. | | + | |
- | ^0x002A ^0x00a8 ^REG_TDD_TX_DP_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller starts to request data from the system memory for transmit. The data rate is controlled by the TDD controller. | | + | |
- | ^0x002B ^0x00ac ^REG_TDD_TX_DP_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller stop requesting data from the system memory for transmit. | | + | |
- | ^0x0030 ^0x00c0 ^REG_TDD_VCO_RX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_ON_2 |RW |0x000000 |The secondary pointer for VCO_RX_ON. | + | |
- | ^0x0031 ^0x00c4 ^REG_TDD_VCO_RX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_OFF_2 |RW |0x000000 |The secondary pointer for VCO_RX_OFF. | | + | |
- | ^0x0032 ^0x00c8 ^REG_TDD_VCO_TX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_ON_2 |RW |0x000000 |The secondary pointer for VCO_TX_ON. | | + | |
- | ^0x0033 ^0x00cc ^REG_TDD_VCO_TX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_OFF_2 |RW |0x000000 |The secondary pointer for VCO_TX_OFF. | | + | |
- | ^0x0034 ^0x00d0 ^REG_TDD_RX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_ON_2 |RW |0x000000 |The secondary pointer for RX_ON. | | + | |
- | ^0x0035 ^0x00d4 ^REG_TDD_RX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_OFF_2 |RW |0x000000 |The secondary pointer for RX_OFF. | | + | |
- | ^0x0036 ^0x00d8 ^REG_TDD_TX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_ON_2 |RW |0x000000 |The secondary pointer for TX_ON. | | + | |
- | ^0x0037 ^0x00dc ^REG_TDD_TX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_OFF_2 |RW |0x000000 |The secondary pointer for TX_OFF. | | + | |
- | ^0x0038 ^0x00e0 ^REG_TDD_RX_DP_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_ON_2 |RW |0x000000 |The secondary pointer for RX_DP_ON. | | + | |
- | ^0x0039 ^0x00e4 ^REG_TDD_RX_DP_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_OFF_2 |RW |0x000000 |The secondary pointer for RX_DP_OFF. | | + | |
- | ^0x003A ^0x00e8 ^REG_TDD_TX_DP_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_ON_2 |RW |0x000000 |The secondary pointer for TX_DP_ON. | | + | |
- | ^0x003B ^0x00ec ^REG_TDD_TX_DP_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_OFF_2 |RW |0x000000 |The secondary pointer for TX_DP_OFF. | | + | |
- | </hidden> | + | The generic TDD controller can have up to 32 output channels, each of them having its unique values when the channel is set/reset under '' |
- | ===== Linux IIO Driver ===== | + | Every bit in '' |
- | The [[https:// | + | The following registers will not be updated unless |
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
- | < | + | The user should configure them before enabling the peripheral. Any subsequent write while the peripheral is enabled will be ignored. |
- | axi_tdd_0: axi-tdd-0@9c460000 { | + | |
- | compatible = " | + | |
- | reg = < | + | |
- | clocks = <& | + | |
- | clock-names = " | + | |
- | }; | + | |
- | </ | + | |
- | <note tip> | + | An exception |
- | The driver needs to know which clock is driving the main clock input '' | + | |
- | </ | + | |
- | The resulting IIO device looks like this, where there is one channel per combination of '' | + | '' |
- | < | + | |
- | iio: | + | |
- | 4 channels found: | + | |
- | data1: | + | |
- | 6 channel-specific attributes found: | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | data1: | + | |
- | 6 channel-specific attributes found: | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | data0: | + | |
- | 6 channel-specific attributes found: | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | data0: | + | |
- | 6 channel-specific attributes found: | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | 10 device-specific attributes found: | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | attr | + | |
- | 1 debug attributes found: | + | |
- | debug attr 0: direct_reg_access value: 0x10061 | + | |
- | No trigger on this device | + | |
- | </ | + | |
- | | [[https:// | + | By adapting the synthesis parameters to the application requirements, |
+ | {{navigation HDL User Guide# |