This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:docs:axi_tdd [27 Sep 2021 16:01] – [Linux IIO Driver] David Winter | resources:fpga:docs:axi_tdd [07 Oct 2022 06:48] – [Theory of Operation] Ionut Podgoreanu | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
+ | |||
+ | TDD (Time-Division Duplex) mode allows the user to control the time period of the receive and transmit bursts. | ||
+ | |||
+ | The generic TDD controller is in essence a waveform generator capable of addressing RF applications which require Time Division Duplexing, as well as controlling other modules of general applications through its dedicated 32 channel outputs. | ||
+ | |||
+ | The reason of creating the generic TDD controller was to reduce the naming confusion around the existing repurposed [[resources: | ||
- | The AXI TDD engine is a relatively simple peripheral originally intended to be used for TDD (wireless) communication systems. | ||
===== Features ===== | ===== Features ===== | ||
- | * 6 independent output channels | + | * Up to 32 independent output channels |
- | * Primary | + | * Start/stop time values per channel |
- | * 24 bit accumulator | + | * Enable |
- | * External (1 PPS, shared or from GPSDO, etc.) synchronization | + | * 32 bit-max internal reference counter |
+ | * Initial startup delay before waveform generation | ||
+ | * Configurable frame length and number of frames per burst | ||
+ | * 3 sources of synchronization: external, internal and software generated | ||
===== Utilization ===== | ===== Utilization ===== | ||
Line 19: | Line 28: | ||
^ Name ^ Description ^ | ^ Name ^ Description ^ | ||
- | | [[https:// | + | | [[https:// |
- | | [[https:// | + | | [[https:// |
- | | [[https:// | + | | [[https:// |
+ | | [[https:// | ||
+ | | [[https:// | ||
+ | | [[https:// | ||
+ | | [[https:// | ||
+ | | [[https:// | ||
| [[https:// | | [[https:// | ||
| [[https:// | | [[https:// | ||
+ | |||
+ | ===== Synthesis Configuration Parameters ===== | ||
+ | |||
+ | ^ Name ^ Description ^ Max value ^ Default ^ | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | ===== Signal and Interface Pins ===== | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ^ Name ^ Type ^ Description ^ | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | | '' | ||
+ | ===== Register Map ===== | ||
+ | |||
+ | {{page>: | ||
+ | |||
+ | |< 100% 10em 10em >| | ||
+ | ^ Access Type ^ Name ^ Description ^ | ||
+ | | HR | Hardware-reset | Register field is reset by hardware. | | ||
+ | | R | Read-only | Reads will return the current register value. Writes have no effect. | | ||
+ | | RW | Read-write | Reads will return the current register value. Writes will change the current register value. | | ||
+ | | U | Unimplemented | Register field is unimplemented. | | ||
===== Theory of Operation ===== | ===== Theory of Operation ===== | ||
- | The central idea of the TDD engine | + | The central idea of the TDD controller |
{{: | {{: | ||
Line 35: | Line 85: | ||
<note tip> | <note tip> | ||
- | ===== Connectivity ===== | ||
- | {{: | + | ==== Detailed description ==== |
- | * Sample '' | + | In order to begin its operation, the peripheral must be enabled. This is done by setting the '' |
- | * AXI4-Lite (Interface, '' | + | |
- | * 6 TDD output channels ( '' | + | |
- | * 1 PPS TDD synchronization input: | + | |
- | * Status output: | + | |
+ | The external synchronization capability allows the alignment of frames between multiple devices in different locations, for example using a GPSDO 1 PPS output. The internal sync signal is generated based on a dedicated counter, when its value matches the one defined in '' | ||
- | ===== Register Map ===== | + | The next diagram shows the peripheral’s FSM, which transitions between 4 states: IDLE, ARMED, WAITING and RUNNING. |
+ | |||
+ | {{: | ||
+ | |||
+ | In case a synchronization signal is received while the TDD core is running, the signal can reset the internal counter to zero by setting '' | ||
+ | |||
+ | The generic TDD controller can have up to 32 output channels, each of them having its unique values when the channel is set/reset under '' | ||
+ | |||
+ | Every bit in '' | ||
+ | |||
+ | The following registers will not be updated unless the peripheral is disabled: | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
+ | |||
+ | The user should configure them before enabling the peripheral. Any subsequent write while the peripheral is enabled will be ignored. | ||
- | < | + | An exception to this rule is '' |
- | |< 100% 5% 5% 5% 25% 5% 5% 50% >| | + | '' |
- | |Address ||Bits |Name |Type |Default |Description | | + | |
- | |DWORD |BYTE |::: |::: |::: |::: |::: | | + | |
- | ^0x0010 ^0x0040 ^REG_TDD_CONTROL_0 ^^^^TDD Control & Status ^ | + | |
- | | | |[5] |TDD_GATED_TX_DMAPATH |RW |0x0 |If this bit is set, the core requests data from the TX DMA, just when the data path is active. Otherwise will requests continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity. | | + | |
- | |::: |::: |[4] |TDD_GATED_RX_DMAPATH |RW |0x0 |If this bit is set, the core provides data for the RX DMA, just when the data path is active. Otherwise will provides continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity. | | + | |
- | |::: |::: |[3] |TDD_TXONLY |RW |0x0 |If this bit is set- the TDD controller ignores all the TX_* timing registers | + | |
- | |::: |::: |[2] |TDD_RXONLY |RW |0x0 |If this bit is set- the TDD controller ignores all the RX_* timing registers | + | |
- | |::: |::: |[1] |TDD_SECONDARY |RW |0x0 |Enable the secondary transmit/ | + | |
- | |::: |::: |[0] |TDD_ENABLE |RW |0x0 |If set, enables the TDD controller- software must set this bit after programming | + | |
- | ^0x0011 ^0x0044 ^REG_TDD_CONTROL_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[7:0] |TDD_BURST_COUNT |RW |0x00 |If set to 0x0 and enabled (TDD_ENABLE is set) - the controller operates in TDD mode as long as the TDD_ENABLE bit is set. If set to a non-zero value, the controller operates for the set number of frames and stops. | | + | |
- | ^0x0012 ^0x0048 ^REG_TDD_CONTROL_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_COUNTER_INIT |RW |0x000000 |The controller sets the frame counter to this value when starting TDD operation. | + | |
- | ^0x0013 ^0x004c ^REG_TDD_FRAME_LENGTH ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_FRAME_LENGTH |RW |0x000000 |The frame length is the terminal count for the 10ms counter running at the digital | + | |
- | ^0x0014 ^0x0050 ^REG_TDD_SYNC_TERMINAL_TYPE ^^^^TDD Control & Status ^ | + | |
- | | | |[0] |TDD_SYNC_TERMINAL_TYPE |RW |0x0 |Set this bit, if the current | + | |
- | ^0x0018 ^0x0060 ^REG_TDD_STATUS ^^^^TDD Control & Status ^ | + | |
- | | | |[0] |TDD_RXTX_VCO_OVERLAP |RO |0x0 |This bit is asserted, if exist a time interval when both the TX and RX VCOs are powered up. | | + | |
- | |::: |::: |[1] |TDD_RXTX_RF_OVERLAP |RO |0x0 |This bit is asserted, if exist a time interval when both the TX and RX RF datapath are powered up. | | + | |
- | ^0x0020 ^0x0080 ^REG_TDD_VCO_RX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX VCO powers up at the first time. The controller enables the receive VCO, when the frame count reaches this value. | + | |
- | ^0x0021 ^0x0084 ^REG_TDD_VCO_RX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX VCO powers down at the first time. The controller disables the receive VCO, when the frame count reaches this value. | + | |
- | ^0x0022 ^0x0088 ^REG_TDD_VCO_TX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX VCO powers up at the first time. The controller enables the transmit VCO, when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. | | + | |
- | ^0x0023 ^0x008c ^REG_TDD_VCO_TX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX VCO powers down at the first time. The controller disables the transmit VCO when the frame count reaches this value. | + | |
- | ^0x0024 ^0x0090 ^REG_TDD_RX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX data path is activated at the first time. The controller enables the receive chain when the frame count reaches this value. | + | |
- | ^0x0025 ^0x0094 ^REG_TDD_RX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the RX data path is deactivated the first time. The controller disables the receive chain when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. | + | |
- | ^0x0026 ^0x0098 ^REG_TDD_TX_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX data path is activated at the first time. The controller enables the transmit chain, when the frame count reaches this value. This register and the TX_DP_ON register controls the delay between the data path being activated and the time to actually push the transmit data through the transmit chain in the device. | | + | |
- | ^0x0027 ^0x009c ^REG_TDD_TX_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the TX data path is deactivated at the first time. The controller disables the transmit chain, when the frame count reaches this value. This register and the TX_DP_OFF register controls the delay between the data path being deactivated and the time to actually stop transmitting data through the transmit chain in the device. | | + | |
- | ^0x0028 ^0x00a0 ^REG_TDD_RX_DP_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller starts to accept data from the digital interface for receive. | | + | |
- | ^0x0029 ^0x00a4 ^REG_TDD_RX_DP_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller stops to accept data from the digital interface for receive. | | + | |
- | ^0x002A ^0x00a8 ^REG_TDD_TX_DP_ON_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_ON_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller starts to request data from the system memory for transmit. The data rate is controlled by the TDD controller. | | + | |
- | ^0x002B ^0x00ac ^REG_TDD_TX_DP_OFF_1 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_OFF_1 |RW |0x000000 |Defines the offset (from frame count equal zero), when the controller stop requesting data from the system memory for transmit. | | + | |
- | ^0x0030 ^0x00c0 ^REG_TDD_VCO_RX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_ON_2 |RW |0x000000 |The secondary pointer for VCO_RX_ON. | + | |
- | ^0x0031 ^0x00c4 ^REG_TDD_VCO_RX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_RX_OFF_2 |RW |0x000000 |The secondary pointer for VCO_RX_OFF. | | + | |
- | ^0x0032 ^0x00c8 ^REG_TDD_VCO_TX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_ON_2 |RW |0x000000 |The secondary pointer for VCO_TX_ON. | | + | |
- | ^0x0033 ^0x00cc ^REG_TDD_VCO_TX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_VCO_TX_OFF_2 |RW |0x000000 |The secondary pointer for VCO_TX_OFF. | | + | |
- | ^0x0034 ^0x00d0 ^REG_TDD_RX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_ON_2 |RW |0x000000 |The secondary pointer for RX_ON. | | + | |
- | ^0x0035 ^0x00d4 ^REG_TDD_RX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_OFF_2 |RW |0x000000 |The secondary pointer for RX_OFF. | | + | |
- | ^0x0036 ^0x00d8 ^REG_TDD_TX_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_ON_2 |RW |0x000000 |The secondary pointer for TX_ON. | | + | |
- | ^0x0037 ^0x00dc ^REG_TDD_TX_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_OFF_2 |RW |0x000000 |The secondary pointer for TX_OFF. | | + | |
- | ^0x0038 ^0x00e0 ^REG_TDD_RX_DP_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_ON_2 |RW |0x000000 |The secondary pointer for RX_DP_ON. | | + | |
- | ^0x0039 ^0x00e4 ^REG_TDD_RX_DP_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_RX_DP_OFF_2 |RW |0x000000 |The secondary pointer for RX_DP_OFF. | | + | |
- | ^0x003A ^0x00e8 ^REG_TDD_TX_DP_ON_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_ON_2 |RW |0x000000 |The secondary pointer for TX_DP_ON. | | + | |
- | ^0x003B ^0x00ec ^REG_TDD_TX_DP_OFF_2 ^^^^TDD Control & Status ^ | + | |
- | | | |[23:0] |TDD_TX_DP_OFF_2 |RW |0x000000 |The secondary pointer for TX_DP_OFF. | | + | |
- | </ | + | By adapting the synthesis parameters to the application requirements, |
===== Linux IIO Driver ===== | ===== Linux IIO Driver ===== | ||
Line 194: | Line 192: | ||
+ | {{navigation HDL User Guide# |