This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:docs:axi_pwm_gen [11 Oct 2021 15:12] – Edit next page to be Using and modifying the HDL design Iulia Moldovan | resources:fpga:docs:axi_pwm_gen [13 Oct 2021 10:07] – Edit footer & title Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
The axi_pwm_gen core is used to generate a maximum of four configurable signals(pwms). The pulses are generated according to the state of a counter, one counter for each pulse. | The axi_pwm_gen core is used to generate a maximum of four configurable signals(pwms). The pulses are generated according to the state of a counter, one counter for each pulse. | ||
- | Features: | + | |
+ | ===== Features | ||
- up to four configurable signals(period, | - up to four configurable signals(period, | ||
- external synchronization | - external synchronization | ||
Line 12: | Line 14: | ||
The axi_pwm_gen core can be synchronized by an external signal. The offset counter will wait for a high to low transition of the synchronization pulse. If another synchronization is needed, the external_sync signal should be set high and the load_config should be toggled(by register write). This will cause the counters to wait for another external_sync high to low transition. | The axi_pwm_gen core can be synchronized by an external signal. The offset counter will wait for a high to low transition of the synchronization pulse. If another synchronization is needed, the external_sync signal should be set high and the load_config should be toggled(by register write). This will cause the counters to wait for another external_sync high to low transition. | ||
To disable a pwm, write 0 to it's period register. | To disable a pwm, write 0 to it's period register. | ||
+ | |||
+ | |||
+ | ===== Block Diagram ===== | ||
{{ : | {{ : | ||
- | ==== Configuration | + | |
+ | ===== Configuration | ||
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ | ||
Line 36: | Line 42: | ||
| '' | | '' | ||
- | ==== Signal and Interface Pins ==== | + | |
+ | ===== Signal and Interface Pins ===== | ||
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
Line 69: | Line 76: | ||
{{ : | {{ : | ||
+ | |||
===== Register map ===== | ===== Register map ===== | ||
Line 114: | Line 122: | ||
^Tue Mar 30 10:21:25 2021 ^^^^^^ | ^Tue Mar 30 10:21:25 2021 ^^^^^^ | ||
- | + | {{navigation | |
- | {{navigation #axi_ip|AXI IP#hdl|Main page# | + |