Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:docs:axi_ad7616 [11 Oct 2021 15:09] – Add footer Iulia Moldovan | resources:fpga:docs:axi_ad7616 [25 Apr 2023 09:34] (current) – Edit according to template Iulia Moldovan |
---|
===== AXI_AD7616 IP core ===== | ====== AXI_AD7616 ====== |
| |
The [[https://github.com/analogdevicesinc/hdl/tree/master/library/axi_ad7616|axi_ad7616]] IP core can be used to interface the [[adi>AD7616]] device using an FPGA. The core has a AXI Memory Map interface for configuration, supports both the serial and parallel data interface of the device, and has a simple FIFO interface for the DMAC. | ===== Overview ===== |
| |
==== AXI_AD7616 with Serial Interface ==== | The [[https://github.com/analogdevicesinc/hdl/tree/master/library/axi_ad7616|axi_ad7616]] IP core can be used to interface the [[adi>AD7616]] device using an FPGA. The core has a AXI Memory Map interface for configuration, supports the parallel data interface of the device, and has a simple FIFO interface for the DMAC. \\ |
{{:resources:fpga:docs:axi_ad7616_ser_v2.svg|AXI_AD7616 with Serial Interface}} | \\ |
| More about the generic framework interfacing ADCs can be read here: [[:resources:fpga:docs:axi_adc_ip]]. |
| |
==== AXI_AD7616 with Parallel Interface ==== | |
{{:resources:fpga:docs:axi_ad7616_par_v2.svg|AXI_AD7616 with Parallel Interface}} | |
| |
==== Configuration Parameter ==== | ===== Parallel interface ===== |
| |
| {{:resources:fpga:docs:axi_ad7616_ip.svg|AXI_AD7616 with Parallel Interface}} |
| |
| |
| ===== Configuration parameter ===== |
| |
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ |
| ''ID'' | Core ID, it can be used in case of multiple cores on a system | 0 | | | ''ID'' | Core ID, it can be used in case of multiple cores on a system | 0 | |
| ''IF_TYPE'' | If **0** the **SERIAL** interface is active, otherwise the **PARALLEL** | 0 | | |
| |
| |
==== Signal and Interface Pins ==== | ===== Interface signals ===== |
| |
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ |
| ''rx_serial'' | **A 3-wire serial interface with two SDI line** ||| | |
| | ''rx_sclk'' |''output'' | Clock | | |
| | ''rx_cs_n'' |''output'' | Chip select | | |
| | ''rx_sdo'' |''output'' | Serial data out | | |
| | ''rx_sdi_0'' |''input'' | First serial data in | | |
| | ''rx_sdi_1'' |''input'' | Second serial data in | | |
| ''rx_parallel'' | **Parallel interface** ||| | | ''rx_parallel'' | **Parallel interface** ||| |
| | ''rx_db_o'' |''output[15:0]'' | Parallel data out | | | | ''rx_db_o'' |''output[15:0]'' | Parallel data out | |
| | ''rx_rd_n'' |''output'' | Active low parallel data read control | | | | ''rx_rd_n'' |''output'' | Active low parallel data read control | |
| | ''rx_wr_n'' |''output'' | Active low parallel data write control | | | | ''rx_wr_n'' |''output'' | Active low parallel data write control | |
| | | ''rx_cs_n'' |''output'' | Active low chip select | |
| ''rx_control'' | **Control interface** | | | ''rx_control'' | **Control interface** | |
| | ''rx_cnvst'' |''output'' | Conversion start signal | | | | ''rx_trigger '' |''input'' | End of conversion signal | |
| | ''rx_busy'' |''input'' | Conversion ready signal | | |
| ''s_axi_*'' | **AXI Slave Memory Map interface** ||| | | ''s_axi_*'' | **AXI Slave Memory Map interface** ||| |
| ''adc_fifo'' | **Write FIFO interface for the DMAC** ||| | | ''adc_fifo'' | **Write FIFO interface for the DMAC** ||| |
| | ''adc_valid'' | ''output'' | Shows when a valid data is available on the bus | | | | ''adc_valid'' | ''output'' | Shows when a valid data is available on the bus | |
| | ''adc_data'' | ''output[15:0]'' | Data bus | | | | ''adc_data'' | ''output[15:0]'' | Data bus | |
| | ''adc_sync'' | ''outpu'' | Shows the first valid beat on a sequence | | | | ''adc_sync'' | ''output'' | Shows the first valid beat on a sequence | |
| ''irq'' | IRQ signal from the SPI engine ||| | | ''irq'' | IRQ signal ||| |
| |
==== Memory Map Registers ==== | |
| |
If the SPI engine is active from offset **0x0000** can be found the [[/resources/fpga/peripherals/spi_engine/axi#register_map|SPI engine memory space]]. | |
| |
The following register space is active in both PARALLEL and SERIAL mode. | ===== Register map ===== |
| |
|< 100% 5% 5% 5% 25% 5% 55% >| | |< 100% 5% 5% 5% 25% 5% 55% >| |
^0x0102 ^0x0408 ^REG_SCRATCH ^^^Version and Scratch Registers ^ | ^0x0102 ^0x0408 ^REG_SCRATCH ^^^Version and Scratch Registers ^ |
| | |[31:0] |SCRATCH[31:0] |RW |Scratch register. | | | | |[31:0] |SCRATCH[31:0] |RW |Scratch register. | |
^0x0103 ^0x040C ^REG_IF_TYPE ^^^ADC Interface Control & Status ^ | |
| | |[31:0] |IF_TYPE |RO | Actual interface type, if **0** SERIAL interface is active, PARALLEL otherwise | | |
^0x0110 ^0x0440 ^REG_UP_CNTRL ^^^ADC Interface Control & Status ^ | ^0x0110 ^0x0440 ^REG_UP_CNTRL ^^^ADC Interface Control & Status ^ |
| | |[0] |RESETN |RW | Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. | | | | |[0] |RESETN |RW | Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. | |
| |
| |
{{navigation #axi_ip|AXI IP#hdl|Main page#tips|Using and modifying the HDL design}} | {{navigation HDL User Guide#ip_cores|IP cores#hdl|Main page#tips|Using and modifying the HDL design}} |