This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:altera:ced1z:common_troubleshooting [30 Nov 2011 15:41] – Moved title to the main page so the table of content to be generated correctly Adrian Costina | resources:fpga:altera:ced1z:common_troubleshooting [25 May 2012 12:43] (current) – Added the "More information" section Andrei Cozma | ||
---|---|---|---|
Line 3: | Line 3: | ||
* Check that the evaluation board is powered. | * Check that the evaluation board is powered. | ||
* Make sure the USB cable is not connected to the CED1Z. In case it is, disconnect it and reset the board. | * Make sure the USB cable is not connected to the CED1Z. In case it is, disconnect it and reset the board. | ||
- | * Check that the USB Blaster cable is properly connected to the device and to the computer and that the **//USB Blaster Device Driver//** driver is installed correctly. If the deriver | + | * Check that the USB Blaster cable is properly connected to the device and to the computer and that the **//USB Blaster Device Driver//** driver is installed correctly. If the driver |
* In uC-Probe right-click on the **//System Browser//** window select **//Remove Symbols// | * In uC-Probe right-click on the **//System Browser//** window select **//Remove Symbols// | ||
Line 17: | Line 17: | ||
{{ : | {{ : | ||
- | | + | ====== More information ====== |
+ | | ||
+ | |