This shows you the differences between two versions of the page.
resources:fpga:altera:bemicro:common_spi_i2c_console [21 Jun 2013 09:32] – created Istvan Csomortani | resources:fpga:altera:bemicro:common_spi_i2c_console [21 Jun 2013 09:44] (current) – Delete every ucProbe reference, update the address table Istvan Csomortani | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | The lab is delivered together with a set of design files that are used to evaluate the ADI part. The FPGA image that must be loaded into the BeMicroSDK FPGA is included in the design files. This section presents the components included in the FPGA image and also the procedure to load the image into the FPGA. | ||
+ | |||
+ | |||
+ | ===== FPGA Components ===== | ||
+ | |||
+ | The following components are implemented in the FPGA design: | ||
+ | |||
+ | ^ Name ^ Address | ||
+ | | CPU | 800 | - | | ||
+ | | Main PLL | 80 | - | ||
+ | | JTAG UART | 90 | 0 | ||
+ | | EPCS FLASH CONTROLLER | ||
+ | | OnChip RAM | 10000 | - | ||
+ | | LED GPIO | 100 | - | ||
+ | | SPI_0_P0 | ||
+ | | SPI_1_P0 | ||
+ | | GPIO | 2080 | - | ||
+ | | CTRL GPIO | 20A0 | - | ||
+ | | SPI_0_P1 | ||
+ | | SPI_1_P1 | ||
+ | | SYS ID | 40 | - | ||
+ | | TIMER | 60 | 2 | ||
+ | | I2C_0 | C0 | 7 | ||
+ | | I2C_1 | E0 | 8 | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ===== Load the FPGA Image ===== | ||
+ | |||
+ | To load the FPGA image the following steps must be performed: | ||
+ | * Plug in the **BeMicroSDK** Stick into a USB port | ||
+ | * Start **Altera Quartus Web edition** and start the programmer by selecting the menu option // | ||
+ | * Select **//Add File//** and select the file **// | ||
+ | * Check the // | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | After finishing, the image is permanently loaded to the configuration Flash and the system will start with a | ||
+ | blinking LED after reset or power up. | ||