Wiki

This version (21 Jun 2013 09:45) was approved by Istvan Csomortani.

The lab is delivered together with a set of design files that are used to evaluate the ADI part. The FPGA image that must be loaded into the BeMicroSDK FPGA is included in the design files. This section presents the components included in the FPGA image and also the procedure to load the image into the FPGA.

FPGA Components

The following components are implemented in the FPGA design:

Name Address IRQ
CPU 800 -
Main PLL 80 -
JTAG UART 90 0
EPCS FLASH CONTROLLER 1800 1
OnChip RAM 10000 -
LED GPIO 100 -
SPI_0_P0 2000 3
SPI_1_P0 2040 5
GPIO 2080 -
CTRL GPIO 20A0 -
SPI_0_P1 0 4
SPI_1_P1 20 6
SYS ID 40 -
TIMER 60 2
I2C_0 C0 7
I2C_1 E0 8

Load the FPGA Image

To load the FPGA image the following steps must be performed:

  • Plug in the BeMicroSDK Stick into a USB port
  • Start Altera Quartus Web edition and start the programmer by selecting the menu option Tools→Programmer
  • Select Add File and select the file ADIEvalBoardLab/FPGA/SDP1_bemicro2.jic
  • Check the Program/Configure box and press Start

image020.jpg

After finishing, the image is permanently loaded to the configuration Flash and the system will start with a blinking LED after reset or power up.

resources/fpga/altera/bemicro/common_spi_i2c_console.txt · Last modified: 21 Jun 2013 09:44 by Istvan Csomortani