Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:eval:user-guides:rpd-6lowpan [14 Aug 2018 11:56] – created Pranit Jadhavresources:eval:user-guides:rpd-6lowpan [24 Sep 2018 05:42] (current) – [Rapid-6LoWPAN Wireless Networking Protocol Solution] Pranit Jadhav
Line 1: Line 1:
-====== EV-6LOWPAN-900Z User Guide ======+====== Rapid-6LoWPAN Wireless Networking Protocol Solution ====== 
 +Analog Devices offers Rapid RapidNet IP Protocol—a long range sub-GHz wireless networking solution that leverages the market proven ADF7023 radio transceiver and lowest power ULP processors (ADuCM3029 or ADuCM4050). 
 +RapidNet IP Protocol uses star-repeater network topology, targeting commercial and industrial applications such as Electronic Shelf Label (ESL), Smart Lock and Structural Health Monitoring (SHM). 
 + 
 +{{ :resources:eval:user-guides:rpd-6lowpan:rapid-6lowpan-network-topology.jpg?nolink&600 |}} 
 +===== Features and Specification ===== 
 +  * Efficient low power network 
 +        *  Low power IEEE802.15.4g/e wireless network with time synchronized channel hopping (TSCH)—no collisions and no lengthy receive waits 
 +        * Lowest power consumption per node with star and extended star network topology configuration. 
 +        * Reliable end-to-end communications with acknowledgements 
 +  * Long range 
 +       * Typical range of 500 m (2 hop and confguration setting dependent) 
 +  * Data rate and frequency 
 +        High throughput (4 pks/sec at 1 kB per packet) 
 +        Fast network join time (for example, 256 motes in 47 sec) 
 +        Low latency—minimum of 5 sec network loop cycle 
 +        ISM frequency band support (433,868,915,920 MHz) 
 +        Multiple data rate support (37.5 kbps to 300 kbps) 
 +        On-demand bandwidth allocation (for example, up to 1 MB per node/1 hr) 
 +  * Supported modes: 
 +       * Master mode (on-chip applications) 
 +       * Slave mode (application coprocessor) 
 +  * Current consumption: 
 +       * Active: <10 µA ave. (3 updates of 1 kB packets/day case) 
 +       * Sleep: <1.5 µA 
 +  * FCC and ARIB STD T108 regulation test feature support integrated 
 +  * Supports OTA (over-the-air) update 
 +  * Reliable scheduling of alert messages from any or all motes 
 +  * Gateway software available for Linux® or ADuCM4050 with various backhaul connectivity options 
 + 
 +===== Evaluation Kit ===== 
 + 
 +Below are the different kits available for evaluating Rapid-6LoWPAN. 
 +  - EV-RAPDID-ESL-900Z - RapidNet IP Evaluation Kit for all the regions except Japan. 
 +  - EV-RAPDID-ESL-900JZ -RapidNet IP  Evaluation kit with TELEC Certification specific for Japan. 
 +  - EV-RAPDID-NODE-900Z- Electronic Shelf Labelling node which should be ordered only if more nodes are required during the evaluation of EV-RAPID-ESL-900Z. 
 + 
 +Below are the kit contents. 
 +  - EV-RAPDID-ESL-900Z / EV-RAPDID-ESL-900jZ  
 +     * [[resources:eval:user-guides:ev-cog-ad3029lz|EV-COG-AD3029LZ]] - development platform for Analog Devices Ultra Low Power Microcontroller [[adi>ADuCM3029]] 
 +     * [[resources:eval:user-guides:ev-dng-rfmod-9001z|EV-DNG-RFMOD-9001Z]] - USB Dongle which acts as Border Router for RapidNet IP Network **(902-958MHz)** 
 +     * [[resources:eval:user-guides:ev-cog-adf7023-9z|EV-COG-ADF7023-9Z]] - [[adi>ADF7023-J]] Connectivity Cog **(902-958MHz)** 
 +     * [[resources:eval:user-guides:ev-gear-eink1z|EV-GEAR-EINK1Z]] - Cog Ecosystem Gear with E-Paper Display from E-INK. 
 +  - EV-RAPDID-NODE-900Z 
 +     * [[resources:eval:user-guides:ev-cog-ad3029lz|EV-COG-AD3029LZ]] - development platform for Analog Devices Ultra Low Power Microcontroller [[adi>ADuCM3029]] 
 +     * [[resources:eval:user-guides:ev-cog-adf7023-9z|EV-COG-ADF7023-9Z]] - [[adi>ADF7023-J]]  Connectivity Cog **(902-958MHz)** 
 +     * [[resources:eval:user-guides:ev-gear-eink1z|EV-GEAR-EINK1Z]] - Cog Ecosystem Gear with E-Paper Display from E-INK. 
 + 
  
resources/eval/user-guides/rpd-6lowpan.txt · Last modified: 24 Sep 2018 05:42 by Pranit Jadhav