Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:inertial-mems:imu:adis16acl1-pcb [10 Dec 2016 00:37] – [OVERVIEW] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16acl1-pcb [13 Dec 2016 16:07] (current) – [OVERVIEW] Mark Looney |
---|
====== ADIS16ACL1/PCBZ Breakout Board Wiki-Guide ====== | ====== ADIS16ACL1/PCBZ Breakout Board Wiki-Guide ====== |
===== OVERVIEW ===== | ===== OVERVIEW ===== |
The ADIS16210 and ADIS16228 products use a 15-pin flexible interface. The mating connector for their interface supports surface-mount solder attachment but does not support direct attachment with ribbon cables. For those who are would like to connect the ADIS16210 and ADIS16228 to an existing processor board, using a ribbon cable, the ADIS16ACL1/PCBZ provides a simple connector translation for this purpose. | The ADIS16ACL1/PCBZ is the breakout board for the ADIS16210 and ADIS16228 vibration sensing solutions. This breakout board function helps connect these two products to the EVAL-ADIS2 evaluation system. It also helps connect these products to existing embedded processor platforms. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16acl1-pcb_pic_0000.png?600|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16acl1-pcb_pic_0000.png?600|}} |