Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis1636x [09 Oct 2013 03:15] – [IMU EVALUATION SOFTWARE REVISION HISTORY] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis1636x [09 Jan 2021 00:39] (current) – user interwiki links Robin Getz |
---|
===== PHYSICAL SETUP ===== | ===== PHYSICAL SETUP ===== |
The [[adi>en/mems-sensors/mems-inertial-sensors/adis16362/products/EVAL-ADIS16362/eb.html|ADIS16362/PCBZ]] includes one interface PCB, which requires two M2 or 2-56 machine screws to secure the baseplate to the system printed circuit board. The [[adi>ADIS16362|ADIS16362]] product family is approximately 22 mm × 32 mm × 24 mm and provides a flexible connector interface that enables multiple mounting orientation options. Set the interface PCB aside, as it is not used for connecting the [[adi>ADIS16362|ADIS16362]] to the [[adi>EVAL-ADIS|EVAL-ADIS]]. | The [[adi>en/mems-sensors/mems-inertial-sensors/adis16362/products/EVAL-ADIS16362/eb.html|ADIS16362/PCBZ]] includes one interface PCB, which requires two M2 or 2-56 machine screws to secure the baseplate to the system printed circuit board. The [[adi>ADIS16362|ADIS16362]] product family is approximately 22 mm × 32 mm × 24 mm and provides a flexible connector interface that enables multiple mounting orientation options. Set the interface PCB aside, as it is not used for connecting the [[adi>ADIS16362|ADIS16362]] to the [[adi>EVAL-ADIS|EVAL-ADIS]]. |
| |
| NOTE: The machine screws that come with the [[adi>EVAL-ADIS|EVAL-ADIS]] can have a moderate impact on local magnetic fields. For those who need the best performance out of the magnetometer solution, consider replacing them with machine screws that are made out of aluminum or other non-ferrous materials. |
{{:resources:eval:user-guides:inertial-mems:imu:36x-part-dimensions.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:36x-part-dimensions.png?400|}} |
{{:resources:eval:user-guides:inertial-mems:imu:adis16364bmlz.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16364bmlz.png?400|}} |
==== EXAMPLE EXERCISES ==== | ==== EXAMPLE EXERCISES ==== |
This section currently has no [[adi>ADIS16362|ADIS16362]]-specific content, but the | This section currently has no [[adi>ADIS16362|ADIS16362]]-specific content, but the |
[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. |
| |
| |