Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adcmxl-pc-eval [24 Sep 2019 00:34] – Photo and files updated Mahdi Sadeghi | resources:eval:user-guides:inertial-mems:imu:adcmxl-pc-eval [02 Nov 2021 14:31] (current) – adcmxl_evaluation_rev_2192 Ian Beavers |
---|
=====ADcmXL3021 EVALUATION ON A PERSONAL COMPUTER===== | =====Evaluation of ADcmXL1021-1 (or ADcmXL3021) ON A PC===== |
| |
| |
The **ADCMXL Evaluation Software** enables PC-based evaluation of the ADcmXL3021, using the following hardware: a ADcmXL3021 interface board (ADCMXL_BRKOUT/PCBZ), FX3 Eval iSensor breakout board and a Cypress FX3™ SuperSpeed Explorer Kit. See the picture below for evaluation kit. | |
\\ | |
\\ | |
Installation Guide can be downloaded here: | |
{{ :resources:eval:user-guides:inertial-mems:accelerometers:eval-adcmkit-vibration_evaluation_application_installation_rev_1.pdf | EVAL-ADCMXL KIT INSTALLATION GUIDE}}\\ | |
| |
User Guide can be downloaded here: | The **ADCMXL Evaluation Software** enables PC-based evaluation of the ADcmXL1021-1 and/or ADcmXL3021, using the following hardware: an ADcmXL interface board (ADCMXL_BRKOUT/PCBZ), FX3 Eval iSensor breakout board and a Cypress FX3™ SuperSpeed Explorer Kit. See the picture below for the evaluation kit. |
{{ :resources:eval:user-guides:inertial-mems:accelerometers:eval-adcmkit-vibration_evaluation_user_guide_rev_1.pdf | EVAL-ADCMXL KIT USER GUIDE}}\\ | \\ \\ |
| **ADcmXL3021** is a 3-axis version of z-axis **ADcmXL1021-1**. |
\\ | \\ |
\\ | \\ |
{{:resources:eval:user-guides:inertial-mems:imu:adcmxl3021wikiphoto4web.gif?direct&400|}} | Installation and User Guide can be downloaded here: {{ :resources:eval:user-guides:inertial-mems:imu:eval-adcm_kit-installation_and_user_guide.pdf | Evaluation Kit Installation and User Guide }} |
\\ PICTURE OF ADCMXL EVALUATION SYSTEM: FX3 Board + ADCMXL_BRKOUT/PCBZ\\ | |
\\ | \\ |
{{:resources:eval:user-guides:inertial-mems:imu:adcmxl3021wikiphoto8web.gif?direct&400|}} | \\ |
\\ \\ PICTURE OF ADCMXL EVALUATION SYSTEM: ADCMXL_BRKOUT/PCBZ + ADcmXL3021 Module\\ | {{ :resources:eval:user-guides:inertial-mems:imu:adcmxl3021bmlzx-kit.gif?direct |}} |
| \\ Picture of ADCMXL Evaluation System: FX3 Board + ADCMXL_BRKOUT/PCBZ + ADcmXL3021 (or ADcmXL1021-1) Module. The picture above shows how to connect the evaluation kit.\\ |
| |
ADCMXL_BRKOUT/PCBZ breakout board and rest of the __**EVAL-ADCM**__ evaluation system. The picture above shows how to connect the evaluation kit. | |
\\ | \\ |
\\ === EVALUATION OPTION PART NUMBERS TO ORDER=== | \\ === EVALUATION OPTION PART NUMBERS TO ORDER=== |
\\ | \\ |
The following two options are available to be used to evaluate the ADcmXL3021 and can be ordered by contacting an ADI distributor to place the order. \\ \\ | The following options are available to be used to evaluate the ADcmXL family and can be ordered by contacting an ADI distributor to place the order. \\ \\ |
**ADCMXL_BRKOUT/PCBZ** \\ | **ADCMXL_BRKOUT/PCBZ** \\ |
For simple breakout of the ADcmXL3021 flex tail connector to header pins. \\ NOTE: The ADcmXL3021 module is required to be ordered separately. | For simple breakout of the ADcmXL1021-1 or ADcmXL3021 flex tail connector to header pins. \\ NOTE: The ADcmXL1021-1 (or ADcmXL3021) module is required to be ordered separately. |
| |
**EVAL-ADCM** \\ | **EVAL-ADCM** \\ |
Includes ADCMXL_BRKOUT/PCBZ and additional hardware to use ADI evaluation software. \\ \\ | Evaluation kit for ADcmXL3021, which includes ADCMXL_BRKOUT/PCBZ, the module and additional hardware to use ADI's ADCMXL Evaluation Software. \\ \\ |
| |
| **EVAL-ADCM-1** \\ |
| Evaluation kit for ADcmXL1021-1, which includes ADCMXL_BRKOUT/PCBZ, the module and additional hardware to use ADI's ADCMXL Evaluation Software. \\ \\ |
\\ | \\ |
\\ === EVALUATION OPTIONS DESCRIPTION=== | \\ === EVALUATION OPTIONS DESCRIPTION=== |
\\ | \\ |
The __**ADCMXL_BRKOUT/PCBZ**__ is a breakout board that has a Hirose DF12(3.0)-14DP-05V(86) receptor which accepts the mating connector on the flex tail of the ADcmXL3021 Module. This breaks out the connections from the ADcmXL3021 module to a 16 pin 2mm header connector. This is available as an option in the case that the user has an existing backend available to power, configure and capture directly to the ADcmXL3021 and needs an interface option to connect to the Hirose header without soldering to the module. The 14 pin, 0.5 mm pitch Hirose connector has the pin configuration shown in Figure below. The ADCMXL_BRKOUT/PCBZ silk screen and schematic are available for download using the links below. \\ | The __**ADCMXL_BRKOUT/PCBZ**__ is a breakout board that has a Hirose DF12(3.0)-14DP-05V(86) receptor which accepts the mating connector on the flex tail of the either ADcmXL1021-1 or ADcmXL3021 Module. This breaks out the connections from the ADcmXL1021-1 (or ADcmXL3021) module to a 16 pin 2mm header connector. This is available as an option in the case that the user has an existing backend available to power, configure and capture directly to the ADcmXL1021-1 or ADcmXL3021 and needs an interface option to connect to the Hirose header without soldering to the module. The 14 pin, 0.5 mm pitch Hirose connector has the pin configuration shown in Figure below. The ADCMXL_BRKOUT/PCBZ silk screen and schematic are available for download using the links below. \\ |
\\ | \\ |
{{:resources:eval:user-guides:inertial-mems:adcmxl_brkout_p1pinout.gif?200|}}\\ | {{:resources:eval:user-guides:inertial-mems:adcmxl_brkout_p1pinout.gif?200|}}\\ |
The __**EVAL-ADCM**__ is an orderable kit that includes the evaluation hardware. It includes the following: \\ \\ | The __**EVAL-ADCM**__ is an orderable kit that includes the evaluation hardware. It includes the following: \\ \\ |
- ADcmXL3021 module\\ | - ADcmXL3021 module\\ |
| - ADCMXL_BRKOUT/PCBZ (more details above) \\ |
| - ADcmXL FX3 Interface board \\ |
| - Cypress FX3 Evaluation Kit \\ |
| - Acrylic mounting plate (2”x3”) \\ |
| - 8 Mounting screws (SCREW, PAN HEAD PHILLIPS, M2.5X6MM) \\ |
| - 2” long Ribbon cable, 16 pin conductor, 2mm connector pitch (required for RTS Mode communications link) \\ |
| - 12” long Ribbon cable, 16 pin conductor, 2mm connector pitch \\ |
| |
| The __**EVAL-ADCM-1**__ is an orderable kit that includes the evaluation hardware. It includes the following: \\ \\ |
| - ADcmXL1021-1 module\\ |
- ADCMXL_BRKOUT/PCBZ (more details above) \\ | - ADCMXL_BRKOUT/PCBZ (more details above) \\ |
- ADcmXL FX3 Interface board \\ | - ADcmXL FX3 Interface board \\ |
| |
| |
NOTE: The ADcmXL3021 uses the following Hirose connector and would require the following mating plug: | NOTE: Both ADcmXL1021-1 and ADcmXL3021 use the following Hirose connector and would require the following mating plug: |
DF12(3.0)–14DS–0.5V(86) – Hirose Receptacle – will be used on flex tail of product | DF12(3.0)–14DS–0.5V(86) – Hirose Receptacle – will be used on flex tail of product |
DF12(3.0)–14DP–0.5V(86) – Hirose Plug – to be used on customer boards, test, eval boards, etc. | DF12(3.0)–14DP–0.5V(86) – Hirose Plug – to be used on customer boards, test, eval boards, etc. |
| |
| |
| |
\\ === SOFTWARE TO DOWNLOAD=== | \\ === SOFTWARE TO DOWNLOAD=== |
\\ | \\ |
Vibration Evaluation Software installation only requires two downloads: \\ | ADCMXL Evaluation Software installation requires two downloads: \\ |
1. Download and unzip the file called FX3Driver.zip (click here to see the download link) \\ | 1. Download and unzip the file called FX3Driver.zip (click here to see the download link) \\ |
{{:resources:eval:user-guides:inertial-mems:fx3driver.zip|(click here to download fx3driver.zip)}} \\ | {{ :resources:eval:user-guides:inertial-mems:imu:fx3_driver.zip|(click here to download fx3driver.zip)}} \\ |
2. Run DriverSetup.exe \\ | 2. Run DriverSetup.exe \\ |
3. Download and unzip the file called “Vibration_Evaluation_revision.zip”, where revision is currently identified as “2_1_8_6” \\ | 3. Download and unzip the file called “ADCMXL_Evaluation_revision.zip”, where revision is currently identified as “2192”. This version supports both ADcmXL1021-1 and ADcmXL3021 modules. \\ |
{{ :resources:eval:user-guides:inertial-mems:imu:vibration_evaluation_2_1_8_6.zip |(click here to download Vibration_Evaluation_2_1_8_6.zip)}}\\ | {{ :resources:eval:user-guides:inertial-mems:imu:adcmxl_evaluation_rev_2192.zip |(click here to download adcmxl_evaluation_rev_2192.zip)}}\\ (NOTE: ADCMXL Evaluation Software revisions 2.1.8.6 and higher, need the most recent {{ :resources:eval:user-guides:inertial-mems:imu:fx3_driver.zip|FX3Driver}} to operate.)\\ |
4. Connect the evaluation setup to the computer \\ | 4. Connect the evaluation setup to the computer \\ |
| |