Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [31 Jul 2017 15:19] – Pranit Jadhav | resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [11 Aug 2017 16:21] (current) – [General Description/Overview] Pranit Jadhav |
---|
===== General Description/Overview ===== | ===== General Description/Overview ===== |
| |
The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI>ADuCM4050]] devices. This software layer is the foundation layer needed when writing applications using this microprocessor family. When combined with the **EV-COG-AD4050LZ** software pack as well as the Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the **EV-COG-AD4050LZ** development platform. | The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI>ADuCM4050]] devices. This software layer is the foundation layer needed when writing applications using this microprocessor family. When combined with the **EV-COG-AD4050LZ** software pack as well as the Sensors software pack, there are many great **Internet of Things(IoT)** applications and demos that can be replicated using the **EV-COG-AD4050LZ** development platform. |
| |
The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack: | The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack: |
<WRAP center round help 60%> | <WRAP center round help 60%> |
| |
ADD DFP RELEASE NOTE LINK HERE | [[http://download.analog.com/tools/EZBoards/ADuCM4050/Releases/DeviceFamilyPack/Release_1.0.0/ADuCM4x50_DFP_1.0.0_Release_Notes.pdf | ADuCM4050 DFP 1.0.0 Release Notes]] |
</WRAP> | </WRAP> |
| |
The software pack can be installed directly by the tool chain's CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager's manual installation to install the pack. | The software pack can be installed directly by the tool chain's CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager's manual installation to install the pack. |
- Downloaded via the tool chain's CMSIS pack manager | - Downloaded via the tool chain's CMSIS pack manager |
* It is **recommended** to download the ADuCM4x50 software pack through from the tool chain's CMSIS pack manager. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the ADuCM4x50 software pack through CrossCore Embedded Studio please see our [[resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide#how_to_install_or_upgrade_the_aducm302x_device_family_pack_dfp_for_cces|CrossCore Embedded Studio Quickstart User Guide]]. | * It is **recommended** to download the ADuCM4x50 software pack through from the tool chain's CMSIS pack manager. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the ADuCM4x50 software pack through CrossCore Embedded Studio please see our [[resources:eval:user-guides:eval-cog-ad4050lz:tools:cces_guide|Cross Core Embedded Studio Quickstart User Guide]]. |
- Downloaded to local directory | - Downloaded to local directory |
* However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to "import" the pack file using your tool chain's CMSIS pack manager's import feature. Note that all software packs can be downloaded from Keil's website. | * However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to "import" the pack file using your tool chain's CMSIS pack manager's import feature. Note that all software packs can be downloaded from Keil's website. |
<WRAP round 80% download> | <WRAP round 80% download> |
| |
ADD LNK HERE DFP | [[http://download.analog.com/tools/EZBoards/ADuCM4050/Releases/DeviceFamilyPack/Release_1.0.0/ADuCM4x50_Device_Family_Pack-Rel1.0.0.zip | ADuCM4050_DFP Pack 1.0.0]] |
| |
</WRAP> | </WRAP> |
| |
// End of Document // | // End of Document // |