This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adtf3175d-nxz-upgrade-firmware [05 Jul 2022 15:45] – changed the config file name in the data_collect firmware update example. Andre Straker-Payne | resources:eval:user-guides:eval-adtf3175d-nxz-upgrade-firmware [13 Jul 2022 17:47] – Harshvardhan Bhatia | ||
---|---|---|---|
Line 10: | Line 10: | ||
* Connect camera - ensure camera network is detected by the PC | * Connect camera - ensure camera network is detected by the PC | ||
- | * Run the following command, using the appropriate firmware filename: **data_collect.exe --ip 10.42.0.1 --fw firmware_upgrade_3123.bin tof-viewer_config.json** | + | * Run the following command, using the appropriate firmware filename: |
+ | | ||
{{ : | {{ : | ||
Line 35: | Line 36: | ||
{{ : | {{ : | ||
* Run the following commands to upgrade firmware (replace upgrade_firmware_xxxx.bin with your version) | * Run the following commands to upgrade firmware (replace upgrade_firmware_xxxx.bin with your version) | ||
- | * cd Workspace/ | + | * '' |
- | * ./ | + | * '' |
{{ : | {{ : |