Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:eval-adpaq3029:sw_tools_setup [05 Nov 2018 15:34] – created Sundar Palani | resources:eval:user-guides:eval-adpaq3029:sw_tools_setup [05 Nov 2018 21:42] (current) – created Sundar Palani |
---|
</WRAP> | </WRAP> |
| |
- Open CCES and click on ''Window'' -> ''Perspective'' -> ''Open Perspective'' -> ''Other'', then select ''CMSIS Pack Manger''. | - Open CCES and click on ''Window'' -> ''Perspective'' -> ''Open Perspective'' -> ''Other'', then select ''CMSIS Pack Manger''. {{ :resources:eval:user-guides:eval-adpaq3029:sw3.png?linkonly | image1}} {{ :resources:eval:user-guides:eval-adpaq3029:sw4.png?linkonly |image2}} |
- Now close the Welcome Window and click on ''Check for Updates on Web''. | - Now close the Welcome Window and click on ''Check for Updates on Web''. {{ :resources:eval:user-guides:eval-adpaq3029:sw5.png?linkonly |image}} |
- Now select ADuCM3029 from the Devices list. | - Now select ADuCM3029 from the Devices list.{{ :resources:eval:user-guides:eval-adpaq3029:sw6.png?linkonly |image}} |
- In ''Packs'' -> ''Generic'' folder, install ''ARM CMSIS version 5.0.1''. | - In ''Packs'' -> ''Generic'' folder, install ''ARM CMSIS version 5.0.1''.{{ :resources:eval:user-guides:eval-adpaq3029:sw7.png?linkonly |image}} |
- Now click on ''import existing packs'' and add the BSP and Device family packs downloaded from Starweb link provided above. | - Now click on ''import existing packs'' and add the BSP and Device family packs downloaded from Starweb link provided above.{{ :resources:eval:user-guides:eval-adpaq3029:sw8.png?linkonly |image}} |
- Ensure that you delete the default ''DFP'' -> ''Analog Devices ADuCM302x_DFP version 2.0.0''. | - Ensure that you delete the default ''DFP'' -> ''Analog Devices ADuCM302x_DFP version 2.0.0''.{{ :resources:eval:user-guides:eval-adpaq3029:sw9.png?linkonly |image}} |
| |
The CCES is now ready for ADPAQ development. | The CCES is now ready for ADPAQ firmware development which is explained [[.:fw_dev|here]]. |
| |
=====mbed Serial port driver===== | =====mbed Serial port driver===== |
The CrossCore Embedded Studio installer will also install the mBed windows serial driver. | The CrossCore Embedded Studio installer will also install the mBed windows serial driver. |
Check by going to ''Device manager'' -> ''Ports (COM and LPT)'', mbed Serial Port should be visible under the ''Ports''. | Check by going to ''Device manager'' -> ''Ports (COM and LPT)'', ''mbed Serial Port'' should be visible under ''Ports''. {{ :resources:eval:user-guides:eval-adpaq3029:sw15.png?linkonly |image}} |
* If not, it can be installed separately by going to - https://developer.mbed.org/handbook/Windows-serial-configuration | * If not, it can be installed separately by going to - https://developer.mbed.org/handbook/Windows-serial-configuration {{ :resources:eval:user-guides:eval-adpaq3029:sw16.png?linkonly |image}} |
* open device manager to check mbed serial port is visible again. | * open device manager to check mbed serial port is visible again. |
| |