The CCES software development environment for EVAL-ADPAQ3029 is based on open source tools, and is maintained by Analog Devices. CCES includes support for DSP (digital signal processing) and ARM Cortex M- and A- devices, and includes the following features and many more:
CrossCore Embedded Studio is based on Eclipse, but because the MBED platform provides a CMSIS-DAP interface to connect to the board, the EVAL-ADPAQ3029 can be used without problems with IAR Embedded Workbench IDE or Keil µVision IDE as well.
To install CrossCore Embedded Studio, double-click ADI_CrossCoreEmbeddedStudio-Rel2.8.0.exe
All the tools will be installed in local directory C:\Analog Devices\CrossCore Embedded Studio 2.8.0\
It is recommended to install the version 2.6.0 and above, since all the sample applications provided here are validated on 2.6.0 version.
CrossCore Embedded Studio can be installed and used on Ubuntu 14.04+ 32-bit and 64-bit.
$> sudo dpkg --add-architecture i386 && apt-get update $> sudo apt-get install -y libc6:i386 libncurses5:i386 libstdc++6:i386 libgtk2.0-0:i386 libxtst6:i386 gtk2-engines-murrine:i386 libcanberra-gtk-module:i386 gtk2-engines:i386 libpng-dev:i386 libssl-dev:i386
$> sudo dpkg -i adi-CrossCoreEmbeddedStudio-linux-x86-2.8.0.deb
The Ubuntu Linux Installer(Debian) installs all necessary components to local directory /opt/analog/
.
The first time you launch CCES, you will be prompted to input a serial number, name, and email address. A full license can be purchased from here. To know more about acquiring, activating and managing licenses, see the manual here.
The New License Wizard will guide you through the process.
CCES does not come with the Analog Device specific packs or the ARM CMSIS Pack file pre-installed. Download the device family pack from the link below.
Download ADuCM3029 IoT Device Family pack
Check for Updates on Web
. imageimport existing packs
and add the BSP and Device family packs downloaded from Starweb link provided above.imageThe CCES is now ready for ADPAQ firmware development which is explained here.
The CrossCore Embedded Studio installer will also install the mBed windows serial driver.
Check by going to Device manager
→ Ports (COM and LPT)
, mbed Serial Port
should be visible under Ports
. image