This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0398 [03 Jan 2021 21:46] – fix links Robin Getz | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0398 [14 Jan 2021 05:24] – use / interwiki links Robin Getz | ||
---|---|---|---|
Line 122: | Line 122: | ||
- Connect the **EVAL-CN0398-ARDZ** to the Arduino connectors **P2, P5, P6, P7, P8** of the **EVAL-ADICUP360** board. | - Connect the **EVAL-CN0398-ARDZ** to the Arduino connectors **P2, P5, P6, P7, P8** of the **EVAL-ADICUP360** board. | ||
- Connect the pH sensor to the **J1** connector of the EVAL-CN0398-ARDZ. | - Connect the pH sensor to the **J1** connector of the EVAL-CN0398-ARDZ. | ||
- | - Connect the RTD sensor to the **P1** connector of the EVAL-CN0398-ARDZ.[[https:// | + | - Connect the RTD sensor to the **P1** connector of the EVAL-CN0398-ARDZ.[[/ |
- | - Connect the moisture sensor to the **P2** connector of the EVAL-CN0398-ARDZ.[[https:// | + | - Connect the moisture sensor to the **P2** connector of the EVAL-CN0398-ARDZ.[[/ |
<note important> | <note important> | ||
- Set the jumpers on the **EVAL-CN0398-ARDZ** to the position shown below. | - Set the jumpers on the **EVAL-CN0398-ARDZ** to the position shown below. | ||
Line 143: | Line 143: | ||
<WRAP center round info 80%> | <WRAP center round info 80%> | ||
- | For more information on importing, debugging, or other tools related questions, please see the [[https:// | + | For more information on importing, debugging, or other tools related questions, please see the [[/ |
</ | </ | ||