This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adxl355 [14 Jan 2021 05:23] – use / interwiki links Robin Getz | resources:eval:user-guides:eval-adicup360:reference_designs:demo_adxl355 [14 Mar 2021 05:54] – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 46: | Line 46: | ||
- Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the **User USB**.(P13) | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the **User USB**.(P13) | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM360_demo_adxl355_pmdz** can be found on Github: | + | Importing the project into CrossCore is going to allow you to change parameters |
+ | |||
+ | The software for the **ADuCM360_demo_adxl355** demo can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | \\ | + | Prebuilt ADXL355 Bin File |
- | CrossCore Embedded Studio Application Source Code: | + | * [[https:// |
- | \\ | + | Complete ADXL355 Source Files |
- | \\ | + | |
- | [[https:// | + | |
</ | </ | ||
+ | |||
<WRAP center round info 80%> | <WRAP center round info 80%> |