This is an old revision of the document!
The circuit below is an arduino compatible, single supply 16-bit volatile organic compound detector using a metal oxide sensor. It uses ADN8810 to precisely control the current running through the sensor to get to within the 1% voltage accuracy needed for the heating element of the sensor.
CN0395 measures indoor air quality by utilizing a Metal Oxide Sensor to detect gases composed of volatile organic compounds. The sensor is composed of a heating resistor and a sensing resistor. When the sense resistor is heated its value changes as a function of the concentrations of different gasses.
P2 header selects the current path from the current output DAC, ADN8810. It is populated across RH+ by default.
Silkscreen | Current Path | Pins |
RCAL1 | 71.5Ω | 1 & 2 |
RCAL1 | 10.0Ω | 3 & 4 |
RH+ | Heating Resistor | 5 & 6 |
A jumper is placed across pins 2 & 3 or GND, as default to maintain the performance specifications of ADN8810.
CN0395 has the TGS8100 on board as default. Using a different set of sensors require a recalculation and replacement of the sense resistors that sets the full scale current for the device. Provision for alphasense sensors or with similar footprint is available and a screw terminal is also in place for any other types of sensors.
Recommended Sensors
Spacers that could cater various surface mount and through hole packages are available on the board to make some modifications on the board easier.
Resistor spacers, R17_SPACER and R19_SPACER, are used to hold the sense resistors to select the maximum output current of the ADN8810. Changing these maximum output current of the ADN8810 allows the board to cater multiple types of sensor that use up to 300mA of current for measurements.
Sense resistors can be calculated by using the formula below:
EVAL-CN0395-ARDZ Design & Integration Files