This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:cn0394 [30 Sep 2016 08:37] – Robert Lee | resources:eval:user-guides:eval-adicup360:hardware:cn0394 [29 Jul 2021 05:17] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== EVAL-CN0391-ARDZ Shield | + | ====== EVAL-CN0394-ARDZ Shield ====== |
+ | |||
+ | ===== Overview ===== | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | {{ : | ||
- | [[ADI> | ||
===== Equipment ===== | ===== Equipment ===== | ||
- | ====== General Setup ====== | + | * EVAL-CN0394-ARDZ Circuit Evaluation Board |
- | + | * [[adi> | |
- | ===== Test Setup Functional Block Diagram | + | * Any combination of B, E, J, K, N, R, S, T type thermocouples (total of 4) |
+ | * PC with Microsoft Windows 7 64-bit or later and USB 2.0 port or higher | ||
+ | * Serial terminal software | ||
+ | * Such as Putty or Tera Term | ||
+ | |||
+ | ===== General Setup ===== | ||
+ | |||
+ | * Connect the EVAL-CN0394-ARDZ to EVAL-ADICUP360 board | ||
+ | * Connect 4 thermocouples to EVAL-CN0394-ARDZ **P1~P4**, marked on PCB with **CH0~CH3** | ||
+ | * Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | ||
+ | |||
+ | ===== Connectors and Configurations | ||
+ | |||
+ | ==== Thermocouple Connectors ==== | ||
+ | |||
+ | Each of the four(4) channels uses an Omega style connector for the thermocouples, | ||
+ | |||
+ | There is an RTD beneath the copper tabs of each connector which is used to measure the cold junction temperature. | ||
+ | |||
+ | ==== Analog Sensor Inputs | ||
+ | |||
+ | The analog outputs of each thermocouple channel and each RTD channel are connected directly to connector P6. Each of these analog voltages is passed directly to the ADuCM360 on the EVAL-ADICUP360 board. | ||
+ | |||
+ | ^ P6 Pin Connections ^ Sensor/ | ||
+ | | Pin 1 | Thermocouple+ (P1) | | ||
+ | | Pin 2 | Thermocouple+ (P2) | | ||
+ | | Pin 3 | Thermocouple+ (P3) | | ||
+ | | Pin 4 | Thermocouple+ (P4) | | ||
+ | | Pin 5 | RTD Output (R1) | | ||
+ | | Pin 6 | RTD Output (R2) | | ||
+ | | Pin 7 | RTD Output (R3) | | ||
+ | | Pin 8 | RTD Output (R4) | | ||
+ | |||
+ | ^ P7 Pin Connections ^ Sensor/ | ||
+ | | Pin 1 | RTD Common | | ||
+ | | Pin 4 | Thermocouple Common (-) | | ||
+ | | Pin 7 | Voltage Reference | | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials | ||
- | ====== Connectors and Jumper Configurations ====== | ||
- | | ||
- | ===== Chip Select ===== | ||
- | |||
- | ====== Schematic, PCB Layout, Bill of Materials ====== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[www.analog.com/ | + | EVAL-CN0394-ARDZ Design & Integration Files |
- | * Schematics | + | * {{: |
- | * PCB Layout | + | * {{: |
- | * Bill of Materials | + | * {{: |
- | * Allegro Project | + | * {{: |
</ | </ | ||
- | ====== Software | + | ===== Software ===== |
- | * [[resources: | + | * [[resources: |
- | * AduCM360 | + | * ADuCM360 |
* [[https:// | * [[https:// | ||
- | |||
{{navigation EVAL-ADICUP360# | {{navigation EVAL-ADICUP360# | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
+ | |||
+ | // End of Document // | ||
+ | |||
+ |