This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:adt7420 [24 May 2017 19:47] – Brandon Bushey | resources:eval:user-guides:eval-adicup360:hardware:adt7420 [03 Mar 2023 07:48] (current) – updated the design files download link Joyce Velasco | ||
---|---|---|---|
Line 5: | Line 5: | ||
The ADT7420 is guaranteed to operate over supply voltages from 2.7 V to 5.5 V. Operating at 3.3 V, the average supply current is typically 210 μA. The ADT7420 has a shutdown mode that powers down the device and offers a shutdown current of typically 2.0 μA at 3.3 V. The ADT7420 is rated for operation over the −40°C to +150°C temperature range. | The ADT7420 is guaranteed to operate over supply voltages from 2.7 V to 5.5 V. Operating at 3.3 V, the average supply current is typically 210 μA. The ADT7420 has a shutdown mode that powers down the device and offers a shutdown current of typically 2.0 μA at 3.3 V. The ADT7420 is rated for operation over the −40°C to +150°C temperature range. | ||
- | Pin A0 and Pin A1 are available for address selection, giving the ADT7420 four possible I2C addresses. The CT pin is an open-drain output that becomes active when the temperature exceeds a programmable critical temperature limit. The INT pin is also an open-drain output that becomes active when the temperature exceeds a programmable limit. The INT pin and CT pin can operate in comparator and interrupt event modes. | + | Pin A0 and Pin A1 are available for address selection, giving the ADT7420 four possible I2C addresses. The CT pin is an open-drain output that becomes active when the temperature exceeds a programmable critical temperature limit. The INT pin is also an open-drain output that becomes active when the temperature exceeds a programmable limit. The INT pin and CT pin can operate in comparator and interrupt event modes. |
{{ : | {{ : | ||
Line 11: | Line 11: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | The PMOD board is small in size with dimensions approximately 1 inch in width by 1 inches | + | The PMOD board is small in size with dimensions approximately 1 inch in width by 1 inch in length. |
==== Power Supply Requirements ==== | ==== Power Supply Requirements ==== | ||
Line 24: | Line 24: | ||
The PMOD interface is a series of standardized digital interfaces for various digital communication protocols such as SPI, I2C, and UART. These interface types were standardized by Digilent, which is now a division of National Instruments. | The PMOD interface is a series of standardized digital interfaces for various digital communication protocols such as SPI, I2C, and UART. These interface types were standardized by Digilent, which is now a division of National Instruments. | ||
- | The specific interface used for the EVAL-ADT7420-PMDZ boards is the extended I2C. In general ADI has adopted the extended I2C connector for all PMOD devices which have an I2C interface. | + | The specific interface used for the EVAL-ADT7420-PMDZ boards is the extended I2C. In general, ADI has adopted the extended I2C connector for all PMOD devices which have an I2C interface. |
^ P1 Pin Number ^ Pin Function ^ Mnemonic ^ | ^ P1 Pin Number ^ Pin Function ^ Mnemonic ^ | ||
Line 61: | Line 61: | ||
{{ : | {{ : | ||
\\ \\ | \\ \\ | ||
- | The temperatures are software configurable, | + | The temperatures are software configurable, |
- | ===== Software | + | ===== Software |
* [[resources: | * [[resources: | ||
Line 70: | Line 70: | ||
===== Schematics, PCB Layout, Bill of Materials ===== | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematic | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * Allegro Project | ||
+ | </ | ||
- | * {{: | + | =====Registration===== |
- | * {{: | + | <WRAP round tip 80% > |
- | * {{: | + | Receive software update notifications, |
- | * {{: | + | |
- | + | ||
- | </ | + | |
// End of Document // | // End of Document // |