This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:adt7420 [20 Dec 2016 22:04] – Brandon Bushey | resources:eval:user-guides:eval-adicup360:hardware:adt7420 [03 Mar 2023 07:48] (current) – updated the design files download link Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADT7420 Digital Temperature PMOD ====== | ====== ADT7420 Digital Temperature PMOD ====== | ||
- | The ADT7420 is a high accuracy digital temperature sensor offering breakthrough performance over a wide industrial range. It contains an internal band gap reference, a temperature sensor, and a 16-bit ADC to monitor and digitize the temperature to 0.0078°C resolution. The ADC resolution, by default, is set to 13 bits (0.0625°C). The ADC resolution is a user programmable mode that can be changed through the serial interface. | + | The [[ADI>ADT7420]] is a high accuracy digital temperature sensor offering breakthrough performance over a wide industrial range. It contains an internal band gap reference, a temperature sensor, and a 16-bit ADC to monitor and digitize the temperature to 0.0078°C resolution. The ADC resolution, by default, is set to 13 bits (0.0625°C). The ADC resolution is a user programmable mode that can be changed through the serial interface. |
The ADT7420 is guaranteed to operate over supply voltages from 2.7 V to 5.5 V. Operating at 3.3 V, the average supply current is typically 210 μA. The ADT7420 has a shutdown mode that powers down the device and offers a shutdown current of typically 2.0 μA at 3.3 V. The ADT7420 is rated for operation over the −40°C to +150°C temperature range. | The ADT7420 is guaranteed to operate over supply voltages from 2.7 V to 5.5 V. Operating at 3.3 V, the average supply current is typically 210 μA. The ADT7420 has a shutdown mode that powers down the device and offers a shutdown current of typically 2.0 μA at 3.3 V. The ADT7420 is rated for operation over the −40°C to +150°C temperature range. | ||
- | Pin A0 and Pin A1 are available for address selection, giving the ADT7420 four possible I2C addresses. The CT pin is an open-drain output that becomes active when the temperature exceeds a programmable critical temperature limit. The INT pin is also an open-drain output that becomes active when the temperature exceeds a programmable limit. The INT pin and CT pin can operate in comparator and interrupt event modes. [[http:// | + | Pin A0 and Pin A1 are available for address selection, giving the ADT7420 four possible I2C addresses. The CT pin is an open-drain output that becomes active when the temperature exceeds a programmable critical temperature limit. The INT pin is also an open-drain output that becomes active when the temperature exceeds a programmable limit. The INT pin and CT pin can operate in comparator and interrupt event modes. |
- | {{ : | + | {{ : |
- | \\ | + | |
- | \\ | + | |
- | \\ | + | |
- | \\ | + | |
- | \\ | + | |
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | The PMOD board is small in size with dimensions approximately 1 inch in width by 1 inches | + | The PMOD board is small in size with dimensions approximately 1 inch in width by 1 inch in length. |
==== Power Supply Requirements ==== | ==== Power Supply Requirements ==== | ||
When using the ADT7420 PMOD board, the 3.3V power for the PMOD comes directly from the host board it is connected to. The power from the host is generally capable of providing up to 100 mA at 3.3V, but for complete PMOD power specifications please [[https:// | When using the ADT7420 PMOD board, the 3.3V power for the PMOD comes directly from the host board it is connected to. The power from the host is generally capable of providing up to 100 mA at 3.3V, but for complete PMOD power specifications please [[https:// | ||
+ | |||
+ | The fastest way to tell if the EVAL-ADT7420-PMDZ board is powered is by seeing if the LED on board is illuminated. | ||
+ | {{ : | ||
==== Digital Interface (PMOD) ==== | ==== Digital Interface (PMOD) ==== | ||
Line 26: | Line 24: | ||
The PMOD interface is a series of standardized digital interfaces for various digital communication protocols such as SPI, I2C, and UART. These interface types were standardized by Digilent, which is now a division of National Instruments. | The PMOD interface is a series of standardized digital interfaces for various digital communication protocols such as SPI, I2C, and UART. These interface types were standardized by Digilent, which is now a division of National Instruments. | ||
- | The specific interface used for the EVAL-ADT7420-PMDZ boards is the extended I2C. In general ADI has adopted the extended I2C connector for all PMOD devices which have an I2C interface. | + | The specific interface used for the EVAL-ADT7420-PMDZ boards is the extended I2C. In general, ADI has adopted the extended I2C connector for all PMOD devices which have an I2C interface. |
^ P1 Pin Number ^ Pin Function ^ Mnemonic ^ | ^ P1 Pin Number ^ Pin Function ^ Mnemonic ^ | ||
Line 39: | Line 37: | ||
- | ^ P1 Pin Number ^ Pin Function ^ Mnemonic ^ | + | ===== Jumper Configuration and Solder Links ===== |
- | | Pin 1 | Chip Select | + | |
- | | Pin 2 | Master Out Slave In | MOSI | | + | |
- | | Pin 3 | Master In Slave Out | MISO | | + | |
- | | Pin 4 | Serial Clock | SCLK | | + | |
- | | Pin 5 | Digital Ground | + | |
- | | Pin 6 | Digital Power | VDD | | + | |
- | | Pin 7 | Chip Select | + | |
- | | Pin 8 | Chip Select | | | + | |
- | | Pin 9 | Chip Select | | | + | |
- | | Pin 10 | Chip Select | | | + | |
- | | Pin 11 | Digital Ground | + | |
- | | Pin 12 | Digital Power | VDD | | + | |
- | {{ : | + | The EVAL-ADT7420-PMDZ has some optional modes of operation to increase flexibility when using multiple EVAL-ADT7420-PMDZ boards in a single system and to help alert the Over/ |
- | ===== Getting Started ===== | + | ==== ADT7420 I2C Address Selection Pins ==== |
- | Using the EVAL-ADT7420-PMDZ is very simple. | + | The ADT7420 |
- | * [[http:// | + | |
- | * [[http:// | + | |
- | * A PC or Laptop with a USB port | + | |
- | * USB Cable to micro USB Cable | + | |
- | * A serial terminal program such as Putty or Tera Term | + | |
- | ===== Connectors | + | {{ : |
+ | \\ \\ | ||
+ | If you decide to change the I2C address, then you will need to switch the position of the JP1 and JP2 solder links using the following table. | ||
+ | \\ | ||
+ | ^ JP1 Solder link Position ^ JP2 Solder link Position ^ A1 Logic Level ^ A0 Logic Level ^ I2C Device Address(Hex) ^ | ||
+ | | Pins 2 & 3 Shorted | Pins 2 & 3 Shorted | Low | Low | 0x48 | | ||
+ | | Pins 2 & 3 Shorted | Pins 1 & 2 Shorted | Low | High | 0x49 | | ||
+ | | Pins 1 & 2 Shorted | Pins 2 & 3 Shorted | High | Low | 0x4A | | ||
+ | | Pins 1 & 2 Shorted | Pins 1 & 2 Shorted | High | High | 0x4B | | ||
- | The EVAL-ADT7420-PMDZ has four locations on the board where users can to increase flexibility when stacking systems together. | + | ==== ADT7420 |
- | {{: | + | The ADT7420 has the capability of monitoring temperature and alerting users of Over/Under temperature conditions, as well as Critical temperature events. |
- | \\ | + | {{ : |
- | ==== ADXL_CS_SEL ==== | + | \\ \\ |
- | ^ Configuration ^ Function ^ | + | The temperatures are software configurable, |
- | | {{: | + | |
- | | {{: | + | |
- | \\ | + | ===== Software Examples ===== |
- | ==== LCD_CS_SEL | + | |
- | ^ Configuration ^ Function ^ | + | |
- | | {{: | + | |
- | | {{: | + | |
- | \\ | + | * [[resources: |
- | ==== ADXL_INT_SEL ==== | + | * [[resources: |
- | ^ Configuration ^ Function ^ | + | |
- | | {{:resources: | + | |
- | | {{:resources: | + | |
- | \\ | ||
- | ==== LDC_RST_SEL ==== | ||
- | ^ Configuration ^ Function ^ | ||
- | | {{: | ||
- | | {{: | ||
- | |||
- | \\ | ||
===== Schematics, PCB Layout, Bill of Materials ===== | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | + | [[adi> | |
- | {{: | + | * Schematic |
- | * Schematics | + | * PCB Layout |
- | * PCB Layout | + | * Bill of Materials |
- | * Bill of Materials | + | |
* Allegro Project | * Allegro Project | ||
- | |||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
- | ===== Software examples ===== | + | // End of Document |
- | * [[resources: | + | |
- | + | ||
- | + | ||
- | ==== Evaluation ==== | + | |
- | + | ||
- | <WRAP round 80% download> | + | |
- | [[ftp://ftp.analog.com/pub/ | + | |
- | </ | + | |
- | + | ||
- | + | ||
- | ===== Schematics, PCB Layout, Bill of Materials ===== | + | |
- | <WRAP round 80% download> | + | |
- | + | ||
- | * {{: | + | |
- | * {{: | + | |
- | * {{: | + | |
- | * {{: | + | |
- | + | ||
- | </WRAP> | + |