This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0531 [06 Jan 2021 14:54] – [Obtaining the Source Code] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0531 [05 Mar 2021 06:20] – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 55: | Line 55: | ||
Note that the ' | Note that the ' | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM3029_demo_cn0531** can be found here: | + | Using the drag and drop method, |
- | <WRAP round 80% download> | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | [[https:// | + | The software for the **ADuCM3029_demo_cn0531** can be found here: |
- | {{ :resources: | + | <WRAP round 80% download> |
+ | Prebuilt CN0531 Hex File | ||
+ | * [[https:// | ||
+ | Complete CN0531 Source Files | ||
+ | * [[https:// | ||
</ | </ |