Wiki

This version is outdated by a newer approved version.DiffThis version (05 Mar 2021 06:20) was approved by Zuedmar Arceo.The Previously approved version (06 Jan 2021 14:54) is available.Diff

This is an old revision of the document!


AD5791 PMOD Application with EVAL-ADICUP3029 (w/ EVAL-CN0531-ADRZ)

The ADuCM3029_demo_cn0531 project provides a solution to control a AD5791 DAC PMOD using the EVAL-ADICUP3029. The AD5791 is a high precision, 1ppm, voltage output DAC that can be controlled in this application using a serial UART CLI connected to a host PC.

General Description/Overview

EVAL-CN0531-PMDZ is a minimalist 1 ppm, 20-Bit, ±1 LSB INL, DAC SPI PMOD board suitable for medical instrumentation, test and measurement equipment, industrial control or high end scientific and aerospace instrumentation. Multiple voltage references and power options are available to adapt this module depending on the application. With this module, the user is capable to use the onboard positive voltage reference or to connect external references.

The ADuCM3029_demo_cn0531 project uses this PMOD with the EVAL-ADICUP3029 board to bring up the DAC, control it's internal registers and control it's voltage output. This control is done using a minimalist CLI interface enabled over the UART controller of the board. This CLI can be used by a host PC connected via USB cable to the system.

Demo Requirements

The following is a list of items needed in order to replicate this demo.

  • Hardware
    • EVAL-ADICUP3029
    • EVAL-CN0531-ARDZ
    • Mirco USB to USB cable
    • PC or Laptop with a USB port
  • Software
    • CrossCore Embedded Studio (2.9.1 or higher)
    • ADuCM302x DFP (3.2.0 or higher)
    • ADICUP3029 BSP (1.1.0 or higher)
    • Serial Terminal Program
      • Such as Putty or Tera Term

Setting up the Hardware

  1. Connect EVAL-CN0414-ARDZ board to the EVAL-ADICUP3029.
  2. Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. FIXME - PICTURE

Configuring the Software

Software does not need configuration to work.

Outputting Data

A serial terminal is an application that runs on a PC or laptop that is used to display data and interact with a connected device (including many of the Circuits from the Lab reference designs). The device's UART peripheral is most often connected to a UART to USB interface IC, which appears as a traditional COM port on the host PC/ laptop. (Traditionally, the device's UART port would have been connected to an RS-232 line driver / receiver and connected to the PC via a 9-pin or 25-pin serial port.) There are many open-source applications, and while there are many choices, typically we use one of the following:

Before continuing, please make sure you download and install one of the above programs.

There are several parameters on all serial terminal programs that must be setup properly in order for the PC and the connected device to communicate. Below are the common settings that must match on both the PC side and the connected UART device.

  1. COM Port - This is the physical connection made to your PC or Laptop, typically made through a USB cable but can be any serial communications cable. You can determine the COM port assigned to your device by visiting the device manager on your computer. Another method for identifying which COM port is associated with a USB-based device is to look at which COM ports are present before plugging in your device, then plug in your device, and look for a new COM port.
  2. Baud Rate - This is the speed at which data is being transferred from the connected device to your PC. These parameters must be the same on both devices or data will be corrupted. The default setting for most of the reference designs in 115200.
  3. Data Bits - The number of data bits per transfer. Typically UART transmits ASCII codes back to the serial port so by default this is almost always set to 8-Bits.
  4. Stop Bits - The number of “stop” conditions per transmission. This usually set to 1, but can be set to 2 for redundancy.
  5. Parity - Is a way to check for errors during the UART transmission. Unless otherwise specified, set parity to “none”.
  6. Flow Control - Is a way to ensure that data lose between fast and slow devices on the same UART bus are not lost during transmission. This is typically not implemented in a simple system, and unless otherwise specified, set to “none”.

In many instances there are other options that each of the different serial terminal applications provide, such as local line echo or local line editing, and features like this can be turned on or off depending on your preferences. This setup guide will not go over all the options of each tool, but just the minor features that will make it easier to read back data from the connected devices.

Example setup using Putty

  1. Plug in your connected device using a USB cable or other serial cable.
  2. Wait for the device driver of the connected device to install on your PC or Laptop.
  3. Open your device manager, and find out which COM port was assigned to your device.
  4. Open up your serial terminal program (Putty for this example)
  5. Click on the serial configuration tab or window, and input the settings to match the requirements of your connected device. The default baud rate for most of the reference designs is 115200. Make sure that you use the correct baud rate for your application.
  6. Ensure you click on the checkboxes for Implicit CR in every LF and Implicit LF in every CF.
  7. Ensure that local echo and line editing are enabled, so that you can see what you type and are able to correct mistakes. (Some devices may echo typed characters - if so, you will see each typed character twice. If this happens, turn off local echo.)
  8. Click on the open button, and as long as your connected device and serial terminal program are setup the same, than you should see data displaying.
Hint: If you see nothing in the serial terminal, try hitting the reset button on the embedded development board.

Available commands

Typing help or h after initial calibration sequence will display the list of commands and their short versions. Bellow is the short command list:

Function Command Description Example
General commands
Help h Display available commands.
DAC specific commands
DAC register read drr Read a DAC register.
<addr> = address of the register to be read in hexadecimal.
drr 1 - read register 1
DAC register write drw Write a DAC register.
<addr> = address of the register to be written in hexadecimal.
<val> = value to be written to the register in hexadecimal.
drw 1 18c - set register 1 to 0x18C
DAC set output do Update the DAC output voltage.
<volt> = new voltage value expressed in volts.
do -2.3 - set DAC output to -2.3V

Note that the 'do' command for setting the output voltage works on the assumption that the on board 5V reference is used.

Obtaining the Software

There are two basic ways to program the ADICUP3029 with the software for the CN0531.

  1. Dragging and Dropping the .Hex to the Daplink drive
  2. Building, Compiling, and Debugging using CCES

Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design

Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain.

The software for the ADuCM3029_demo_cn0531 can be found here:

Prebuilt CN0531 Hex File

Complete CN0531 Source Files

How to use the Tools

The official tool we promote for use with the EVAL-ADICUP3029 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.

Importing

For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.

Debugging

For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.

Project Structure

The program is composed of two main parts:

  1. Board setup with initial values.
  2. Main process.

 Main flow chart

Board setup initializes UART and SPI communications and sets the DAC value register to 0. The DAC RBUF bit is also set to 0 to provide the widest voltage range for the application. The DAC output will be between -5V and 5V and coded in two's complement. The coding can be changed to offset binary and the 'do' CLI command will take that into consideration, as it will also take into consideration the RBUF bit. If the RBUF is changed to narrow the output field to 0V - 5V the coding will not change. As such the 0x00000 value of the DAC register will correspond to the middle range value of 2.5V. If not using the 'do' command to change the output, this will have to be taken into consideration.

End of Document

resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0531.1614921639.txt.gz · Last modified: 05 Mar 2021 06:20 by Zuedmar Arceo