This is an old revision of the document!
THE GOAL IS TO CREATE A DOCUMENT CUSTOMERS WILL USE WHEN SETTING UP THEIR CFTL DEMO, SO THEY DON'T ASK YOU SO MANY QUESTIONS. IT'S DESIGNED TO HELP YOU GET STARTED WRITING YOUR REFERENCE DEMO USER GUIDE.
ALL OF THE CONTENT IS PLACEHOLDER INFORMATION, SO YOU WILL NEED TO POPULATE RELEVANT INFORMATION TO YOUR CFTL. SOME(OR SEVERAL) OF THE SECTION HEADERS MAY NOT APPLY TO YOU, SIMPLY REMOVE THEM. ALSO I MAY NOT HAVE CAPTURED EVERYTHING RELATIVE TO YOUR BOARD, SO ADDING INFORMATION IS ACCEPTABLE.
DON'T FORGET TO CREATE A MEDIA FOLDER SPECIFIC TO YOUR DEMO FOR ANY IMAGES, FILES, OR DOCUMENTS YOU WISH TO INCLUDE. THIS WILL HELP US KEEP THE WIKI ORGANIZED AND ENSURE YOUR CONTENT DOESN'T GET REMOVED.
The ADuCM3029_demo_cn0503 project provides a solution to get multiple liquid parameters (for example turbidity, pH, fluorescence, etc.) using the EVAL-CN0503-ARDZ and the EVAL-ADICUP3029. It uses a a complete multimodal sensor front end, stimulating up to eight LEDs and measuring the return signal on up to eight separate current inputs using photo-diodes. The board is controlled via a command line interface (CLI), Python scripts that provide high level functions or a Python GUI that communicates with the firmware via serial terminal.
The ADuCM_demo_cn0503 project uses EVAL-CN0503-ARDZ to provide a method to determine properties of liquids, for example turbidity, fluorescence and pH. To do this the application must configure the ADPD4101 sensor, read the data from it and perform calculations on the data to improve SNR and pre-processes it to units as close to the desired measurement as possible.
The application configures the device to stimulate LEDs and read the PDs in 4 time slots, each corresponding to one of the optical paths present on the board. It enables 2 ADC channels per time slot to measure the light beam before and after passing through the substance. This means that a packet of 8 samples of data come from the ADC once per sampling period.
add diagram
The samples can then be plugged into a user defined equation that can include any of the samples and any random constant to generate a ratio, which the application defines as the 'absolute ratio'. Before being displayed or used any further the absolute ratio is filtered by a block average filter and a rolling average filter to digitally increase the SNR and take out unwanted frequencies. The bandwidth of the rolling average filter can be set by the user. After getting the absolute ratio that describes the liquid that is now in the vat, it can be used to compare it to the baseline measurement using either 1 - (absolute ratio / baseline) or (absolute ratio / baseline) equations. The user has to input the baseline for each optical path as well as the equation from these options. The application defines this result as the 'relative ratio'. The application then has 2 more options of processing the information in the form of two 5th order polynomials in which the relative ratio can be inserted as the variable. The coefficients of each of the polynomial members are also input by the user via the CLI. To be noted that the result of the first equation is the variable for the second equation. This gives the user a high degree of flexibility in getting data out of the platform.
The following is a list of items needed in order to replicate this demo.
The ADuCM3029_demo_cn0503 does not need any software configuration. It can be built and run as is.
A serial terminal is an application that runs on a PC or laptop that is used to display data and interact with a connected device (including many of the Circuits from the Lab reference designs). The device's UART peripheral is most often connected to a UART to USB interface IC, which appears as a traditional COM port on the host PC/ laptop. (Traditionally, the device's UART port would have been connected to an RS-232 line driver / receiver and connected to the PC via a 9-pin or 25-pin serial port.) There are many open-source applications, and while there are many choices, typically we use one of the following:
Before continuing, please make sure you download and install one of the above programs.
There are several parameters on all serial terminal programs that must be setup properly in order for the PC and the connected device to communicate. Below are the common settings that must match on both the PC side and the connected UART device.
In many instances there are other options that each of the different serial terminal applications provide, such as local line echo or local line editing, and features like this can be turned on or off depending on your preferences. This setup guide will not go over all the options of each tool, but just the minor features that will make it easier to read back data from the connected devices.
Example setup using Putty
Typing help after the application has started will display the list of commands:
Function | Command | Description | Example |
---|---|---|---|
Application commands | |||
HELP | Display available commands. | ||
REG? XXX | Read an ADPD register. <XXX> = register address in hexadecimal | REG? 10A - read register 0x10A | |
REG XXX YYYY | Write an ADPD register. <XXX> = register address in hexadecimal <YYYY> = register new value in hexadecimal | REG 10A 301 - write 0x301 to register 0x10A | |
MODE? | Read the data display mode. Return a 4 character code: CODE - raw data is displayed; ARAT - absolute ratio is displayed; RRAT - relative ratio is displayed; INS1 - data processed for instrument 1 is displayed; INS2 - data processed for instrument 2 is displayed. | ||
MODE XXXX | Set the data display mode. XXXX = 4 character code to describe the data display mode. The options are: CODE - raw data is displayed; ARAT - absolute ratio is displayed; RRAT - relative ratio is displayed; INS1 - data processed for instrument 1 is displayed; INS2 - data processed for instrument 2 is displayed. | MODE CODE - set display mode to raw codes | |
STREAM X | Start calculating and displaying a stream of data. X = If 0 or not present enter continuous streaming mode; if X>0 stream data for X values. | STREAM 10 - stream for 10 values of the output. | |
IDLE? | Queries the idle condition. | ||
IDLE x | If X=0 or not listed only the terminal stream is terminated, but the application continues sampling. If X=1 stop sampling altogether. | IDLE 0 - stop streaming, but keep sampling. | |
ALRM? | Query alarm status; if returned 0 no alarm is present; If bit 0 of the returned value is 1 instrument 2 value is below lower threshold; If bit 1 of the returned value is 1 instrument 2 value is above higher threshold. | ||
DEFn? XXXX | Query operation parameters. n = ID of the required optical path (can be from 0 to 8). XXXX = the operation parameter to be queried. The following options exist: ARAT = absolute ratio expression in reverse polish notation (RPN); RFLT = the digital low pass filter bandwidth applied to the absolute ratio measurements; ALRM = the high and low alarm threshold for the INS2 measurements; RATB = baseline ratio used in calculating the relative ratio; INS1 = the coefficients of the fifth order polynomial used to calculate the first instrument measurements; INS2 = the coefficients of the fifth order polynomial used to calculate the second instrument measurements. | DEF0? ARAT - query the abslute ratio expression for optical path 0 | |
BOOT | Perform a software reset. | ||
ODR? | Query the Output Data Rate of the STREAM command. | ||
ODR XX.XX | Sets Output Data Rate for the STREAM command. XX.XX = The new ODR in Hz. It can have only certain values and will round down to them: ODR options between 5 Hz and 0.01 Hz and can be calculated by 5/ODR = integer number. | ODR 2.5 - set output data rate to 2.5 SPS | |
RATMASK? | Query the active channels mask. Returns a hexadecimal 8 bit number that has 1 for every active channel and 0 for every hidden channel. For example if 1 - only optical path 0 is turned on; if 3 - Optical paths 0 and 1 are turned on and the rest are hidden; etc. | ||
RATMASK XX | Set the active channels mask. XX = New optical path mask. | RATMASK F - turn on optical paths 0, 1, 2 and 3 and leave the rest(4, 5, 6 and 7) off | |
FL_HELP | Display the tooltip for the flash commands. | ||
PCB-LEDn YY.Y XXX.X | Do an automatic calibration of the specified PCB LED current so that the corresponding ADC channels returns a percentage of the saturation. n = LED ID from the PCB.(1, 2, 3 or 4) YY.Y = percentage of ADC saturation. XXX.X = maximum LED current. If left not specified will default at 338 mA. | PCB-LED1 45.8 190.5 - calibrate LED 1 so that the cresponding optical path(s) return 45.8% from the ADC saturation, but limit the current to 190.5 mA. | |
DEFn args | Set operation parameters. n = ID of the required optical path (can be from 0 to 8). args = operation parameters and their new value. | ||
DEFn ARAT RPN | Set the absolute ratio expression; RPN = new ARAT expression. | DEF0 ARAT A2A1/ - set the optical path 0 absolute ratio to be calculated as (slotA_ch2 / slotA_ch1); | |
DEFn RFLT XX.XX | Set the digital filter bandwidth, in Hz, used for the absolute ratio measurement; XX.XX = new digital filter bandwidth in Hz. | DEF1 RFLT 0.5 - set the optical path 1 digital filter bandwidth to 0.5 Hz. Not all values are possible, query the parameter to get the actual value set; | |
DEFn ALRM XXXX YYYY | Set high and low alarm thresholds for instrument 2 measurements; XXXX = new alarm high threshold; YYYY = new alarm low threshold; | DEF0 ALRM 25 15 - set optical path 0 high alarm threshold to 25 and low alarm threshold to 15; | |
DEFn RATB X.XXXXX | Set baseline ratio for to calculate relative ratio of the signal path; X.XXXXX = new baseline ratio. | DEF2 RATB 2.3 - set the baseline ratio as 2.3 for signal path 2; | |
DEFn INS1 X.XXE+XX Y.YYE+YY … | Set the fifth order polynomial coefficients for calculating instrument 1, ordered from lowest to highest power; | DEF0 INS1 0 1 0.54 1.23e+0 5.48e-4 44.22 - set coefficients for optical path 0; | |
DEFn INS2 X.XXE+XX Y.YYE+YY … | Set the fifth order polynomial coefficients for calculating instrument 2, ordered from lowest to highest power; | DEF4 INS2 0 1 0.54 1.23e+0 5.48e-4 44.22 - set coefficients for optical path 4; | |
Flash commands | |||
FL_CLEARBUF | Clear the software buffer. | ||
FL_LOAD X | Load the software buffer with data from flash configuration page. x = 0 to load from User Update page; 1 to load from the Manufacture Default page. | ||
FL_PROGRAM X | Program the flash configuration page with data from the software buffer. x = 0 to program the User Update page; key to program the Manufacture Default page. | ||
FL_ERASE X | Erase the flash configuration page. x = 0 to erase the User Update page; key to erase the Manufacture Default page. | ||
FL_APPLY | Settings currently in the software buffer are applied to the application and device. | ||
FL_WRITE CMD | Save a specific device or application parameter into the software buffer. cmd = register or application command to input the relevant parameter. For register commands the buffer contains an array of register-value pairs that will be written in order to the device. Calling this function with a register command will add a new register-value pair at the end of the array. The only application command supported by this command is the def command. Calling the DEF command will update that value into the software buffer. It can be later applied to the application. | FL_WRITE REG 10A 3355 - write the register 0x10A to the value 0x3355. FL_WRITE DEF2 RFLT 0.01 - set filter bandwidth of ration 2 to 0.01Hz |
|
FL_READ CMD | Read a specific device or application parameter value from the software buffer. cmd = register or application command to input the relevant parameter. For register commands the buffer contains an array of register-value pairs that will be written in order to the device. Calling this function with a regiter command will display the value of the first occurrence of the register. The only application command supported by this command is the def command. Calling the DEF command will read that value from the software buffer. | FL_READ REG? 10A - return the first value of the register 0x10A FL_READ DEF2? RFLT - display the setting of the ration 2 filter bandwidth from the software buffer. |
- ADD CLI PICTURE
We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace.
The source code and include files of the ADuCM3029_demo_cn0503 can be found here:
The official tool we promote for use with the EVAL-ADICUP3029 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.
The program is composed of two main parts:
Board setup initializes UART, SPI and I2C communication and verifies if there is an active EVAL-CN0414-ARDZ board connected by reading the AD4111 ID register. Here is also initialized the update timer for the internal channel registers.
The main process routine implements the CLI and calls the commands input by the user. This routine also checks the flags asserted in the asynchronous events (the update channel register flag, the HART received flag and the floating channel flags) and calls the appropriate handler methods. There is also a flag asserted by the channel register update rate and the ADC output data rate. If the update rate would be too close to the output data rate, the actual update rate might slow down to be possible for the program to maintain all functionality. The update rate may never be bigger or equal to the ADC output data rate divided by 8 (for 8 channels).
The flow chart below represents the way the channel registers are updated. Only one channel is active at any one time (the channel that must be read).
End of Document