Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0415 [05 Mar 2021 04:09] – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceoresources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0415 [19 Aug 2021 07:12] (current) – title word spell edit erbe reyta
Line 1: Line 1:
-====== Solenoind Closed Loop Control Demo ======+====== Solenoid Closed Loop Control Demo ======
  
 The **ADuCM3029_demo_cn0415** provides a solution for controlling and monitoring solenoid actuator current, using an **EVAL-CN0415-ARDZ** shield installed on an **EVAL-ADICUP3029** base board. The user interface is implemented as a command line interface (CLI) through a serial UART connection. The project is created using **CrossCore Embedded Studio** and **GNU ARM compiler**. The **ADuCM3029_demo_cn0415** provides a solution for controlling and monitoring solenoid actuator current, using an **EVAL-CN0415-ARDZ** shield installed on an **EVAL-ADICUP3029** base board. The user interface is implemented as a command line interface (CLI) through a serial UART connection. The project is created using **CrossCore Embedded Studio** and **GNU ARM compiler**.
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0415.1614913768.txt.gz · Last modified: 05 Mar 2021 04:09 by Zuedmar Arceo