Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0397 [20 Jul 2017 20:49] – added more step by step details Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0397 [03 Jan 2021 21:55] – fix links Robin Getz |
---|
===== General Description/Overview ===== | ===== General Description/Overview ===== |
| |
The **ADICUP3029_CN0397** project uses the [[http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0397|EVAL-CN0397-ARDZ shield]] which is a single-supply, low power, low noise, 16-bit light detector utilizing wavelength specific photodiodes. The photodiodes used in this circuit are sensitive at different wavelengths, to read light intensity levels over the visible light spectrum where the plants are photosynthetically active. | The **ADICUP3029_CN0397** project uses the [[adi>en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0397|EVAL-CN0397-ARDZ shield]] which is a single-supply, low power, low noise, 16-bit light detector utilizing wavelength specific photodiodes. The photodiodes used in this circuit are sensitive at different wavelengths, to read light intensity levels over the visible light spectrum where the plants are photosynthetically active. |
| |
\\ | \\ |
The **EVAL-CN0397-ARDZ** board uses [[http://www.analog.com/ad8500|AD8500]], a low power, precision CMOS op amp with a low input bias current of a typical 1pA which is used in a transipedance amplifier configuration to convert the current output of the photodiodes into voltage. It also features [[http://www.analog.com/ad7798|AD7798]] a 3-channel, low noise, low power 16-bit ADC that converts the analog voltage into digital data in for the processing of data into light intensity. The circuit utilizes RGB photodiodes from Everlight with their peak sensitivities 620nm (**R**), 550nm (**G**) and 470nm (**B**). | The **EVAL-CN0397-ARDZ** board uses [[adi>ad8500|AD8500]], a low power, precision CMOS op amp with a low input bias current of a typical 1pA which is used in a transipedance amplifier configuration to convert the current output of the photodiodes into voltage. It also features [[adi>ad7798|AD7798]] a 3-channel, low noise, low power 16-bit ADC that converts the analog voltage into digital data in for the processing of data into light intensity. The circuit utilizes RGB photodiodes from Everlight with their peak sensitivities 620nm (**R**), 550nm (**G**) and 470nm (**B**). |
| |
The **ADICUP3029_CN0397** application perform ADC readings for all 3 channels, processes them and make all necessary calculations in order to provide light intensity and light concentration for each color. | The **ADICUP3029_CN0397** application perform ADC readings for all 3 channels, processes them and make all necessary calculations in order to provide light intensity and light concentration for each color. |
| |
| |
The 16-bits ADC data are received using **SPI interface** of the EVAL-ADICUP360 board. The **UART interface** (**9600** baud rate and **8-bits** data length) is used to send(and to receive) data to (from) a terminal window. | The 16-bits ADC data are received using **SPI interface** of the EVAL-ADICUP3029 board. The **UART interface** (**9600** baud rate and **8-bits** data length) is used to send(and to receive) data to (from) a terminal window. |
| |
**Light intensity** [Lux] is calculated using ADC output value for selected channel and a constant value for each color: | **Light intensity** [Lux] is calculated using ADC output value for selected channel and a constant value for each color: |
===== Configuring the Software ===== | ===== Configuring the Software ===== |
| |
In the //cn0398_app.h// header files you can configure the following parameters: | In the //cn0397_app.h// header files you can configure the following parameters: |
\\ | \\ |
* **ADI_APP_DISPATCH_TIMEOUT** - //DISPATCH TIMEOUT// will define how often the data is sent over Bluetooth. | * **ADI_APP_DISPATCH_TIMEOUT** - //DISPATCH TIMEOUT// will define how often the data is sent over Bluetooth. |