The ADICUP3029_CN0397 is a RGB light detection demo project for the EVAL-ADICUP3029 base board with additional EVAL-CN0397-ARDZ shield, created using the Analog Devices Cross Core Embedded Studio.
The ADICUP3029_CN0397 project uses the EVAL-CN0397-ARDZ shield which is a single-supply, low power, low noise, 16-bit light detector utilizing wavelength specific photodiodes. The photodiodes used in this circuit are sensitive at different wavelengths, to read light intensity levels over the visible light spectrum where the plants are photosynthetically active.
The EVAL-CN0397-ARDZ board uses AD8500, a low power, precision CMOS op amp with a low input bias current of a typical 1pA which is used in a transipedance amplifier configuration to convert the current output of the photodiodes into voltage. It also features AD7798 a 3-channel, low noise, low power 16-bit ADC that converts the analog voltage into digital data in for the processing of data into light intensity. The circuit utilizes RGB photodiodes from Everlight with their peak sensitivities 620nm (R), 550nm (G) and 470nm (B).
The ADICUP3029_CN0397 application perform ADC readings for all 3 channels, processes them and make all necessary calculations in order to provide light intensity and light concentration for each color.
The 16-bits ADC data are received using SPI interface of the EVAL-ADICUP3029 board. The UART interface (9600 baud rate and 8-bits data length) is used to send(and to receive) data to (from) a terminal window.
Light intensity [Lux] is calculated using ADC output value for selected channel and a constant value for each color:
Light Intensity = CODE * Light intensity Constant
Light Concentration [%] is calculated based on the light intensity and optimal level for each color:
Light concentration = Intensity*100/Optimal Level
Beside light intensity and light concentration values, for each channel will be displayed a colored bar in [0%, 100%] format for light concentration representation. It will inform the user when the concentration for a specific channel will reach 100%. Application offer the possibility to perform a system offset calibration for each RGB channel. All calculation are using data specific to each color of the used LEDs:
The following is a list of items needed in order to replicate this demo.
In the cn0397_app.h header files you can configure the following parameters:
The CN0397 needs to be calibrated first before using it in order to achieve best performance. A system zero offset calibration needs to be run to cancel the offset for all of the channels.
Calibration, which is enabled by default, can be done by covering and not allowing any light to reach the photodiodes within the first 5 second of the program start.
Once all the channels have been calibrated, the circuit is now ready for use. The output data will be available for each LED on android device if enabled.
Once the hardware setupand software is configured, user needs to select how they want to view the data coming from Visible Light Detection\Measurement demo.(CN0397)
There are three different ways to visualize the data:
Depending on how you want to operate the board and visualize the data, there are two different options that must be selected from. Below is a table outlining the general operation, and you need to click on which launch file you need to program onto the EVAL-ADICUP3029, and hit the <F5> key on your keyboard.
Data Output Destination | Connected to Debugger | Configuration File |
---|---|---|
CCES Console Window | Yes | ADICUP3029_Debug.launch |
PC/Laptop Serial Terminal | No | ADICUP3029_Release.launch |
IoTNode Smart App | Yes | ADICUP3029_Debug.launch |
IoTNode Smart App | No | ADICUP3029_Release.launch |
Debug launch mode is used when connected to the debugger. In debug mode, all the outputs are directed to the console window of the CrossCore tools via semihosting. The data is also sent by default to the IoTNode smart app (ADI_APP_USE_BLUETOOTH =1), but can be turned of if desired by setting ADI_APP_USE_BLUETOOTH = 0.
Figure shows when ADI_APP_USE_BLUETOOTH is set to 1, sensor data is sent to the smart app. If you have the app installed on your phone, these figure shows the output on android device.
Do not try to connect directly (or pair) to the EVAL-ADICUP3029 from your phone.
Figure shows when ADI_APP_USE_BLUETOOTH is set to 0.
Release launch mode is used for running without the debugger connected. When in release mode, console output is redirected to UART. Bluetooth is enabled, and sensor data is sent to android application. If disabled, sensor data is directed only to the UART. If you are using the UART to make print to the PC/laptop, here are the settings your TCP client must be set too. Following is the UART configuration.
Select COM Port Baud rate: 9600 Data: 8 bit Parity: none Stop: 1 bit Flow Control: none
If ADI_APP_USE_BLUETOOTH is set to 1, BLE will advertise and UART terminal will wait for an connection. Now start the Android App and tap scan. Once device is found, App will show CN0397 Light Demo which is the Bluetooth device name for ADICUP3029_CN0397 demo. Tap on it to connect. Sensor data can now be seen on Android App as well as terminal. If you have the app installed on your phone, these figure shows the output on android device.
Do not try to connect directly (or pair) to the EVAL-ADICUP3029 from your phone.
There are two basic ways to program the ADICUP3029 with the software for the CN0397.
Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design
Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain.
The software for the ADuCM3029_demo_cn0397 can be found here:
Prebuilt CN0414 Hex File
Complete CN0414 Source Files
The official tool we promote for use with the EVAL-ADICUP3029 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.
After completion of the steps above the program will be loaded onto the system FLASH and it will run by default every time the board is powered up.
The ADICUP3029_CN0397 is a C project that uses ADuCM3029 C/C++ Project structure.
This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripherals; port configuration for ADC, SPI read/write; configuring and reading from AD7798, UART read/write functions; calibration and calculation of light information.
cn0397_app.cpp and cn0397.h are the main source and header files related to ADICUP3029_CN0397 application. Visible light sensor (CN0397) drivers are located in RTE/Sensor folder. All ADuCM3029 related drivers can be found under RTE/ADuCM3029 folder. BLE related files can be seen under RTE/Board_Support folder.
pinmux.c – contains GPIO pinmuxing for UART and SPI.
End of Document