This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [29 May 2017 05:25] – created Srinivas Gollakota | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_blink [23 Nov 2022 16:23] – [Obtaining the Source Code] updated to no-os repo for project files Brandon Bushey | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== General Description/ | ===== General Description/ | ||
- | The **ADICUP3029_Blink** project uses [[http:// | + | The **ADICUP3029_Blink** project uses [[adi>en/ |
+ | ===== Demo Requirements | ||
+ | |||
+ | The following is a list of items needed in order to replicate this demo. | ||
+ | * Hardware | ||
+ | * EVAL-ADICUP3029 | ||
+ | * Mirco USB to USB cable | ||
+ | * PC or Laptop with a USB port | ||
+ | * Software | ||
+ | * CrossCore Embedded Studio (2.6.0 or higher) | ||
+ | * ADuCM302x DFP (2.0.0 or higher) | ||
+ | * ADICUP3029 BSP (1.0.0 or higher) | ||
+ | |||
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== | ||
No specific hardware setup required for this demo | No specific hardware setup required for this demo | ||
Line 21: | Line 33: | ||
===== Obtaining the Source Code ===== | ===== Obtaining the Source Code ===== | ||
- | We recommend not opening the project directly, but rather use CCES example browse to open the project. Below screen shot shows how to open project from CCES Example browser. | + | The source code and include files of the **ADuCM3029_Blink** demo can be found here: |
- | + | ||
- | {{: | + | |
- | + | ||
- | + | ||
- | + | ||
- | The source code and include files of the **ADICUP3029_Blink** demo can be found here: | + | |
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | <fc #ff0000>**ADD GITHUB LINK HERE!**</fc> | + | [[repo> no-OS/tree/ |
</ | </ | ||
Line 48: | Line 54: | ||
==== Project Structure ==== | ==== Project Structure ==== | ||
- | The **ADICUP3029_ADXL362** is a C project that uses ADuCM3029 C/C++ Project structure. | + | The **ADICUP3029_Blink** is a C project that uses ADuCM3029 C/C++ Project structure. |
- | This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripherals; | ||
- | |||
{{: | {{: | ||
\\ | \\ | ||
blinky_example.c and blinky_example.h are the main source and header files related to **ADICUP3029_Blink** be found under Source folder. | blinky_example.c and blinky_example.h are the main source and header files related to **ADICUP3029_Blink** be found under Source folder. | ||
- | |||
// End of Document // | // End of Document // | ||