This is an old revision of the document!
The ADICUP3029_Blink is a Blink LED demo project for the EVAL-ADICUP3029 base board which is created using the Analog Devices Cross Core Embedded Studio.
The ADICUP3029_Blink project uses EVAL-ADICUP3029 which is an Ultra Low Power, Arduino compatible ARM Cortex M3 based platform. The platform support various sensor shields.
No specific hardware setup required for this demo
No specific configuration required for this demo
This example blinks the DS3 (green) and DS4 (red) LEDs on the EVAL-ADICUP3029 board. The example blinks the two LEDs in a binary count pattern. The test runs for a fixed number of iterations before exits. All Done message is printed on to console once program exits.
We recommend not opening the project directly, but rather use CCES example browse to open the project. Below screen shot shows how to open project from CCES Example browser.
The source code and include files of the ADICUP3029_Blink demo can be found here:
ADD GITHUB LINK HERE!
The official tool we promote for use with the EVAL-ADICUP3029 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.
The ADICUP3029_ADXL362 is a C project that uses ADuCM3029 C/C++ Project structure.
This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripherals; port configuration for SPI read/write; configuring and reading from ADXL362, UART read/write functions;
blinky_example.c and blinky_example.h are the main source and header files related to ADICUP3029_Blink be found under Source folder.
End of Document