This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:tools:sensorpal_setup_guide [26 Sep 2018 14:09] – created Micheál Lambe | resources:eval:user-guides:eval-ad5940:tools:sensorpal_setup_guide [10 Mar 2022 06:33] (current) – Hans Laurence Josafat | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== How to setup and use SensorPal ====== | ====== How to setup and use SensorPal ====== | ||
- | This page provides | + | SensorPal is an easy to use configuration tool designed to work with the the **EVAL-AD5940BIOZ, |
+ | |||
+ | =====Download Instructions===== | ||
+ | To download | ||
+ | - AD5940 [[adi> | ||
+ | {{ : | ||
+ | |||
+ | =====Installation Instructions===== | ||
+ | - Navigate | ||
+ | - Follow the Install Wizard instructions to complete the setup. | ||
+ | - When complete click Finish | ||
+ | |||
+ | =====How to Use SensorPal===== | ||
+ | - To launch SensorPal go to the start menu-> All Programs-> | ||
+ | - To get started ensure the AD5940 evaluation kit is connected to the PC. Click on the Firmware Load button in the top toolbar as per below screenshot. {{ : | ||
+ | - Select the correct board, it should be similar to DAPLINK(E: | ||
+ | - Once the firmware is loaded plug out the evaluation kit from the PC and reconnect to power cycle the hardware. | ||
+ | - In the center of the screen hit the refresh symbol beside the Com port drop-down text box. Then select the com port the ADICUP3029 microcontroller is connected to from the drop down list. {{ : | ||
+ | - To select an application to run, drag it from the left hand column of techniques and drop into the Work Area. A number of configurable parameters are available. Modify them as required. | ||
+ | - To begin a measurement click on the green Measure button to the right side of the GUI. | ||
+ | - The measurement results will be displayed in the graph window. | ||
+ | - To stop a measurement click on the Abort Measurement button. |