This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:tools:sensorpal_setup_guide [15 Mar 2021 12:54] – [How to setup and use SensorPal] Micheál Lambe | resources:eval:user-guides:eval-ad5940:tools:sensorpal_setup_guide [10 Mar 2022 06:33] (current) – Hans Laurence Josafat | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== How to setup and use SensorPal ====== | ====== How to setup and use SensorPal ====== | ||
- | SensorPal is an easy to use configuration tool designed to work with the the **EVAL-AD5940BIOZ, | + | SensorPal is an easy to use configuration tool designed to work with the the **EVAL-AD5940BIOZ, |
+ | =====Download Instructions===== | ||
+ | To download the latest SensorPal installer click on the link below. **Note**, if the link do not open correctly, try using an alternative browser such as Google Chrome, Microsoft Edge, etc. | ||
+ | - AD5940 [[adi> | ||
+ | {{ : | ||
=====Installation Instructions===== | =====Installation Instructions===== |