This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-ad5940:tools:keil_setup_guide [20 Nov 2018 13:00] – Updated Micheál Lambe | resources:eval:user-guides:eval-ad5940:tools:keil_setup_guide [16 Jun 2019 09:42] – Dave A | ||
---|---|---|---|
Line 18: | Line 18: | ||
</ | </ | ||
- Navigate to the **examples-> | - Navigate to the **examples-> | ||
- | - Double click on ADICUP3029.uvprojx file to open the project in Keil | + | - Double click on ADICUP3029.uvprojx file to open the project in Keil [The package at https:// |
- The project structure is shown in the left hand side of the screen. It is divided into 4 sub sections: | - The project structure is shown in the left hand side of the screen. It is divided into 4 sub sections: | ||
* **AD5940Lib** - This conatins the AD5940.c source file which has all the AD5940 library functions. This file is common to all examples. The ADICUP3029Port.c file is located here also and contains port functions for the ADuCM3029 microcontroller. | * **AD5940Lib** - This conatins the AD5940.c source file which has all the AD5940 library functions. This file is common to all examples. The ADICUP3029Port.c file is located here also and contains port functions for the ADuCM3029 microcontroller. |