How to setup and use Keil IDE
The AD5940 SDK provides support for Keil IDE to develop firmware. Keil provides an evaluation licence that is free but limits the code size to 32 kB. Currently, none of the evaluation examples in the AD5940 development pack exceed this.
How to Download Keil
To download Keil IDE click on the following link https://www.keil.com/demo/eval/arm.htm
This will open up a form which must be filled out to download the software. Click Submit when complete to begin the download process.
Once the software has downloaded an evaluation licence is required. Keil offers two different evaluation licences, time limited and size limited. Choose the size limited licence. This limits the allowable code size to 32kB. All the AD5940 example projects are within this limitation.
The latest versions of Keil use the ARM compiler v6, but the example code still uses v5, and refuses to compile under v6. Therefore, you will also need to download the legacy compiler, and install it at the correct location (not the default location), as shown in https://developer.arm.com/documentation/ka005073/latest
How to edit and run example code in Keil
To edit and run example code in Keil follow these steps:
Download the AD5940 SDK from the the GitLab repository:
(Hint: Also download the included submodule in examples/ad5940lib. This can be done with the git bash in one step by executing: “git clone --recurse-submodules https://github.com/analogdevicesinc/ad5940-examples.git” (without the double quotes))
Navigate to the examples→AD5940_ADC→ADICUP3029
-
The project structure is shown in the left hand side of the screen. It is divided into 4 sub sections:
AD5940Lib - This contains the AD5940.c source file which has all the AD5940 library functions. This file is common to all examples. The ADICUP3029Port.c file is located here also and contains port functions for the ADuCM3029 microcontroller.
Application - This sub section contains the application code and main.c file.
CMSIS - This contains the arm CMSIS math library.
Device - This folder contains the startup code for the ADuCM3029 micrcontroller. These files should not be modified.

Double click on AD5940_ADCPolling.c to open the file in the editor.
Modify code as required.
To compile and build the project go to Project→Rebuild all target files. It may take a couple of seconds to fully compile all the source code.
If you see build errors like 'Fatal Error[Pe1696]: cannot open source file “adi_cycle_counting_config.h”', you need to add/adjust include paths:
Click Menu > Project > Options > C/C++ Compiler > Preprocessor > Additional include directories (click on the three dots on the right)
Click on '<Click to add>'
Find the file on your computer and add it,
e.g. navigate to (and then select): 'C:\ad5940-examples\examples\AD5940_BATImpedance\ADICUP3029\RTE\Device\ADuCM3029' (adjust the path depending on where you stored the example folder, which example project you use and which include file is missing)
Click OK twice, then Menu > Project > Clean
Click Menu > Project > Rebuild All
To download the code to the evaluation boards first ensure the boards are connected to the PC or laptop. Then click on the red icon in the toolbar to download the source code and begin the debugging session.

To set breakpoints click to the left of the line of code. A red dot will appear as in below screenshot.
To begin executing press the “Run” button which is highlighted in below screenshot.

Hint: If downloading the code didn't work because of an error like this: 'Failed to load flash loader: C:/Users/YourUsername/IAR-CMSIS-Packs/AnalogDevices/ADUCM302x_DFP/3.2.0/\ARM\config\flashloader\AnalogDevices\FlashADUCM3029.flash':