This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-ad5940:tools:keil_setup_guide [16 Jun 2019 09:41] – Dave A | resources:eval:user-guides:eval-ad5940:tools:keil_setup_guide [24 Aug 2021 11:34] – [How to Download Keil] Tracey Johnson | ||
---|---|---|---|
Line 7: | Line 7: | ||
This will open up a form which must be filled out to download the software. Click Submit when complete to begin the download process. | This will open up a form which must be filled out to download the software. Click Submit when complete to begin the download process. | ||
- | Onve the software has downloaded an evaluation licence is required. Keil offers two different evaluation licences, time limited and size limited. Choose the size limited licence. This limits the allowable code size to 32kB. All the AD5940 example projects are within this limitation. | + | Once the software has downloaded an evaluation licence is required. Keil offers two different evaluation licences, time limited and size limited. Choose the size limited licence. This limits the allowable code size to 32kB. All the AD5940 example projects are within this limitation. |
===== How to edit and run example code in Keil===== | ===== How to edit and run example code in Keil===== | ||
Line 18: | Line 18: | ||
</ | </ | ||
- Navigate to the **examples-> | - Navigate to the **examples-> | ||
- | - Double click on ADICUP3029.uvprojx file to open the project in Keil [The package at https:// | + | - Double click on ADICUP3029.uvprojx file to open the project in Keil [The package at https:// |
- The project structure is shown in the left hand side of the screen. It is divided into 4 sub sections: | - The project structure is shown in the left hand side of the screen. It is divided into 4 sub sections: | ||
* **AD5940Lib** - This conatins the AD5940.c source file which has all the AD5940 library functions. This file is common to all examples. The ADICUP3029Port.c file is located here also and contains port functions for the ADuCM3029 microcontroller. | * **AD5940Lib** - This conatins the AD5940.c source file which has all the AD5940 library functions. This file is common to all examples. The ADICUP3029Port.c file is located here also and contains port functions for the ADuCM3029 microcontroller. |