This is an old revision of the document!
This demo will use EVAL-ADICUP3029, EVAL_AD5940BIOZ and Impedance-Test board to carry out BIA measurements.
This example project is designed to carry out body impedance analysis (BIA) measurements. The Impedance Test board is provided with the hardware which models body impedance. It consists of a range of resistors and capacitors which can be used to model body impedance, contact impedance and electrode impedance.
Alternatively, the custom cables can be connected to the body to measure actual body impedance.
The following is a list of items required to carry out the measurement.
The AD5940 Z Test board is designed to model skin impedance, body impedance, electrode contact impedance and electrode impedance. There are 5 banks of switches on the board labelled S1, S2, S3, S4 and S5. The function of each bank is described in the following table:
Switch Bank | Bank Function |
---|---|
S1 | Used to model Body Impedance |
S2 | Used to model contact impedance on F+ electrode |
S3 | Used to model contact impedance on S+ electrode |
S4 | Used to model contact impedance on F- electrode |
S5 | Used to model contact impedance on S- electrode |
The following tables indicate the resistor or capacitor value associated with each switch in the bank. Moving the switch to the ON position connects the corresponding resistor or capacitor value in series on the signal path. If more than one switch is active the corresponding resistor values are connected in series.
S1 Bank | Corresponding Res/Cap Value |
---|---|
S1 | 100 Ω |
S2 | 200 Ω |
S3 | 300 Ω |
S4 | 340 Ω |
S5 | 510 Ω |
S6 | 1 kΩ |
S7 | 2 kΩ |
S8 | 3.01 kΩ |
S9 | 4.02 kΩ |
S10 | 4.99 kΩ |
S11 | 1000 pF |
S12 | 0.01 μF |
S2 Bank | Corresponding Res/Cap Value |
---|---|
S1 | 100 Ω |
S2 | 200 Ω |
S3 | 300 Ω |
S4 | 402 Ω |
S5 | 10 kΩ |
S6 | 23.7 kΩ |
S7 | 42.2 kΩ |
S8 | 42.2 kΩ |
S9 | 100 kΩ |
S10 | 200 kΩ |
S11 | 1000 pF |
S12 | 0.01 μF |
S3 Bank | Corresponding Res/Cap Value |
---|---|
S1 | 100 Ω |
S2 | 200 Ω |
S3 | 300 Ω |
S4 | 402 Ω |
S5 | 4.22 MΩ |
S6 | 4.22 MΩ |
S7 | 1.43 MΩ |
S8 | 1 MΩ |
S9 | 300 kΩ |
S10 | 300 kΩ |
S11 | 1000 pF |
S12 | 0.01 μF |
S4 Bank | Corresponding Res/Cap Value |
---|---|
S1 | 100 Ω |
S2 | 200 Ω |
S3 | 300 Ω |
S4 | 402 Ω |
S5 | 499 Ω |
S6 | 1 kΩ |
S7 | 2 kΩ |
S8 | 3.01 kΩ |
S9 | 4.02 kΩ |
S10 | 4.99 kΩ |
S11 | 1000 pF |
S12 | 0.01 μF |
S5 Bank | Corresponding Res/Cap Value |
---|---|
S1 | 100 Ω |
S2 | 200 Ω |
S3 | 300 Ω |
S4 | 402 Ω |
S5 | 499 Ω |
S6 | 1 kΩ |
S7 | 2 kΩ |
S8 | 3.01 kΩ |
S9 | 4.02 kΩ |
S10 | 4.99 kΩ |
S11 | 1000 pF |
S12 | 0.01 μF |
The source code and include files for the project can be found on Git
To compile and run the example open the project in either Keil or IAR. The AD5940BIAStructInit() function configures the main application parameters. These include the sample frequency (BiaODR), and number of samples to feed to DFT block (DFT_Num). Compile the project and download to the hardware.
The measurement results are sent to the PC via UART. To establish connection over UART, connect the Micro-USB cable to the PC and to the EVAL-ADICUP3029 board. A terminal program such as RealTerm or Putty is required to display the results
Following is the UART configuration.
Select COM Port Baud rate: 230400 Data: 8 bit Parity: none Stop: 1 bit Flow Control: none
The data on the terminal consists of the Frequency of the excitation signal, the magnitude of the impedance and the phase of the impedance in degrees as in below screenshot.