This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940elcz [24 Sep 2019 19:58] – Corrected JP10/11 labels to match AN-1563.pdf Andy Akers | resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940elcz [12 Feb 2024 14:38] (current) – [USB Connector and Cable] Akila M | ||
---|---|---|---|
Line 33: | Line 33: | ||
| ::: | B| Connect network B to CE, RE and SE | | | ::: | B| Connect network B to CE, RE and SE | | ||
^JP9, | ^JP9, | ||
- | ^ JP9 (DE0 Mux) | A| DE0 connected to Gas sensor connector | | + | ^ JP9 (DE0 Mux) | A| DE0 connected to gas sensor connector | |
| ::: | B| DE0 connected to dummy network | | ::: | B| DE0 connected to dummy network | ||
| ::: | C| DE0 connected to USB port | | | ::: | C| DE0 connected to USB port | | ||
Line 51: | Line 51: | ||
The following table shows which color lead corresponds to which input: | The following table shows which color lead corresponds to which input: | ||
- | ^ Connector | + | ^ Cable Color ^Description ^ Schematic Reference ^ |
| Red | Counter Electrode | USB_1 | | Red | Counter Electrode | USB_1 | ||
- | | Blue | Reference Electrode | USB_2 | | + | | Blue/white | Reference Electrode | USB_2 | |
| Green | Working Electrode | USB_3| | | Green | Working Electrode | USB_3| | ||
| Black | Connected to DE0 input | USB_4| | | Black | Connected to DE0 input | USB_4| | ||
Line 62: | Line 62: | ||
Note, the USB to crocodile cable is intended for rapid prototyping. There is a parasitic resistance and capacitance associated with it which may effect measurement accuracy. This is especially through for high frequency impedance measurements. | Note, the USB to crocodile cable is intended for rapid prototyping. There is a parasitic resistance and capacitance associated with it which may effect measurement accuracy. This is especially through for high frequency impedance measurements. | ||
===== EC Gas Connector ===== | ===== EC Gas Connector ===== | ||
- | M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position | + | M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position |
===== BNC Connector ===== | ===== BNC Connector ===== | ||
The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor' | The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor' | ||
Line 69: | Line 69: | ||
EVAL-AD5940ELCZ Rev A Design and Integration Files | EVAL-AD5940ELCZ Rev A Design and Integration Files | ||
- | * {{ : | + | * {{: |
* {{ : | * {{ : | ||
- | * {{ : | + | * {{ : |
* {{ : | * {{ : | ||
</ | </ |