Wiki

This version (12 Feb 2024 14:38) was approved by Akila M.The Previously approved version (10 Aug 2021 12:01) is available.Diff

AD5940 Electrochemical Shield User Guide

Introduction

The EVAL-AD5940ELCZ shield was designed specifically for carrying out electrochemical measurements. These include:

  • Measurements on a dummy RC sensor
  • Electrochemical Gas Sensing
  • Water Quality
    • Conductivity
    • pH
    • Oxidation Reduction
  • General electrochemical measurements through cables provided

The platform is an Arduino form factor that can be used with any Arduino form-factor base board. This section describes the features of the evaluation board and how to use it.

Connectors and Jumpers

All the connectors and their default configurations are described in the table below.

Connector Jmpr Position. Description
JP1 (DVDD) A DVDD powered from 3.3V on Arduino Header (Default)
B DVDD powered from LDO
C DVDD powered from external source connected to P11
JP2 (AVDD) A AVDD powered from 3.3V on Arduino Header (Default)
B AVDD powered from LDO
C AVDD powered from external source connected to P8
JP3 (Reset) A Reset pin connected to ARST Button (Default)
B Reset pin connected to Arduino Header Reset pin
C Reset pin connected to Arduino header P1.3 (Default)
P9 (LDO Enable) 1-2 LDO Enabled
2-3 LDO Disabled (Default)
P10 (LDO Aux Enable) 1-2 LDO Enabled
2-3 LDO Disabled (Default)
JP6 (Dummy RC) A Connect network A to CE, RE and SE (Default)
B Connect network B to CE, RE and SE
JP9,JP10,JP11 Note, A is 1-2, B is 3-4, C is 5-6 (USB)
JP9 (DE0 Mux) A DE0 connected to gas sensor connector
B DE0 connected to dummy network
C DE0 connected to USB port
JP10 (RE0 Mux) A RE0 connected to gas sensor
B RE0 connected to dummy network
C RE0 connected to USB port
JP11 (SE0 Mux) A SE0 connected to gas sensor
B SE0 connected to dummy network
C SE0 connected to USB port
JP4 (Cable Shield Mux) A Shield connected to CE0
B Shield connected to Bead
JP5 (BNC Mux) A Water conductivity
B pH Measurement
C Connected to AFE1

USB Connector and Cable

The USB connector provides an interface to connected the provided USB to Crocodile cable to the AD5940. This USB connector is only intended to be used in conjunction with the provided USB to crocodile cable. No other USB cable should be ever be connected.

The following table shows which color lead corresponds to which input:

Cable Color Description Schematic Reference
Red Counter Electrode USB_1
Blue/white Reference Electrode USB_2
Green Working Electrode USB_3
Black Connected to DE0 input USB_4

The image below shows the crocodile connected to the EVAL-AD5940ELCZ. A dummy sensor consisting of a Resistor in parallel with a capacitor is connected. The counter and reference connectors are connected to one end and the working electrode is connected to the other end.

Note, the USB to crocodile cable is intended for rapid prototyping. There is a parasitic resistance and capacitance associated with it which may effect measurement accuracy. This is especially through for high frequency impedance measurements.

EC Gas Connector

M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position A.

BNC Connector

The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor's such as pH sensors and for water conductivity measurements.

Schematics, PCB Layout, Bill of Materials

resources/eval/user-guides/eval-ad5940/hardware/eval-ad5940elcz.txt · Last modified: 12 Feb 2024 14:38 by Akila M