This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940elcz [29 May 2019 07:13] – Dave A | resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940elcz [12 Feb 2024 14:38] (current) – [USB Connector and Cable] Akila M | ||
---|---|---|---|
Line 32: | Line 32: | ||
^ JP6 (Dummy RC) | A| Connect network A to CE, RE and SE (Default) | ^ JP6 (Dummy RC) | A| Connect network A to CE, RE and SE (Default) | ||
| ::: | B| Connect network B to CE, RE and SE | | | ::: | B| Connect network B to CE, RE and SE | | ||
- | ^JP9, | + | ^JP9, |
- | ^ JP9 (DE0 Mux) | A| DE0 connected to Gas sensor connector | | + | ^ JP9 (DE0 Mux) | A| DE0 connected to gas sensor connector | |
| ::: | B| DE0 connected to dummy network | | ::: | B| DE0 connected to dummy network | ||
| ::: | C| DE0 connected to USB port | | | ::: | C| DE0 connected to USB port | | ||
- | ^ JP10 (RE0 Mux) | A| RE0 connected to dummy network | | + | ^ JP10 (RE0 Mux) | A| RE0 connected to gas sensor | |
- | | ::: | B| RE0 connected to gas sensor | + | | ::: | B| RE0 connected to dummy network |
| ::: | C| RE0 connected to USB port | | | ::: | C| RE0 connected to USB port | | ||
- | ^ JP11 (SE0 Mux) | A| SE0 connected to dummy network | | + | ^ JP11 (SE0 Mux) | A| SE0 connected to gas sensor | |
- | | ::: | B| SE0 connected to gas sensor | + | | ::: | B| SE0 connected to dummy network |
| ::: | C| SE0 connected to USB port | | | ::: | C| SE0 connected to USB port | | ||
^ JP4 (Cable Shield Mux)| A| Shield connected to CE0 | | ^ JP4 (Cable Shield Mux)| A| Shield connected to CE0 | | ||
Line 47: | Line 47: | ||
| ::: | B| pH Measurement | | ::: | B| pH Measurement | ||
| ::: | C| Connected to AFE1 | | | ::: | C| Connected to AFE1 | | ||
- | ===== USB Connector ===== | + | ===== USB Connector |
- | The USB connector provides an interface to connected the USB to Crocodile cable to the AD5940. This USB connector | + | The USB connector provides an interface to connected the provided |
+ | |||
+ | The following table shows which color lead corresponds | ||
+ | ^ Cable Color ^Description ^ Schematic Reference ^ | ||
+ | | Red | Counter Electrode | USB_1 | ||
+ | | Blue/ | ||
+ | | Green | Working Electrode | USB_3| | ||
+ | | Black | Connected to DE0 input | USB_4| | ||
+ | |||
+ | The image below shows the crocodile connected to the EVAL-AD5940ELCZ. A dummy sensor consisting of a Resistor in parallel with a capacitor is connected. The counter and reference connectors are connected to one end and the working electrode is connected to the other end. | ||
+ | {{ : | ||
+ | |||
+ | Note, the USB to crocodile cable is intended for rapid prototyping. There is a parasitic resistance and capacitance associated with it which may effect measurement accuracy. This is especially through for high frequency impedance measurements. | ||
===== EC Gas Connector ===== | ===== EC Gas Connector ===== | ||
- | M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position | + | M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position |
===== BNC Connector ===== | ===== BNC Connector ===== | ||
The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor' | The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor' | ||
Line 57: | Line 69: | ||
EVAL-AD5940ELCZ Rev A Design and Integration Files | EVAL-AD5940ELCZ Rev A Design and Integration Files | ||
- | * {{ : | + | * {{: |
* {{ : | * {{ : | ||
- | * {{ : | + | * {{ : |
* {{ : | * {{ : | ||
</ | </ |