Software Packs & Board Support Package
A modular software framework is provided for quick application prototyping. Based on the application use case, developers need to download the respective software packs.
There are no seperate toolchain,software packs and board support package for EV-COG-AD4050WZ, the toolchain,software packs and board support package for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
Please make sure you install either of the below toolchain before installing any of the below packs
IAR Embedded Workbench for ARM 8.20.1 or higher
CrossCore Embedded Studio 2.7.0 ® or higher
The Cog software development kit consists of the following packs:-
-
Version: 3.1.0 - Extended support for IAR Embedded Workbench and Keil uVision. [Latest]
-
Version 3.1.0 - Extended support for IAR Embedded Workbench.[Latest]
End Document
Back