Wiki

This version (13 Feb 2018 11:31) was approved by Pranit Jadhav, Rajalakshmi Jayaraman.The Previously approved version (12 Sep 2017 08:35) is available.Diff

EV-COG-AD4050LZ On-Board Peripheral Drivers & Software

General Description/Overview

The EV-COG-AD4050LZ software pack provides access to all the necessary on-board peripheral drivers for the EV-COG-AD4050LZ development platform. This software layer is the secondary layer needed when writing applications using this development platform. The EV-COG-AD4050LZ software pack builds on top of what the ADuCM4x50 software pack provides. The EV-COG-AD4050LZ software pack makes it easier to use the on-board peripherals so creating your application layer is will be easier. Combined with the ADuCM4x50 and Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD4050LZ development platform.

The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio 2.6.0 ® and the ADuCM4x50 Device Family Pack.

EV-COG-AD4050LZ software pack contains the following components:

  • On-Chip Driver Examples ( GPIO,RTC, SPI, Systick, TMR, UART, WDT)
  • Documentation

For detailed information regarding the EV-COG-AD4050LZ software pack, please see our complete EV-COG-AD4050LZ software user guide.

You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD4050LZ platform.

Downloading the EV-COG-AD4050LZ Software Pack

The software pack can be downloaded in following ways.

  1. Downloaded via the tools program
    • It is recommended to download the EV-COG-AD4050LZ software pack through from the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the EV-COG-AD4050LZ software pack through CrossCore Embedded Studio please see our CrossCore Embedded Studio Quickstart Userguide.
  2. Downloaded to local directory
    • However if you do decide to download the EV-COG-AD4050LZ software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.

Download EV-COG-AD4050LZ Board Support Pack.

End of Document

Back

resources/eval/user-guides/ev-cog-ad4050lz/software/eval-cog-ad4050lz.txt · Last modified: 13 Feb 2018 10:01 by Pranit Jadhav