Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:ev-cog-ad4050lz:tools_driver [12 Aug 2017 09:43] – Pranit Jadhav | resources:eval:user-guides:ev-cog-ad4050lz:tools_driver [14 May 2018 12:26] – . Gowtham shanmugaraj |
---|
====== Tools and Driver Details ====== | ====== Tools and Driver Details ====== |
| |
| <note important>There is no seperate toolchain,DFP,BSP for EV-COG-AD4050WZ, the toolchain,DFP,BSP for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on his/her application.For help regarding pinmapping refer to the Hardware Details section. |
| </note> |
This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. There is also information on the different USB modes and drivers needed. | This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. There is also information on the different USB modes and drivers needed. |
| |
It contains two main sections: | It contains two main sections: |
| |
- **[[resources:eval:user-guides:ev-cog-ad4050lz:tools:cces_download|CrossCore Embedded Studio Download & Install]]** - Provides all the necessary instructions on how to download and install the CrossCore Embedded Studios software development environment. | - **[[resources:eval:user-guides:ev-cog-ad4050wz:tools:cces_download|CrossCore Embedded Studio Download & Install]]** - Provides all the necessary instructions on how to download and install the CrossCore Embedded Studios software development environment. |
* **[[resources:ev:user-guides:ev-cog-ad4050lz:tools:cces_guide|CrossCore Embedded Studio Quickstart Userguide]]** - Provides information about using the CrossCore Embedded Studios IDE, in particular, the process of importing, building, debugging, and creating user applications for the EV-COG-AD4050LZ. | * **[[resources:ev:user-guides:ev-cog-ad4050wz:tools:cces_guide|CrossCore Embedded Studio Quickstart Userguide]]** - Provides information about using the CrossCore Embedded Studios IDE, in particular, the process of importing, building, debugging, and creating user applications for the EV-COG-AD4050LZ. |
- **[[resources:eval:user-guides:ev-cog-ad4050lz:tools:hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]]** - Provides detailed information how to load pre-compiled .HEX or .BIN files using the USB drive of the EV-COG-AD4050LZ board. | - **[[resources:eval:user-guides:ev-cog-ad4050lz:tools:hardware_usb|Driver Installation for On-board Debugger (CMSIS DAP)]]** - Provides detailed information how to load pre-compiled .HEX or .BIN files using the USB drive of the EV-COG-AD4050LZ board. |
| |