There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. There is also information on the different USB modes and drivers needed.
It contains two main sections:
-
CrossCore Embedded Studio Quickstart Userguide - Provides information about using the CrossCore Embedded Studios
IDE, in particular, the process of importing, building, debugging, and creating user applications for the EV-COG-AD4050LZ.
-
End Document
Back