Select all the packs and import. This will install the packs. Ignore the warnings seen on the console window. In order to remove these warnings, additional packs needs to be installed which are available in the last section of this page.
Please refer to this link to download and install mbed serial driver on PC.
Running an Example Project
Power the MCU Cog using a USB (micro-B) Cable. You should see a red LED and a yellow LED turn on by default.
In CCES IDE, click CMSIS Pack Manager icon .
Select EV-COG-AD4050LZ from the Boards tab on the Left panel. (see below image)
Copy button_press example from the Examples tab on the Right panel.
Click C/C++ perspective icon
Under Project Explorer select button_press example, click build icon .
Click on Debug icon once build is complete. Below are the Debug Configuration settings.
Click “ok” on Perspective Switch and Semihosting Enabled window.
Click run on the Debug perspective.
Now press BTN1 or BTN2 on EV-COG-AD4050LZ and inspect corresponding LED.