This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:ev-cog-ad4050lz:help_support [12 Aug 2017 09:27] – created Pranit Jadhav | resources:eval:user-guides:ev-cog-ad4050lz:help_support [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Help and Support ====== | ====== Help and Support ====== | ||
+ | |||
+ | <note >There are no seperate toolchain, | ||
+ | </ | ||
Do you need help or have general support questions, than I hope this page helps you resolve those. | Do you need help or have general support questions, than I hope this page helps you resolve those. | ||
Line 15: | Line 18: | ||
- Program the EV-COG-AD4050LZ | - Program the EV-COG-AD4050LZ | ||
* Sometimes a flashed program doesn' | * Sometimes a flashed program doesn' | ||
- | * The first thing to try in this case, is to [[resources: | + | * The first thing to try in this case, is to [[resources: |
* If drag and drop is not working, it may be necessary to erase the flash. To do so: | * If drag and drop is not working, it may be necessary to erase the flash. To do so: | ||
- | - Download and install the CrossCore Serial Flash Programmer from here: [[http:// | + | - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/ |
- Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | ||
- Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. | - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. | ||
- Select the mbed serial COM port in the CrossCore Serial Flash Programmer, and erase the flash. | - Select the mbed serial COM port in the CrossCore Serial Flash Programmer, and erase the flash. | ||
- | - Then try [[resources: | + | - Then try [[resources: |
* If the mass erase didn't work, and you are trying to drag and drop a large .BIN file on EV-COG-AD4050LZ hardware, it's possible that the mbed interface file needs to be updated to support your application. | * If the mass erase didn't work, and you are trying to drag and drop a large .BIN file on EV-COG-AD4050LZ hardware, it's possible that the mbed interface file needs to be updated to support your application. | ||
- | - Please visit the [[resources: | + | - Please visit the [[resources: |
- | - Once you are in " | + | - Once you are in " |
- Not receiving/ | - Not receiving/ | ||
* Make sure that the UART header (P8) is positioned in the correct destination to transmit/ | * Make sure that the UART header (P8) is positioned in the correct destination to transmit/ | ||
| | ||
This is just a brief self-help guide to troubleshooting common issues. | This is just a brief self-help guide to troubleshooting common issues. | ||
+ | |||
+ | |||
===== Hardware, Software, and Documentation Questions ===== | ===== Hardware, Software, and Documentation Questions ===== | ||
Line 59: | Line 64: | ||
// End of Document // | // End of Document // | ||
+ | |||
+ | |