Help and Support
There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
Do you need help or have general support questions, than I hope this page helps you resolve those.
This page has a quickstart troubleshooting approach that goes over some very general questions and common pitfalls, but if you have a specific issue which requires more information or detail please contact us through EngineerZone or Email. (links can be found further down on the page where to direct specific questions)
What to do When Things Go Wrong
There are many things that can go wrong with an ecosystem this complex, but if you are having issues getting the board or software working, here are a few simple things you can try before contacting Analog Devices.
Check the Power
Program the EV-COG-AD4050LZ
Sometimes a flashed program doesn't run properly or can make it difficult to run the debugger.
The first thing to try in this case, is to
drag and drop a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)
If drag and drop is not working, it may be necessary to erase the flash. To do so:
-
Make sure that the
USB is connected and on
UART header (P8) 1 & 2 and 7 & 8 are shorted.
Power cycle the EV-COG-AD4050LZ board while holding down the boot switch.
Select the mbed serial COM port in the CrossCore Serial Flash Programmer, and erase the flash.
-
If the mass erase didn't work, and you are trying to drag and drop a large .BIN file on EV-COG-AD4050LZ hardware, it's possible that the mbed interface file needs to be updated to support your application.
-
-
Not receiving/transmitting data to the
UART
Make sure that the
UART header (P8) is positioned in the correct destination to transmit/receive
UART data.
This is just a brief self-help guide to troubleshooting common issues. If you have other questions that need answering please direct those requests to the locations outlined below.
Hardware, Software, and Documentation Questions
If you have any questions regarding the EV-COG-AD4050LZ or are experiencing any problems using the software or issues following any of the documentation feel free to ask us a question.
When asking a question please take the time to give a detailed description of your problem. If you are experiencing a problem please state the steps you have executed, the result you expected you would get and the result you actually got. By doing so you enable us to provide you precise and detailed answers in a timely manner.
Before asking questions please take the time to check if somebody else already asked the same question. You might just find your question already answered.
CrossCore Embedded Studio questions
If you have questions regarding the tools and tool chain that is used with the EVAL-ADICUP3029, either post a question or send an email.
End of Document
Back