Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:ev-cog-ad4050lz:help_support [14 May 2018 12:26] – . Gowtham shanmugarajresources:eval:user-guides:ev-cog-ad4050lz:help_support [03 Jan 2021 22:04] (current) – fix links Robin Getz
Line 1: Line 1:
 ====== Help and Support ====== ====== Help and Support ======
  
-<note important>There is no seperate toolchain,DFP,BSP for EV-COG-AD4050WZ, the toolchain,DFP,BSP for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on his/her application.For help regarding pinmapping refer to the Hardware Details section.+<note >There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
 </note> </note>
  
Line 20: Line 20:
     * The first thing to try in this case, is to [[resources:eval:user-guides:ev-cog-ad4050lz:tools:hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)     * The first thing to try in this case, is to [[resources:eval:user-guides:ev-cog-ad4050lz:tools:hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best)
     * If drag and drop is not working, it may be necessary to erase the flash. To do so:       * If drag and drop is not working, it may be necessary to erase the flash. To do so:  
-      - Download and install the CrossCore Serial Flash Programmer from here: [[http://www.analog.com/en/design-center/processors-and-dsp/evaluation-and-development-software/crosscore-serial-flash-programmer.html#dsp-overview]].  +      - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/design-center/processors-and-dsp/evaluation-and-development-software/crosscore-serial-flash-programmer.html#dsp-overview]].  
       - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted.        - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. 
       - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch.        - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. 
resources/eval/user-guides/ev-cog-ad4050lz/help_support.txt · Last modified: 03 Jan 2021 22:04 by Robin Getz