This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ev-cog-ad4050lz:help_support [12 Aug 2017 09:38] – [What to do When Things Go Wrong] Pranit Jadhav | resources:eval:user-guides:ev-cog-ad4050lz:help_support [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Help and Support ====== | ====== Help and Support ====== | ||
+ | |||
+ | <note >There are no seperate toolchain, | ||
+ | </ | ||
Do you need help or have general support questions, than I hope this page helps you resolve those. | Do you need help or have general support questions, than I hope this page helps you resolve those. | ||
Line 17: | Line 20: | ||
* The first thing to try in this case, is to [[resources: | * The first thing to try in this case, is to [[resources: | ||
* If drag and drop is not working, it may be necessary to erase the flash. To do so: | * If drag and drop is not working, it may be necessary to erase the flash. To do so: | ||
- | - Download and install the CrossCore Serial Flash Programmer from here: [[http:// | + | - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/ |
- Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | ||
- Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. | - Power cycle the EV-COG-AD4050LZ board while holding down the boot switch. | ||
Line 31: | Line 34: | ||
- | \\ End Document \\ | ||
- | **[[resources: | ||
===== Hardware, Software, and Documentation Questions ===== | ===== Hardware, Software, and Documentation Questions ===== | ||